Test & Tools
  • Technologies
  • More
Test & Tools
Forum Feasability of Adding a Second Parallel Darlington?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 388 subscribers
  • Views 6228 views
  • Users 0 members are here
  • control
  • voltage
  • darlington
Related

Feasability of Adding a Second Parallel Darlington?

jw0752
jw0752 over 11 years ago

        I am currently working on a small circuit that controls the voltage to an electric dental lab handpiece. Please see the schematic below. This circuit has had a chronic problem with failure of the TIP-122 Darlington. The problem arises when the handpiece operator applies pressure which adds load to the motor and the motor then demands more current from the circuit. This circuit is very simple with basically no overload protection. The original design did not even have a flyback diode across the motor. My question is if it is practical to add another TIP-122 Darlington in parallel with the first one in order to improve current handling capacity. Does anyone have any experience with this type of modification? I also have a curiosity codicil to my question. If it is practical to add another Darlington, what would be the limiting factor to how many parallel Darlingtons can be added in this way? Any insights would be appreciated.

John

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    Hi John, a very good question, and the answer is fairly straight forward If the Darlington is getting overloaded due to exceeding the current limit of the Darlington then an additional one in parallel…
  • vsluiter
    vsluiter over 11 years ago +1
    Hi John, You say that the circuit has no short circuit protection, but the 3k resistor with a hFE of 1000 means some current limit: The supply is 36×√2 -(1.2V diode bridge drop) ≅ 50V. At startup the motor…
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to Problemchild

    image, yup, your right, I just gotta get there , not as easy as it sounds

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to vsluiter

    Hi Victor, This is a motor unit that the dentists use to trim and polish things like dentures outside the mouth. Each time they use it they pick a setting for VR-1 that they want and then they use the handpiece to grind away plastic or polish a surface. As they apply pressure the motor slows and demands more current due to less counter EMF. I have already repaired and sent the unit back or I would be able to measure DC resistance and operational current which I did not do when it was on my bench.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to Robert Peter Oakes

    This is a commercial design that I just pulled off the circuit board onto paper. It is an inexpensive Chinese knock off of an inexpensive Korean unit, which is probably why I am having problems. As I mentioned I followed you last advice and put in an equivalent Darlington with about 40% more tolerance for voltage and current. We will have to wait to see if it comes back to me or not. I have been really impressed with the support I have gotten on this question. Everyone has such good ideas and helpful suggestions. Lucky to have smart friends.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • mcb1
    mcb1 over 11 years ago in reply to jw0752

    John, guys

     

    While you are quite right that it's really just a voltage source with transistor to boost the current, the fact the design destroys transistors means there is a design issue.

     

    The schematic shows a 36vac input and with no smoothing cap gives around 36v output (give or take). This non smooth supply is a bit brutal on the regulator ...

    Full Wave Rectifier and Bridge Rectifier Theory

     

    My checks show that V2 can adjust the regulator from (approx) 2.55v to 38.75v, and the only current limiting is the R-6 1ohm 5w resistor.

    The TIP122 is rated at 5A max, and without knowing the current rating of the motor, seems very light to me.

     

    A TIP140 at 10A might be a simple substitution and it might require a slight adjustment to the R-3 3K base resistor.

     

    One thing I would suggest next repair is to try the motor with just the 36v and a variac to measure what currents you're seeing at the loads.

     

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to mcb1

    Hi Mark, You are right I should have taken the time to do a little more research on the characteristics of the motor. Victor wanted more info on the motor too. I will be more thorough next time. I too wondered at the unfiltered supply of the LM317. I decided to leave it alone as this was the design and it seemed to be working. I have learned that even my best intentions to make improvements always have side effects. I have to admit that I have created problems for my self enough times that I now always spend extra time considering side effects before I try something. Peter suggested I try a heavier Darlington so I found I had a TIP102 which is the same TO-220 case and has higher specs on the data sheet. I found that it worked well and so I sent the unit back to the dentist. Fortunately this unit is used in the Lab to work on dentures and prosthetics out of the mouth so the operation isn't critical.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to mcb1

    Totally agree,

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to jw0752

    I must be slipping, I did not even pick up on the fact there was no smoothing there

     

     

     

    Good catch, and yes that is not a good design

     

     

     

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • D_Hersey
    D_Hersey over 11 years ago

    The pwr on led needs a reversed signal diode in shunt.  LEDs have a reverse breakdown potential of about 6V.  When we parallel bipolars, as an earlier poster stated, we need ballast resistors to minimize current hogging due to the negative tempco of the Qs.

     

    Hanging an emitter follower  on the VR produces an output a diode drop below the regulator output.  As a prior poster noted your Q is operating in the linear mode, probably you should embiggen your heatsink.  When one does that (hangs a Q on a VR) he does increase the ampacity of the regulator.  But he loses the thermal shutdown feature.

     

    The http://www.ti.com.cn/cn/lit/ds/symlink/lm395.pdf LM195 is the transistor for you.  Even though it is bipolar, they can be paralleled freely as they have thermal feedback control on-board.

     

    You can do better than this.  I suggest you read a book or two on operational amplifiers and maybe one on SMPS design.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to D_Hersey

    Hi Don, Thanks for the information on the LM195. This looks like a very nice component to know about. As for the design of the circuit we are all in agreement that it is not a particularly good one. Not saying that I personally could have done better but at least in this case it can not be hung around my neck as it is a commercial product that I have been tasked with fixing. I took the circuit board and drew the schematic from it so that my friends here could better advise me. Button up your coat as some really cold weather is blowing by headed in your direction.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<