Test & Tools
  • Technologies
  • More
Test & Tools
Forum Feasability of Adding a Second Parallel Darlington?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 29 replies
  • Subscribers 388 subscribers
  • Views 6438 views
  • Users 0 members are here
  • control
  • voltage
  • darlington
Related

Feasability of Adding a Second Parallel Darlington?

jw0752
jw0752 over 11 years ago

        I am currently working on a small circuit that controls the voltage to an electric dental lab handpiece. Please see the schematic below. This circuit has had a chronic problem with failure of the TIP-122 Darlington. The problem arises when the handpiece operator applies pressure which adds load to the motor and the motor then demands more current from the circuit. This circuit is very simple with basically no overload protection. The original design did not even have a flyback diode across the motor. My question is if it is practical to add another TIP-122 Darlington in parallel with the first one in order to improve current handling capacity. Does anyone have any experience with this type of modification? I also have a curiosity codicil to my question. If it is practical to add another Darlington, what would be the limiting factor to how many parallel Darlingtons can be added in this way? Any insights would be appreciated.

John

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    Hi John, a very good question, and the answer is fairly straight forward If the Darlington is getting overloaded due to exceeding the current limit of the Darlington then an additional one in parallel…
  • vsluiter
    vsluiter over 11 years ago +1
    Hi John, You say that the circuit has no short circuit protection, but the 3k resistor with a hFE of 1000 means some current limit: The supply is 36×√2 -(1.2V diode bridge drop) ≅ 50V. At startup the motor…
Parents
  • vsluiter
    vsluiter over 11 years ago

    Hi John,

     

    You say that the circuit has no short circuit protection, but the 3k resistor with a hFE of 1000 means some current limit:

    The supply is 36×√2 -(1.2V diode bridge drop)  ≅ 50V.

    At startup the motor does not generate back-EMF, and the capacitor is empty, so you'll basically just have the 1 Ohm as load.

    I did a short calculation here (this will link to an editable version):

    image

    The combination of the 1 Ohm resistor and the darlington base resistor limit the current to somewhere around 10.95A. Of course this will heat up the darlington, but it is a current limit. If you will meddle with this circuit, this behaviour will also change. As you can see, changing the output voltage of the LM317 will also change the current limit. If you parallel, double each darlington's base resistor to keep the current limit.

     

    Now for parallelling: this will only work nicely if the darlingtons' conductance has a negative temperature coefficient: if they heat up, they should conduct less. In that way the load will balance evenly over the darlingtons. If the temperature coefficient for conductance is positive, one of them will heat up, conducting better, so getting more amps and heating up more, etcetera.

     

    Succes!

    edit: added the Rload of 1 Ohm in the calculation of the current limit

     

    Victor

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to vsluiter

    Hi Victor,

    Thank you for the well written analysis of the current limitations in my circuit. I am going to study it closely to help me learn from this situation. Your mention of the change in circuit characteristics when the Darlingtons have a positive or negative temperature coefficient reminds me of number series in mathematics and determining whether they converge or diverge. A positive coefficient will cause the two darlingtons to diverge triggered by small differences in their specs while a negative coefficient will keep them working together as either one that is taking more of the load will heat up and self regulate to a lower current level. One thing that has me concerned is that the rectified voltage 36V * 1.4 = 49.7V should be too high for the LM317. Is this possible because the adjust and output are not at 0V? I have already taken up too much of your time. It was good to hear from you again and thanks again for your insights.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to jw0752

    This may help in your understanding John

     

    http://en.wikipedia.org/wiki/Common_collector

     

    this is effectively what you have.

     

    overall the Darlington is providing a bypass boost to the voltage regulator in order to increase its output current capacity, and in fact take over that job entirely

     

    common collector transistors are almost self governing due to the negative feedback provided at the emitter from the load, anyway, have a read of the article and it will help your understanding

     

    in addition to this the series emitter resister de-generates the transistor when used in parallel circuits in order to mitigate the negative temperature co-efficient of the BJT. (FETS of course having positive Temp co do not suffer this problem)

     

    to quote this article http://www.allaboutcircuits.com/vol_3/chpt_4/12.html

     

    Common-collector amplifiers have much negative feedback, due to the placement of the load resistor between emitter and ground. This feedback accounts for the extremely stable voltage gain of the amplifier, as well as its immunity against thermal runaway

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to Robert Peter Oakes

    Hi Peter, Thanks for the followup. I have printed the article on Feedback and will read it tonight. I have also bookmarked the All About Circuits Web site as it looked like it had other good information for a person in learning mode, like me. I also see that I have another one of your Power Supply Tutorials to look forward to. It is great to be retired so I have enough time to look at all this great information.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to jw0752

    Yup, my videos seem to be too long for currently employed folks to watch and still have a life... image, im working on it lol

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • vsluiter
    vsluiter over 11 years ago in reply to jw0752

    Hi John,

     

    Today, driving the car, I found back the way to include the load correctly in the calculation of the output current. I updated the calculation above.

     

    John Wiltrout wrote:

     

    One thing that has me concerned is that the rectified voltage 36V * 1.4 = 49.7V should be too high for the LM317. Is this possible because the adjust and output are not at 0V?

    Probably it is saved by a slowly rising supply in combination with the voltage at the adjust terminal.

     

    important question:

    Do you know what the calibration procedure is? Is the output voltage tuned to a certain value, or is it tuned per load device?

     

    more important question:

    you have a problem with overload. Do you know what the requirements are for the load? Do you need a constant voltage, or a constant current limit or both? Without this, it's hard to know what the 'right' solution for your problem is. Adding a thermal fuse (polyfuse) might protect the darlington, but cut down the motor power too much.

    If you know what current / voltage limit you need, you could design for that purpose. Linear has some nice constant current / constant voltage solutions, actually meant for LEDs, but maybe also for this application.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to vsluiter

    The LM317 is good for 0 - 37V out according to https://www.fairchildsemi.com/datasheets/LM/LM317.pdf

    and it can have a Vin to Vout of up to 40V so as long as the output is never taken to less than about 10V on the LM317 it should be good

     

    regards

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to Robert Peter Oakes

    Peter your videos are well on the way to been the same length as Dave Jones's.

    I think that they could easily be split in to two although how you do it is a different matter.

    Either way as you know very well making the video is the easy bit all the prep and post work is the hard bit!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to Problemchild

    For sure, I start out intending to keep it to 30 mins or less, then start filming, then oops, 1 hr. elapsed and I’m only half way through… Yes that’s what I said, I already broke it into two image

     

     

     

    Second half is rendering as we speak, dealing with MOSFETs N and P channel and it too is an hour I’m afraid

     

     

     

    I guess a logical split would be 30Mins for NPN, 30 for PNP, 30 for N Channel… you get the idea

     

     

     

    Problem was there was no easy break in the middle to split it

     

     

     

    In future I will try to deliberately pretend there is an end every 20-30 mins and if I don’t want it I can always delete the ending statements and concatenate

     

     

     

    I just hope I don’t ramble on too much, I can sometimes get kinda carried away image and I’m always conscious of trimming too much and losing the less experienced viewers that may not get the concepts with the abridged versions so I ere on the side of longer

     

     

     

    I know this does not help the poor souls who have to sit and watch, but then that’s what pause and fast forward are for no image ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Problemchild
    Problemchild over 11 years ago in reply to Robert Peter Oakes

    problem with pause and fast forward is that you need to know where to fast forward. I may not be our target audience either in as far as I can remember at least some of my transistor theory and  watch your videos the way through when I start image

     

    The attention span for the average youtuber is less than 2 mins... to go much longer than that you need either boobs, explosions, lol cats, or BS .... preferably several of each in every video.

     

    That said I bet you generally get much better than that I would imagine since electrogeeks have already found you and are generally willing to watch.

     

    Even so 4 x 15 min videos may be better ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to Problemchild

    image, yup, your right, I just gotta get there , not as easy as it sounds

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 11 years ago in reply to vsluiter

    Hi Victor, This is a motor unit that the dentists use to trim and polish things like dentures outside the mouth. Each time they use it they pick a setting for VR-1 that they want and then they use the handpiece to grind away plastic or polish a surface. As they apply pressure the motor slows and demands more current due to less counter EMF. I have already repaired and sent the unit back or I would be able to measure DC resistance and operational current which I did not do when it was on my bench.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • jw0752
    jw0752 over 11 years ago in reply to vsluiter

    Hi Victor, This is a motor unit that the dentists use to trim and polish things like dentures outside the mouth. Each time they use it they pick a setting for VR-1 that they want and then they use the handpiece to grind away plastic or polish a surface. As they apply pressure the motor slows and demands more current due to less counter EMF. I have already repaired and sent the unit back or I would be able to measure DC resistance and operational current which I did not do when it was on my bench.

    John