Test & Tools
  • Technologies
  • More
Test & Tools
Forum Need help measuring 120VAC main
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 12 replies
  • Subscribers 389 subscribers
  • Views 3066 views
  • Users 0 members are here
Related

Need help measuring 120VAC main

totalhighspeed
totalhighspeed over 10 years ago

I built a circuit board to measure 120VAC using a Raspberry PI. I have a bridge rectifier and voltage divider. All using surface mount 1206 parts. Everything works well. When I put a voltmeter on the test point it shows 1/100th the line voltage in DC. However, when I actually look at it on a scope, I see that the ripple is 0 to 1.2v, essentially the full rectified voltage. The filter isn't doing hardly anything.

 

I'm trying to keep is all as small as possible so I'd like to stick with 1206 package for the filtering capacitors especially since the PCB has already been manufactured using these. I did use a through hole for the inductor it has 5mm lead spacing. Can someone recommend what capacitor and inductor values to use to get a cleaner DC(ish) voltage. The voltage divider is before the filtering so using low voltage capacitors are not a problem.

 

I was using 1000pF on C1 and 2200pF on C2 and 100mH for the Inductor. Below is the layout:

 

>-------- L1 ---------->

      |             |

     C1        C2

      |             |

>----------------------->

 

Any help would be GREATLY appreciated...

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 10 years ago in reply to totalhighspeed +3 verified
    First I must give you the quick lecture on mains safety: USE AN ISOLATING TRANSFORMER !!! If your circuit is connected to the mains supply it is not safe. Now to filtering some safe 60Hz AC to measure…
  • D_Hersey
    D_Hersey over 10 years ago +2
    Listen to the nice, smart and pretty folks on this thread and USE A T-FORMER!
Parents
  • peterjcs23
    0 peterjcs23 over 10 years ago

    You could step down the voltage with a transformer to make the voltage safe to handle on a PCB.

     

    77DB-06-09. IDEAL POWER, AC/AC Power Supply, UK, 240 V, 10 W, 9 VAC, 670 mA | Farnell element14

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • peterjcs23
    0 peterjcs23 over 10 years ago

    You could step down the voltage with a transformer to make the voltage safe to handle on a PCB.

     

    77DB-06-09. IDEAL POWER, AC/AC Power Supply, UK, 240 V, 10 W, 9 VAC, 670 mA | Farnell element14