Test & Tools
  • Technologies
  • More
Test & Tools
Forum Keithley 2000 and True RMS for square wave with offset 1V
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 0 replies
  • Subscribers 385 subscribers
  • Views 227 views
  • Users 0 members are here
Related

Keithley 2000 and True RMS for square wave with offset 1V

alex2
alex2 over 9 years ago

Salve,

avrei una domanda sul Keithley 2000:

con un generatore Agilent ho posto in ingresso un segnale di tensione onda quadra con Valore picco picco pari a 2 V,

e con OFFSET pari a 1, lo strumento mi restituisce un valore efficace di circa 1 V, cioè come se non ci fosse l'offset,

mentre per il segnale che ho messo dovrebbe darmi circa 1,4 V.

Come mai?

Dato che lo strumento è a vero valore efficace, non dovrebbe restituirmi il valore corretto?

Come posso risolvere

Grazie in anticipo per la risposta

Alex

 

Hi,
I have a question about Keithley 2000:

I have sent, by a signal generator Agilent, a voltage square wave to input of Keithley 2000,
with the next parameters:  Value peak to peak 2 V, i.e.  amplitude 1 V, and OFFSET 1 V.

The instrument gives me an RMS about 1 V, as if the OFFSET was not there;

indeed, the right RMS is about 1,4 V.

Why?

Since the tool is True RMS, should it give me back the correct value? Shouldn't?

How can I fix the problem?

Thanks for the answers.

Alex