Test & Tools
  • Technologies
  • More
Test & Tools
Forum TENMA  72-10510 Input Voltage
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 385 subscribers
  • Views 1091 views
  • Users 0 members are here
Related

TENMA  72-10510 Input Voltage

tobben24
tobben24 over 10 years ago

Hi,

 

Does anyone know what input voltage TENMA  72-1051072-10510 can handle Cannot seem to find that info on farnell or on google

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 10 years ago +1 verified
    It says in the spec that it can handle 20V per division "Dual analog channels width range 1mV/div ~ 20V/div" Typically you get 8 divisions so I guess it's +/- 80V, with x10 probes it will be more, but…
  • baldengineer
    baldengineer over 6 years ago +1 suggested
    Are you looking for the maximum voltage you can measure? Or the maximum voltage the oscilloscope can tolerate before there is damage? For the maximum measurable voltage, looking at the max volts/div is…
Parents
  • baldengineer
    0 baldengineer over 6 years ago

    Are you looking for the maximum voltage you can measure? Or the maximum voltage the oscilloscope can tolerate before there is damage? For the maximum measurable voltage, looking at the max volts/div is the most appropriate method.

     

    For maximum ratings of the scope input and probe, both are available in the manual/datasheet.

     

    Max Scope Input: PDF page 51. It can tolerate up to 400 Volts-peak.

     

    Max Probe Input: PDF page 61, shows that in the x1 setting max input voltage is 150 V and in the x10 setting it is 300 V.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • baldengineer
    0 baldengineer over 6 years ago

    Are you looking for the maximum voltage you can measure? Or the maximum voltage the oscilloscope can tolerate before there is damage? For the maximum measurable voltage, looking at the max volts/div is the most appropriate method.

     

    For maximum ratings of the scope input and probe, both are available in the manual/datasheet.

     

    Max Scope Input: PDF page 51. It can tolerate up to 400 Volts-peak.

     

    Max Probe Input: PDF page 61, shows that in the x1 setting max input voltage is 150 V and in the x10 setting it is 300 V.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer