Test & Tools
  • Technologies
  • More
Test & Tools
Forum Oscilloscope vertical position
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Answers 4 answers
  • Subscribers 389 subscribers
  • Views 2781 views
  • Users 0 members are here
Related

Oscilloscope vertical position

krik
krik over 9 years ago

Bought my first oscilloscope a couple weeks ago, a Rigol DS1054 Z. And with some help from videos and blogs I am learning how to use it. While I have other things I plan to use it for, the reason that triggered buying it was to measure flicker in florescent and LED lighting. The reason I am testing them is that my niece suffers from seizures and after some reading I had to wonder if florescent or LED lights maybe contributing to the problem. Originally I thought just get some LED's that run on DC and the problem would be solved. It's not that easy, the 2 kinds I bought both flicker at 120 Hz, they are actually worse than florescent bulbs they were to replace. And after thinking about it, the LED's can be built without a good capacitor, so they may flicker. So basically now I am testing several different bulbs, fixtures and drivers.

 

So the issue is that the LED lights I am testing run between 12 and 36 volts, but to get the signal on my screen I am finding I have to spend several minutes turning the vertical position knob. I did eventually find that pressing the "Auto" button will put the signal in the middle of the screen, but it may set the vertical scale to 10mv, for example, so if I want to see it at 20mv I am back to spending a fair amount of time with the vertical position knob. In all the videos I watched it seemed to me that once they hooked up the test lead the signal was on their screen. Maybe that is the magic of editing but I doubt it as some do not cut way. So I am guessing either there is a setting I messed up at some point or there is another way that no one ever mentions when they are creating videos. So how do I get the oscilloscope to always keep the signal on the screen? Especially when I change the scale, but it would also be nice if it would also just automatically start out on the screen.

 

PS I hope this question is in the right place. These forums are very complicated to figure out. I have never seen forums setup like this.

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 9 years ago +4
    A simple fact to bear in mind LEDs are not AC or DC. They are ALWAYS DC and are current devices. So even if your powering one from an AC supply, it will be rectified (All or partially) and current will…
  • michaelwylie
    michaelwylie over 9 years ago +2 suggested
    Not sure if I'm reading the problem correctly but it sounds like you're trying to observe an AC waveform on top of the DC signal. If this is the case simply set the coupling on that channel to AC.
  • jw0752
    jw0752 over 9 years ago in reply to krik +1 verified
    Hi Shane, I suspect that you want to look at the ripple. this is the inconsistency of the DC voltage. To do this you have to do what Michael told you and switch to the AC coupling. This causes the scope…
Parents
  • volly
    0 volly over 9 years ago

    krik,

     

    Have a look at this:

    https://learn.sparkfun.com/tutorials/how-to-use-an-oscilloscope

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • volly
    0 volly over 9 years ago

    krik,

     

    Have a look at this:

    https://learn.sparkfun.com/tutorials/how-to-use-an-oscilloscope

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • krik
    0 krik over 9 years ago in reply to volly

    I think I have read that before but just in case I scanned over it again. In particular I reread the "Vertical System" section, I didn't see anything that would help. Is there a particular part of that article I should be looking at?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer