Test & Tools
  • Technologies
  • More
Test & Tools
Forum Soldering Stations & The Right Accessories - Where to start?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 54 replies
  • Answers 34 answers
  • Subscribers 394 subscribers
  • Views 8748 views
  • Users 0 members are here
  • weller
  • solder tips
  • soldering_tip_life
  • commfeedback
  • weller_soldering_irons
Related

Soldering Stations & The Right Accessories - Where to start?

tbartonnewark
tbartonnewark over 8 years ago

Hi I work at Newark and I'm researching kitting soldering stations and replacement soldering tips together Assuming I start with a Basic Weller 120V 50W Station(WES51 or  WESD51WESD51 What tips sizes or shapes would you recommend for an entry level kit Any thoughts on tinners and sponges to extend tip life What would be the dream starter pack

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago in reply to mcb1 +11 suggested
    Hi Mark, I actually cheated too and I also found this small ceramic thingy at the $ store. It is supposed to be used to heat aromatic oil like a scented candle but I retasked it. I have glued it to a hockey…
  • jw0752
    jw0752 over 8 years ago +10 suggested
    Hi Tom, The recommendations that have been tendered so far are all great. I have always bought a variety of tips when I bought a system but as dougw points out they almost never get used and the tip he…
  • dougw
    dougw over 8 years ago +7 suggested
    I do all my soldering with the same size tip - it is not practical to swap hot tips all the time. But extra tips of the same type are always useful. The tip should be fairly short and fairly fine to get…
Parents
  • dougw
    0 dougw over 8 years ago

    I do all my soldering with the same size tip - it is not practical to swap hot tips all the time. But extra tips of the same type are always useful. The tip should be fairly short and fairly fine to get the maximum heat to the smallest area.

    I use a wet sponge for tip cleaning - I don't know if it extends life better, but it cleans better, providing better performance. So a tip cleaner tray for the sponge is essential. A couple of extra sponges would be useful. I also keep a bottle of (preferably DI) water nearby to keep the sponge wet. Like a sports water bottle - so the water can't evaporate between sessions.

    Other useful accessories are:

    • a solder dispenser (stand with an axle for the solder reel)
    • a magnifier (ideally a stereo microscope) (even jewelers glasses can work)
    • some lights
    • a PCB holder
    • tweezers
    • solder wick
    • solder sucker
    • flux syringe
    • small nozzle hot air gun
    • a fume extractor/filter
    • a third hand
    • extra solder (two different diameters are useful)

    You can find low-cost starter versions of all of these except maybe the fume extractor.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • tbartonnewark
    0 tbartonnewark over 8 years ago in reply to dougw

    Thanks Doug

     

    From the comments it seems like the accessories are more valuable as a starter kit than the tips.  Good advice.

     

    TB

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • tbartonnewark
    0 tbartonnewark over 8 years ago in reply to dougw

    Thanks Doug

     

    From the comments it seems like the accessories are more valuable as a starter kit than the tips.  Good advice.

     

    TB

    • Cancel
    • Vote Up +4 Vote Down