Test & Tools
  • Technologies
  • More
Test & Tools
Forum Soldering Stations & The Right Accessories - Where to start?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 54 replies
  • Answers 34 answers
  • Subscribers 394 subscribers
  • Views 8508 views
  • Users 0 members are here
  • weller
  • solder tips
  • soldering_tip_life
  • commfeedback
  • weller_soldering_irons
Related

Soldering Stations & The Right Accessories - Where to start?

tbartonnewark
tbartonnewark over 8 years ago

Hi I work at Newark and I'm researching kitting soldering stations and replacement soldering tips together Assuming I start with a Basic Weller 120V 50W Station(WES51 or  WESD51WESD51 What tips sizes or shapes would you recommend for an entry level kit Any thoughts on tinners and sponges to extend tip life What would be the dream starter pack

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago in reply to mcb1 +11 suggested
    Hi Mark, I actually cheated too and I also found this small ceramic thingy at the $ store. It is supposed to be used to heat aromatic oil like a scented candle but I retasked it. I have glued it to a hockey…
  • jw0752
    jw0752 over 8 years ago +10 suggested
    Hi Tom, The recommendations that have been tendered so far are all great. I have always bought a variety of tips when I bought a system but as dougw points out they almost never get used and the tip he…
  • dougw
    dougw over 8 years ago +7 suggested
    I do all my soldering with the same size tip - it is not practical to swap hot tips all the time. But extra tips of the same type are always useful. The tip should be fairly short and fairly fine to get…
Parents
  • jadew
    0 jadew over 8 years ago

    I find myself using a 1.2 mm chisel tip most of the time, since it works great on both SMD and through-hole. The next tip I use is a bevel tip, for drag soldering.

     

    The dream pack for me would also include a pair of hot tweezers or a second soldering station. I have a second station, and when I'm not picking up SMD parts, I can have it equipped with a different tip.

     

    Edit: I also use a 100 W soldering gun for wires and other things with a higher thermal mass. I'd go for a higher power gun if I were to buy it again.

     

    Razvan

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • mcb1
    0 mcb1 over 8 years ago in reply to jadew

    Edit: I also use a 100 W soldering gun for wires and other things with a higher thermal mass. I'd go for a higher power gun if I were to buy it again.

     

    I'm curious if your iron is temperature controlled.

     

    While there is no substitue for power, the ability to keep the temperature close to the desired value means you aren't cooking the solder and then experiencing a drop when it gets loaded.

     

     

    Mark

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • mcb1
    0 mcb1 over 8 years ago in reply to jadew

    Edit: I also use a 100 W soldering gun for wires and other things with a higher thermal mass. I'd go for a higher power gun if I were to buy it again.

     

    I'm curious if your iron is temperature controlled.

     

    While there is no substitue for power, the ability to keep the temperature close to the desired value means you aren't cooking the solder and then experiencing a drop when it gets loaded.

     

     

    Mark

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • jadew
    0 jadew over 8 years ago in reply to mcb1

    mcb1, the two stations I have are temperature controlled, but the soldering gun isn't.