Test & Tools
  • Technologies
  • More
Test & Tools
Forum Soldering Stations & The Right Accessories - Where to start?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 54 replies
  • Answers 34 answers
  • Subscribers 394 subscribers
  • Views 8566 views
  • Users 0 members are here
  • weller
  • solder tips
  • soldering_tip_life
  • commfeedback
  • weller_soldering_irons
Related

Soldering Stations & The Right Accessories - Where to start?

tbartonnewark
tbartonnewark over 8 years ago

Hi I work at Newark and I'm researching kitting soldering stations and replacement soldering tips together Assuming I start with a Basic Weller 120V 50W Station(WES51 or  WESD51WESD51 What tips sizes or shapes would you recommend for an entry level kit Any thoughts on tinners and sponges to extend tip life What would be the dream starter pack

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago in reply to mcb1 +11 suggested
    Hi Mark, I actually cheated too and I also found this small ceramic thingy at the $ store. It is supposed to be used to heat aromatic oil like a scented candle but I retasked it. I have glued it to a hockey…
  • jw0752
    jw0752 over 8 years ago +10 suggested
    Hi Tom, The recommendations that have been tendered so far are all great. I have always bought a variety of tips when I bought a system but as dougw points out they almost never get used and the tip he…
  • dougw
    dougw over 8 years ago +7 suggested
    I do all my soldering with the same size tip - it is not practical to swap hot tips all the time. But extra tips of the same type are always useful. The tip should be fairly short and fairly fine to get…
Parents
  • ninjatrent
    0 ninjatrent over 8 years ago

    This conversation sounds like a good reason for an experiment to determine which is ideal for proper soldering tip matainance, sponge or brass wool as method of cleaning solder tip.

     

    I currently use a cheap wet sponge pad but have found the brass wool to be very effective when used in the past.

     

    A wet sponge works great but the sudden temp changes do not seem like it would be beneficial to the lifespan of the tip, heating element, and any temp sensor the soldering iron might have.

     

    The concern with a brass tip cleaner might be some damage to the surface of the soldering tip with extended use.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rachaelp
    0 rachaelp over 8 years ago in reply to ninjatrent

    ninjatrent  wrote:

     

    This conversation sounds like a good reason for an experiment to determine which is ideal for proper soldering tip matainance, sponge or brass wool as method of cleaning solder tip.

    That experiment could take a long time to complete, it's the sort of thing I expect the big soldering station manufacturers may have done but it would be interesting to see this done or maybe try and collect data from a number of people over time and see if there are any trends in how the iron tips last vs how people look after their iron tips.

     

    In my experience I have had soldering iron tips have what appears to be an outer coating delaminate after extended use when using a wet sponge but I have never seen this on tips since using the brass cleaner. I'm particular about keeping my tips clean and re-tinning them after cleaning so they don't get any oxidisation and I do this regardless of the cleaning method. I don't have enough data to draw any concrete conclusions about tip life vs cleaning method as the tips I had issues with were from a different soldering station brand than I now use so maybe that's a factor in longevity too.

     

    Best Regards,


    Rachael

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 8 years ago in reply to rachaelp

    Since this thread got going I've happened to buy some new bits and a second Ersa iCon Pico iron and controller. It came with the brass brillo pad bat but I'm not finding it that good. This may be because I've been using a camera microscope to solder under for the first time and can now really see what I'm doing. I've found that a piece of kitchen paper does pretty well for cleaning the needle like tip I've been using. You need to be careful not to burn your fingers, and I've no idea how long the bit will last - but actually I don't care very much - the parts I'm soldering cost way, way more than the bits do.

     

    MK

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 8 years ago in reply to michaelkellett

    I second the microscope for soldering. I solder with a stereo microscope and it really helps with precision and seeing all the crud and dodgy joints.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 8 years ago in reply to dougw

    I've used a stereo optical microscope for years but I find it lees than ideal because:

     

    the field of view is too small

    I have to take my glasses off to look through it, but I need them on to see other things so going from microscope to BOM or parts bins is slow or blurred

    the posture you end up with hunched over the microscope is OK for an hour but not so good for a 2 day stint

     

    So I looked around and got a Mantis Elite in on loan (see Dave Jones review, he loved it) But I hated it - £3k+ but the posture problem is still there, the dealer said I could put the work on a stand but I'd end up working with my hands at chest level like a hamster.

    Next I looked at camera based systems, Vision Engineering do one, and there are two Swedish companies, but all at the £2k - £5k level.

    My son suggested a decent camera - you can get a MFT camera which will do 4k video for about £500 an a decent lens will be about another £400. But as a trial and stopgap I bought a Chinese job from Ebay for £180 (could probably have got it cheaper if I had looked around). Its really pretty good in absolute terms and very good for the money. It's much nicer to work with than peering into the stereo microscope, well worth the loss of stereo-ness. I thought it might be hard to get used to not looking at where my hand are but it's not been a problem.

     

    image

     

    The fancy camera project is in hand but I haven't got the bits for the long reach stand yet - so far it's only managed pictures of the dog.

     

    MK

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • dougw
    0 dougw over 8 years ago in reply to michaelkellett

    Very nice set up. I was also worried about the problem of looking away from my hands - even with a stereo microscope it takes a little getting used to. It is nice to know that it isn't too bad. Also nice to know that a decent rig isn't too expensive.

    I don't need glasses for anything closer than 8 feet so I don't have that problem. Everyone over 40 needs vision correction, but it is really nice to have your eyes end up with at least one useful distance range without correction.

    I use a custom vice/card holder which puts the cards a few inches off the bench and use movable hand rests to achieve maximum precision and minimum fatigue. My stereo scope has me sitting up pretty straight but I still wouldn't enjoy it hours on end.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • dougw
    0 dougw over 8 years ago in reply to michaelkellett

    Very nice set up. I was also worried about the problem of looking away from my hands - even with a stereo microscope it takes a little getting used to. It is nice to know that it isn't too bad. Also nice to know that a decent rig isn't too expensive.

    I don't need glasses for anything closer than 8 feet so I don't have that problem. Everyone over 40 needs vision correction, but it is really nice to have your eyes end up with at least one useful distance range without correction.

    I use a custom vice/card holder which puts the cards a few inches off the bench and use movable hand rests to achieve maximum precision and minimum fatigue. My stereo scope has me sitting up pretty straight but I still wouldn't enjoy it hours on end.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer