Test & Tools
  • Technologies
  • More
Test & Tools
Forum Soldering Stations & The Right Accessories - Where to start?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 54 replies
  • Answers 34 answers
  • Subscribers 374 subscribers
  • Views 7204 views
  • Users 0 members are here
  • weller
  • solder tips
  • soldering_tip_life
  • commfeedback
  • weller_soldering_irons
Related

Soldering Stations & The Right Accessories - Where to start?

tbartonnewark
tbartonnewark over 8 years ago

Hi I work at Newark and I'm researching kitting soldering stations and replacement soldering tips together Assuming I start with a Basic Weller 120V 50W Station(WES51 or  WESD51WESD51 What tips sizes or shapes would you recommend for an entry level kit Any thoughts on tinners and sponges to extend tip life What would be the dream starter pack

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago in reply to mcb1 +11 suggested
    Hi Mark, I actually cheated too and I also found this small ceramic thingy at the $ store. It is supposed to be used to heat aromatic oil like a scented candle but I retasked it. I have glued it to a hockey…
  • jw0752
    jw0752 over 8 years ago +10 suggested
    Hi Tom, The recommendations that have been tendered so far are all great. I have always bought a variety of tips when I bought a system but as dougw points out they almost never get used and the tip he…
  • dougw
    dougw over 8 years ago +7 suggested
    I do all my soldering with the same size tip - it is not practical to swap hot tips all the time. But extra tips of the same type are always useful. The tip should be fairly short and fairly fine to get…
Parents
  • gam3t3ch
    0 gam3t3ch over 8 years ago

    Well I like soldering rework stations myself but to be honest if I was going to buy another just soldering station Weller would be off the table I would probably check the TENMA  21-1011521-10115 But this is just my preference As far as tips go I think I use between.03.07 inch on a regular basis The only thing I would suggest that could be added would be a heating element if the part is there Just had mine go on my soldering iron but I had a spare waiting To me the WES51 and  WESD51WESD51 are great units but I think more information on who you are gearing these kits too would be ideal as well

     

    But to be fair the best would be the cheapest kit possible and then go from there as far as the addons.  I only say that because realistically if I could buy a soldering iron, hot air station, fume extractor, solder, bulb, flux, tweezers, wire cutter, extra tips and elements, hot plate, and ultimately a deslodering iron in a kit just starting out that didn't suck it would be more worth my while.

     

    But to me the  WR5000MWR5000M is my ultimate which isn't going to happen but would be killer to have

     

    Everything comes back to who you are going to be gearing this towards tho.   So maybe a bit more info.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • gam3t3ch
    0 gam3t3ch over 8 years ago

    Well I like soldering rework stations myself but to be honest if I was going to buy another just soldering station Weller would be off the table I would probably check the TENMA  21-1011521-10115 But this is just my preference As far as tips go I think I use between.03.07 inch on a regular basis The only thing I would suggest that could be added would be a heating element if the part is there Just had mine go on my soldering iron but I had a spare waiting To me the WES51 and  WESD51WESD51 are great units but I think more information on who you are gearing these kits too would be ideal as well

     

    But to be fair the best would be the cheapest kit possible and then go from there as far as the addons.  I only say that because realistically if I could buy a soldering iron, hot air station, fume extractor, solder, bulb, flux, tweezers, wire cutter, extra tips and elements, hot plate, and ultimately a deslodering iron in a kit just starting out that didn't suck it would be more worth my while.

     

    But to me the  WR5000MWR5000M is my ultimate which isn't going to happen but would be killer to have

     

    Everything comes back to who you are going to be gearing this towards tho.   So maybe a bit more info.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer