Test & Tools
  • Technologies
  • More
Test & Tools
Forum Torque Screwdrivers - What do you use?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 7 replies
  • Answers 5 answers
  • Subscribers 389 subscribers
  • Views 5269 views
  • Users 0 members are here
  • torque_tools
  • screwdrivers
  • tools
Related

Torque Screwdrivers - What do you use?

tbartonnewark
tbartonnewark over 8 years ago

Hi

 

I work at Newark and I'm reviewing Torque Screwdrivers.  Do you use them?  If so what increment range is common and are you using metric or imperial.

 

My background is in rough electrical work, but I'm interested in how the torque screwdrivers are used by engineers or if they are used in PCB assembly.

 

Thanks

 

TB

  • Sign in to reply
  • Cancel

Top Replies

  • rsc
    rsc over 8 years ago +4 suggested
    Hi Tom, When I worked for Bosch we used many types of torque drivers from a few g-mm to several hundred Nm. To get the best control of clamping force, you need a device that also measures rotation angle…
  • abrain
    abrain over 8 years ago +2 suggested
    Hi Tom, I’ve recently been using one of these Wera Wera torque screwdrivers, which goes up to 3Nm and was ideal for the M3 screws used to hold some enclosures together. Personally it’s rare I use them…
Parents
  • abrain
    0 abrain over 8 years ago

    Hi Tom, I’ve recently been using one of these WeraWera torque screwdrivers, which goes up to 3Nm and was ideal for the M3 screws used to hold some enclosures together.

     

    Personally it’s rare I use them, as usually I subcontract final assembly, this was a case of needing to do some field upgrades and ensure the units weren’t going to shake apart afterwards!

     

    This 3Nm range seemed ideal for screws up to M3, for fitting these enclosure onto other equipment or mountings I’d probably look to a torque wrench instead for the M4 or M5 fasteners that usually get used in the industries I deal with.

     

    You can see I’m pretty much metric, for the fasteners, but appreciate the options a 1/4” drive brings!

     

    Hope that helps!

     

    A

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • abrain
    0 abrain over 8 years ago

    Hi Tom, I’ve recently been using one of these WeraWera torque screwdrivers, which goes up to 3Nm and was ideal for the M3 screws used to hold some enclosures together.

     

    Personally it’s rare I use them, as usually I subcontract final assembly, this was a case of needing to do some field upgrades and ensure the units weren’t going to shake apart afterwards!

     

    This 3Nm range seemed ideal for screws up to M3, for fitting these enclosure onto other equipment or mountings I’d probably look to a torque wrench instead for the M4 or M5 fasteners that usually get used in the industries I deal with.

     

    You can see I’m pretty much metric, for the fasteners, but appreciate the options a 1/4” drive brings!

     

    Hope that helps!

     

    A

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer