Test & Tools
  • Technologies
  • More
Test & Tools
Forum measure the distance between existing connectors
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 5 replies
  • Answers 2 answers
  • Subscribers 387 subscribers
  • Views 1155 views
  • Users 0 members are here
Related

measure the distance between existing connectors

houandreas
houandreas over 8 years ago

Hi, I'm now designing an adapter board for my system. There are two 2x20 female headers on the board, so I need two 2x20 male headers on my adapter board. For the final layout it's important to measure the distance of these connectors precisely. But is there a precise way to measure the distance of these two headers? Has anyone any experience for such measurement?

  • Sign in to reply
  • Cancel

Top Replies

  • jw0752
    jw0752 over 8 years ago +5 suggested
    Hi Bin, If I was making these measurements I would use a caliper to make the measurements on the existing board and I would use a drawing program like Corel to draw the second board. These drawing programs…
  • genebren
    genebren over 8 years ago +4 verified
    For a precise way to measure the distance between the two female headers, you should be using a precise measurement tool. For this I would recommend calipers. I would the measure the distance, using the…
  • mcb1
    mcb1 over 8 years ago in reply to jw0752 +3 suggested
    Good suggestions. If you want to measure the centre to centre distance of a hole, pins, etc, then measure the distance between the closest side of the closest hole/pin/etc to the closest side of the furtherest…
Parents
  • genebren
    0 genebren over 8 years ago

    For a precise way to measure the distance between the two female headers, you should be using a precise measurement tool.  For this I would recommend calipers. I would the measure the distance, using the outside (large) jaws of the outer most edges of the two female headers.  I would the measure the width of one of the female headers and subtract that from the first measurement.  The resulting value is the distance between the centerlines of the two headers.  This measurement could be off a bit if the two headers are tilted or soldered in crooked, but it should be very close.

     

    Good luck,

    Gene

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • houandreas
    0 houandreas over 8 years ago in reply to genebren

    thx !!!image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • houandreas
    0 houandreas over 8 years ago in reply to genebren

    thx !!!image