Test & Tools
  • Technologies
  • More
Test & Tools
Forum Newbie help diagnosing a Stereo system
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 9 replies
  • Answers 7 answers
  • Subscribers 388 subscribers
  • Views 1557 views
  • Users 0 members are here
  • stereo system power issues
Related

Newbie help diagnosing a Stereo system

napthyme
napthyme over 8 years ago

Hi, I have not done any of this since HS 25+ years ago, so I am a bit lost because the system is acting strange.

 

I have a cariole compact stereo system from the 70's recently it started having power issues. It did not always have power to the stereo part when I pushed the power button, yet the clock which is always on is still working. Now it rarely has power when pressing the power button. It has been dead for the last several months and today again I heard popping sounds coming from the speakers with the power button in the off position and found it again had power. I put on a record and played the first side, the middle of the second side the power died and its dead as a doorknob again save for the clock which is still on.

 

So I know it can't just be a fuse. It can't be a total power supply failure because the clock is still working. If it was a bad tube I would think it would be totally dead by now same with a bad large capacitor in the power supply. The power switch was on when it lost power, so I would assume its not the switch. The selector switch was functioning when it had power so I assume it was not that.

 

So where do I start in trying to diagnose this system to find out where the issue is to fix it as it works fine when it has power in the system,.

 

Thanks in advance.... Jimimage

  • Sign in to reply
  • Cancel

Top Replies

  • DAB
    DAB over 8 years ago +3 suggested
    In a system that old, you probably have some bad capacitors in the power train along with corroded contacts on switches and connectors. Time to get out a voltmeter and oscilloscope to start tracking the…
  • jw0752
    jw0752 over 8 years ago +2 suggested
    Hi James, I am very suspicious of the switch itself. These switches do wear out and certainly over twenty five years the contacts will tarnish. Once they start to arc it is the beginning of the end as…
  • jw0752
    jw0752 over 8 years ago in reply to napthyme +2 suggested
    Hi James, Sorry I can't guess more at this time. You will have to get out the tool box and crack it open and see what the situation is with the switch. By the way the link at the end of your post doesn…
Parents
  • rusgray
    0 rusgray over 8 years ago

    You say that the system "rarely" has power after actuating the power switch, but you don't quantify how often it gets power. Odds are that the drive units in your speakers have a sensitivity of at least 80dB, which means that audible pops indicate a nontrivial amount of signal present at the amplifier outputs.

    Open the enclosure, connect the system to power through a GFCI outlet/plug, and start looking at the operation of the power supply. The potential culprits for non-deterministic operation are too numerous to list, but if you follow standard troubleshooting practices, you should be able to track the issue down quickly. If you want a quick sanity check to reassure yourself, disconnect the onboard PSU and power the electronics with a bench supply to confirm proper operation of the rest of the system (difficult loads can cause problems for some types of PSUs; this check allows you to confirm that the problem is within the PSU section.)




    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • rusgray
    0 rusgray over 8 years ago

    You say that the system "rarely" has power after actuating the power switch, but you don't quantify how often it gets power. Odds are that the drive units in your speakers have a sensitivity of at least 80dB, which means that audible pops indicate a nontrivial amount of signal present at the amplifier outputs.

    Open the enclosure, connect the system to power through a GFCI outlet/plug, and start looking at the operation of the power supply. The potential culprits for non-deterministic operation are too numerous to list, but if you follow standard troubleshooting practices, you should be able to track the issue down quickly. If you want a quick sanity check to reassure yourself, disconnect the onboard PSU and power the electronics with a bench supply to confirm proper operation of the rest of the system (difficult loads can cause problems for some types of PSUs; this check allows you to confirm that the problem is within the PSU section.)




    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer