Test & Tools
  • Technologies
  • More
Test & Tools
Forum Insulation Tester Component Identification
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 2 replies
  • Subscribers 385 subscribers
  • Views 1128 views
  • Users 0 members are here
  • mosfet
  • component identification
  • switching transistor
  • chauvin arnoux
  • ca6526
  • insulation tester
Related

Insulation Tester Component Identification

three-phase
three-phase over 6 years ago

Hello All,

 

I have a component in the CA6526 insulation tester that I am trying to identify. It looks like it is switching the HV transformer, but it is a 4 legged device that I am not used to. Generally I see an IGBT or MOSFET performing this function. Three of the pins are shorted together, so it could be that it still is a type of switching transistor, but all the searches I have done, have drawn a blank at the moment.

 

The text on the component is;

 

39100

PEm

1722 D4

4205

 

This is the actual component

 

image

 

This is where the component sits on the PCB;

 

image

 

A different angle with the focus on the other components;

 

image

 

Could anybody assist with identification of the component and then hopefully I can find a data sheet?

 

Kind regards

  • Sign in to reply
  • Cancel

Top Replies

  • genebren
    genebren over 6 years ago +4 verified
    Donald, It is always difficult to lookup a part based on the markings on the package. First looking at the package and PCB traces, this looks like a MOSFET device. Using the markings, I found a close match…
  • three-phase
    three-phase over 6 years ago in reply to genebren +2
    Many thanks Gene, Awesome piece of detective work. Googling the PSMN039-100 part number does bring up pictures of a device with very similar markings to the one on the board. The device ratings seem similar…
  • genebren
    0 genebren over 6 years ago

    Donald,

     

    It is always difficult to lookup a part based on the markings on the package.  First looking at the package and PCB traces, this looks like a MOSFET device.  Using the markings, I found a close match that might make sense.(https://assets.nexperia.com/documents/data-sheet/PSMN039-100YS.pdf ).  No guarantees, but this might be close.

     

    Gene

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • three-phase
    0 three-phase over 6 years ago in reply to genebren

    Many thanks Gene,

     

    Awesome piece of detective work. Googling the PSMN039-100 part number does bring up pictures of a device with very similar markings to the one on the board. The device ratings seem similar to other MOSFETs I have seen in these circuits and the pin configuration seems to match the circuit as well.

     

    It is the best option I have at the moment.

     

    Kind regards.