Test & Tools
  • Technologies
  • More
Test & Tools
Forum DIY Lab PSU (or bench power supply): what to choose?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 5 replies
  • Answers 5 answers
  • Subscribers 386 subscribers
  • Views 4359 views
  • Users 0 members are here
  • diy
  • power supplies
Related

DIY Lab PSU (or bench power supply): what to choose?

s1m0n3t
s1m0n3t over 6 years ago

I apologize if I will write a lot, I invite you to read only if you have a lot of free time... image

 

For some time now I have needed a versatile bench power supply, which would be useful for several general tests. I understand that the word "general" in electronics does not mean anything, because an instrument suitable for any situation is only a utopia, but from my experience I can say that it has hardly happened to me that I need voltages higher than 24V and currents higher than 3A, for small applications.

I would therefore like to build a power supply with two separate channels (possibly usable in series or in parallel), for example with maximum 2x15V.

I would like to have a very stable power supply with very low noise, so I would like it to be linear, not switching.

 

I have available (in addition to a nice metal case with "generous" dimensions) a 2x12V 6.25A (150VA) toroidal transformer. These two outputs, after being rectified, should give me 12 x 1.41 = 16.92V. After subtracting a dropout voltage, typically 1.5V, I should get my 15V per channel.

I also have two LT1083 linear regulators, which hold up to 7.5A continuous. They are very beautiful and have a TO-3P package easily mountable on a heatsink. But unfortunately it is an obsolete model, not replaced by any equivalent, so I would prefer not to use them, to make a future replacement easy, should one break.

I have found many solutions with linear regulators and a current of many amps, both with many regulators (like LM317 and equivalent) in parallel, and with bridge-connected mosfets.

 

Then I would have to make other choices:

1) Start from 1.2V of minimum voltage or adopt a more complex circuit to start from 0V

2) Adjust only the voltage or also the current (not of primary importance to me)

3) Use a simple analogue control with multiturn precision potentiometers and display to measure voltages and currents, or insert a microcontroller to control the settings with PWM, with a digital interface (in the future possibly also controlled by software)

 

But the crucial point is another: the maximum current and its dissipation.

If I want each channel to go from 0 to 15V, for low voltages I would have a maximum dropout of about 15V, which at 6A would require a dissipation of 90W !!!

Normally I would not reach this condition, because when could I ever need a 1V to 6A output? For example, it would be more likely to use 12V at 6A ((17-12) * 6 = 30W of dissipation). But I should still be in the worst conditions and I think that dissipating 90W of heat is really too much for a bench power supply, even with forced ventilation.

What do you think? What would you do for me? Settle for a much lower maximum current, not taking full advantage of my toroid? Make sure to limit the current as a function of the voltage, with a digital control, so as to keep the total dissipation below a set threshold?

After all, a good compromise could be having a precise linear variable power supply, with a low current, and a second switching power supply in case I need a higher current.

But even if I limit myself to 3A per channel, dissipating 45W of heat may not be that simple.

 

Any advice and opinions will be welcome...thank you in advice! image

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 6 years ago +5 suggested
    Hi Simone, I feel for your desired voltage range, a good achievable aim for a linear PSU is 1A per channel. Once you've got that built you'll have something always usable, and can consider a higher-current…
  • dougw
    dougw over 6 years ago +5 suggested
    As you mention, you will likely need to keep the current to limits implied by practical heat dissipation methods. You could apply any excess current capacity to extra channels. For example some standard…
  • jeff_electron
    jeff_electron over 6 years ago +2 suggested
    Hmm tricky, the real problem is to get the best potential out of your toroid. power dissipation can normally be greatly reduced by putting a variable switcher behind the linear regulator allowing for a…
Parents
  • shabaz
    0 shabaz over 6 years ago

    Hi Simone,

     

    I feel for your desired voltage range, a good achievable aim for a linear PSU is 1A per channel. Once you've got that built you'll have something always usable, and can consider a higher-current supply later.

    I have higher current power supplies, but I still use my home-made dual 0-15V linear supply which barely achieves 1A.

    The transformer is too large however. I think it's better to buy an approx 50VA transformer, with 0-15V windings for slightly more headroom in case that is needed.

    Personally I'd use decent potentiometers from Farnell/Newark, and an off-the-shelf low-cost digital panel meter (e.g. from aliexpress).

    There's some nice examples of home-made power supplies if you examine jw0752 blog posts.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 6 years ago

    Hi Simone,

     

    I feel for your desired voltage range, a good achievable aim for a linear PSU is 1A per channel. Once you've got that built you'll have something always usable, and can consider a higher-current supply later.

    I have higher current power supplies, but I still use my home-made dual 0-15V linear supply which barely achieves 1A.

    The transformer is too large however. I think it's better to buy an approx 50VA transformer, with 0-15V windings for slightly more headroom in case that is needed.

    Personally I'd use decent potentiometers from Farnell/Newark, and an off-the-shelf low-cost digital panel meter (e.g. from aliexpress).

    There's some nice examples of home-made power supplies if you examine jw0752 blog posts.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer