Test & Tools
  • Technologies
  • More
Test & Tools
Forum Anyone familiar with the Hantek 1008?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 3 replies
  • Answers 1 answer
  • Subscribers 386 subscribers
  • Views 8715 views
  • Users 0 members are here
Related

Anyone familiar with the Hantek 1008?

bigsexy
bigsexy over 5 years ago

I Have been searching for an affordable usb scope for a few months and ran across the Hantek 1008. Anyone familiar with it or ever used one? I am wondering if it would possibly be a ok-decent low cost bench scope. I may occasionally use it on a car audio system that’s already installed, but that would be the exception to removing it from the workbench. I’ve had a Rigol 1054Z but sold it. I didn’t like having to take it off the bench and store it when not in use. I am curious if the 8 channels is a gimmick or legit. Or is it more of an overpriced logic level analyzer?

thanks for the input and any suggestions or ideas.
Kevin

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 5 years ago +2 suggested
    Hantek do make USB oscilloscopes, the 1008 is not one of them. Sometimes Hantek call it a DAQ and sometimes they do describe it as an oscilloscope. It has a very low acquisition rate (2.4MS/s), almost…
  • michaelkellett
    0 michaelkellett over 5 years ago

    Hantek do make USB oscilloscopes, the 1008 is not one of them. Sometimes Hantek call it a DAQ and sometimes they do describe it as an oscilloscope.

     

    It has a very low acquisition rate (2.4MS/s), almost no memory (4k points)  and only 100kHz bandwidth. (All those stated as "single channel", so likely to be worse by a factor of the number of channels in use.)

     

    It is not a logic analyser (far too slow).

     

    The Rigol 1054Z is a real (if entry level) digital scope.

     

    This is even cheaper, https://www.amazon.co.uk/HANTEK-Portable-Based-Digital-Oscilloscope/dp/B00EEX1W5G/ref=sr_1_6?dchild=1&keywords=hantek+os…

     

    but it is a scope in the conventional sense - it's about £60 so it will be very limited.

     

    You could get a Pico 2204A for £118, much better quality product and with known decent software.

    https://www.amazon.co.uk/Technology-PicoScope-2204A-Oscilloscope-channels/dp/B00GZMRZ3M/ref=bmx_4/258-4273423-6510169?_e…

     

    The Pico has a lower bandwidth (10MHz) than the Hantek 2 channel scope but a faster sampling rate, which will mean that in practice it is actually usable over the stated bandwidth. the software is the same as for the 6424E which I am currently road testing on E14 (but of course the hardware being very different it can't do all the same stuff.)

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • bigsexy
    0 bigsexy over 5 years ago in reply to michaelkellett

    Thank you. You managed to tell me what I couldn’t discern from the available details and will be looking into the pico.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • parasquid
    0 parasquid over 5 years ago in reply to michaelkellett

    Thanks for this, I've been using one of those DIY DSO mini scopes and I feel I want to "graduate" to an actual beginner scope. I looked at the Rigol 1054Z thanks to your suggestion and it seems the best bang for the buck scope I've seen so far image