Test & Tools
  • Technologies
  • More
Test & Tools
Forum Consumption profile equipment
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 10 replies
  • Answers 4 answers
  • Subscribers 387 subscribers
  • Views 2222 views
  • Users 0 members are here
  • tools
Related

Consumption profile equipment

jpnbino
jpnbino over 5 years ago

Hi all,

 

I've been searching for tools to measure ( profile)  the dynamic consumption of devices in normal operation and then give a report.

 

features desirable:

  • measure Max current, Average current
  • Max Voltage, Average current
  • Configurable voltage supply ( 0 ~ 12V )
  • can afford at least 1A
  • Good Software for reporting
  • Possibility to connect a battery and log the voltage and current

 

For instance, I've found was this one, but it is limited to 5V output max which is too low for my case (12v would be better ) :

https://www.qoitech.com/

 

If you people had a pleasant experience with any tool and can share, I'd appreciate it!

 

thanks,

  • Sign in to reply
  • Cancel

Top Replies

  • hlipka
    hlipka over 5 years ago +3 suggested
    The JouleScope should tick all boxes - 15V, 3A, 250kHz bandwidth. Its not exactly cheap, but for what it does its also not too expensive. Look for more current reviews - from what I remember the software…
  • michaelkellett
    michaelkellett over 5 years ago in reply to hlipka +3
    It looks quite good, and actually claims to switch the current sense resistors really fast - which must take a lot of effort since the resistance is so low on the 3A range. It's cheaper than the Quotech…
  • jpnbino
    jpnbino over 5 years ago in reply to michaelkellett +3
    Hi Michael, In my current work, we have basically all boards being powered by solar panels, batteries ( Lithium , Lead-acid battery), or supercap. Those boards are designed to: Wake up time to time read…
Parents
  • michaelkellett
    0 michaelkellett over 5 years ago

    It depends a lot on exactly what you want to measure, most power supplies and even data loggers struggle with the dynamic range of the current drawn by IOT like devices,

    1A maximum is not uncommon but the sleep current might be down in the uA or less region.

    Very few systems can measure and log this if you want to catch fast spikes of high current  - the Keysight boxes can but you are looking at £5k+.

    As Shabaz points out, if you want to simulate a battery then that's a whole extra can of worms.

     

    I looked at the Qoitech and I did not like what I saw, the claimed operating temperature range is 15C - 25C - this looks like a company that doesn't know what it's doing.

    The detail in their specs is just a joke comapred with that from Keysight, R & S, Keithley etc. And they seem to want loads of extra money for software licenses.

     

    Like Shabaz, I've always ended up using multiple instruments, bench psu with computer control, Keithley DMM6500 (nice programmable DMM with fast logging if needed), or maybe use Kesysight DAQ.

     

    Can you tell us a bit more about the typical current profiles of things you want to measure ?

     

    MK

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • jpnbino
    0 jpnbino over 5 years ago in reply to michaelkellett

    Hi Michael,

     

    In my current work, we have basically all boards being powered by solar panels, batteries ( Lithium, Lead-acid battery), or supercap. Those boards are designed to:

    • Wake up time to time read many different sensors applied in agriculture: temperature, ultrasonic wind sensor, soil moisture, salinity... ; (Normally currents are way below 100mA)
    • and via LoRa/NBIOT/CAT/2G/3G Modems report the sensors data to a server; ( when transmitting data can range from 40mA in LORA to 300mA on the modems )
    • also, connect and power other boards  ( sensor node made by us too );
    • To have switches to cut energy from the peripherals which even sleeping can consume some mA. (some boards in sleep mode go for 9uA-12uA)

     

    Therefore in order to have a better estimation of battery life and the power consumption of our boards and also the sensors attached to them I am looking for such a tool.

     

    ...if you want to catch fast spikes of high current...

    I think I don't have issues with fast spikes in these applications, at least up to now.

     

    Like Shabaz, I've always ended up using multiple instruments, bench psu with computer control, Keithley DMM6500 (nice programmable DMM with fast logging if needed), or maybe use Kesysight DAQ.

    I would go for it, but I'm not sure if the current budget can handle it. I will investigate this option; in the meantime, I'm looking carefully for the option pointed by Hendrik Lipka

     

    I hope I could clarify a bit more,

     

    Thanks

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • jpnbino
    0 jpnbino over 5 years ago in reply to michaelkellett

    Hi Michael,

     

    In my current work, we have basically all boards being powered by solar panels, batteries ( Lithium, Lead-acid battery), or supercap. Those boards are designed to:

    • Wake up time to time read many different sensors applied in agriculture: temperature, ultrasonic wind sensor, soil moisture, salinity... ; (Normally currents are way below 100mA)
    • and via LoRa/NBIOT/CAT/2G/3G Modems report the sensors data to a server; ( when transmitting data can range from 40mA in LORA to 300mA on the modems )
    • also, connect and power other boards  ( sensor node made by us too );
    • To have switches to cut energy from the peripherals which even sleeping can consume some mA. (some boards in sleep mode go for 9uA-12uA)

     

    Therefore in order to have a better estimation of battery life and the power consumption of our boards and also the sensors attached to them I am looking for such a tool.

     

    ...if you want to catch fast spikes of high current...

    I think I don't have issues with fast spikes in these applications, at least up to now.

     

    Like Shabaz, I've always ended up using multiple instruments, bench psu with computer control, Keithley DMM6500 (nice programmable DMM with fast logging if needed), or maybe use Kesysight DAQ.

    I would go for it, but I'm not sure if the current budget can handle it. I will investigate this option; in the meantime, I'm looking carefully for the option pointed by Hendrik Lipka

     

    I hope I could clarify a bit more,

     

    Thanks

    • Cancel
    • Vote Up +3 Vote Down