Test & Tools
  • Technologies
  • More
Test & Tools
Forum Thoughts on an entry level scope?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 386 subscribers
  • Views 2279 views
  • Users 0 members are here
  • test
  • oscilloscope
Related

Thoughts on an entry level scope?

DaveYoung
DaveYoung over 15 years ago

Well, I have decided with my latest project that it is time to step up and buy a scope instead of continuing to use an old rummaged one.  Since I'll mainly be using it for side projects, fun stuff, audio, and troubleshooting I think I'm going to succumb to my natural price-sensitive, optimizing ways (Not the usual do-it-right path I like to take for tools).

 

I've got a couple ideas of scopes to buy in a Rigol DS1000 or an Instek GDS-1062A.

 

Does anyone have any other suggestions for me to check out?  Any thoughts on the two above?  Even with the discount rack, it's great to buy new gear!

 

-Dave Young

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 15 years ago
    First of all, I do have to share that I work for Tektronix.
     
    As you pointed out, when choosing an oscilloscope, many factors come into play. Price is one, but the first one certainly is that the scope needs to measure the signals you are actually interested in. If you haven’t already purchased an oscilloscope, there are currently a number of very interesting promotions that could help meet your budget requirements. I’d recommend looking at either the MSO/DPO2000 Series or the TDS2000C Series.
     
    The MSO/DPO2000 Series has 100MHz and 200MHz models, 1M points record length on each channel (even if you use multiple channels, you still have the 1MPoints for each of your channel), and a sample rate of 1GS/s on each of the channels. If you ever need to do any serial data work, the optional serial decode capability allows you to get even more functionality out of the MSO/DPO2000 scope for your dollars spent. Alternatively, for basic signal visualization, the TDS2000C is a great choice. Models start at 50MHz, 2.5Kpoints memory length, up to 2Gs/s sample rate and have a limited lifetime warranty. Check out the MSO/DPO2000 datasheet (http://www.tek.com/products/oscilloscopes/mso2000/) and the TDS2000C datasheet (http://www.tek.com/products/oscilloscopes/tds2000/) to see if these recommendations are a fit for your application needs.
     
    Tektronix currently has some awesome promotions running on these products, check out the following link to see how you can save: http://www2.tek.com/cmswpt/podetails.lotr?ct=PO&cs=pro&ci=18086&lc=EN. I hope this helps!
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Hi Sara,

    Thanks for mentioning your employer, I appreciate the clarity.  It's also timely, as I have a question about the Tektronix  DSOs you mentioned: Since the MSO/DPO2000C Series have very long  acquisition memory, I was wondering how that memory is handled when it  is output to the screen.  It's easier to propose an example so hard  numbers are being used.  If you set the timebase to 0.1 milliseconds per  division, the total time recorded will be 1 millisecond across the  screens 10 divisions.  At the maximum sample rate, the whole memory  buffer will be filled, or 1 million samples will be taken and stored in  the acquisition memory.  Since the display is 480 pixels wide, and with  typical edge surrounds, it means that the display part of the screen (10  divisions) looks to be around 450 pixels.  This means that 1 million  data points has to be represented by 450 pixels.  How is this done?  Is  the acquisition memory decimated, showing only 1 data point out of every  1,000,000/450=2,222 (approx) points?  Or is there some  acquisition_memory_to_display_compression_algorithm that runs in the  background to make any amplitude variation visible on the normal  screen?  I'm not talking about using waveform zoom to see the pulse, but  when you first set the scope to 0.1 millisecond per division.  As an  example, if there was a single pulse of 0.1 microseconds width somewhere  in the memory, it would occupy about 100 memory words.  If this 100  points fell in between the displayed points, every 2,222 points, would  this always be displayed on the main screen without using zoom?

    Thanks, Colin

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Hi Colin,

     

    You are exactly right. There is some display compression occurring with more samples than pixels (which happens a lot, especially for long records). As you imagine, long records aren't useful for visual inspection and debug. To get better detail you would use the zoom function. In fact, on the MSO/DPO2000 Series you could use the Wave Inspector controls which allows you to quickly zoom and pan with one set of knobs (kinda like a Digital Video Recorder controller for pausing/playing/fast forwarding TV shows).

     

    One more thing to point out is that part of the display compression algorithm accounts for unique or low duty cycle events. Say you have a clock that has a glitch appear this glitch would be more prominent while the other normal cycles would be "blended" into each other. This is also true with MSO digital channels where glitches, runts and other signal anomalies are highlighted in white. Again, it can be difficult to observe events without zoom but we do try to make easier with some built-in display tools like highlighting and weighted signal display features. I hope this helps.

     

    ~Sara

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to e14 Contributor

    Hi Colin,

     

    You are exactly right. There is some display compression occurring with more samples than pixels (which happens a lot, especially for long records). As you imagine, long records aren't useful for visual inspection and debug. To get better detail you would use the zoom function. In fact, on the MSO/DPO2000 Series you could use the Wave Inspector controls which allows you to quickly zoom and pan with one set of knobs (kinda like a Digital Video Recorder controller for pausing/playing/fast forwarding TV shows).

     

    One more thing to point out is that part of the display compression algorithm accounts for unique or low duty cycle events. Say you have a clock that has a glitch appear this glitch would be more prominent while the other normal cycles would be "blended" into each other. This is also true with MSO digital channels where glitches, runts and other signal anomalies are highlighted in white. Again, it can be difficult to observe events without zoom but we do try to make easier with some built-in display tools like highlighting and weighted signal display features. I hope this helps.

     

    ~Sara