Test & Tools
  • Technologies
  • More
Test & Tools
Forum 0-1000 psi pressure sensor needed
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 387 subscribers
  • Views 1054 views
  • Users 0 members are here
  • test
  • pressure
  • measurement
  • sensor
Related

0-1000 psi pressure sensor needed

Catwell
Catwell over 15 years ago
I need a cheap pressure sensor capable of going from 0-1000 psi to measure various compressed gases. Most I have found were well over $100 USD. There must be some alternatives out there.
 
Cabe
  • Sign in to reply
  • Cancel
Parents
  • jvdberg@ieee.org
    0 jvdberg@ieee.org over 15 years ago
    Hi Cabe,
    An analog pressure meter using a bourdon tube gauge is cheaper than an electronic one.
    These meters are second hand available for very low prizes.
    Look what I found in a few seconds on the internet.
    image
    They are used for several applications, like diving equipment and gas containers.
    When a pressure meter is not accurate anymore, it is often discarded.
    The accuracy problem could be caused by wear or by dirt on the mechanism between the bourdon tube and the needle.
    You can get such a meter for free from the trash container of a place where maintenance is performed on diving equipment.
    The accuracy problem could be caused by dirt or a worn out mechanism between the bourdon tube and the needle.
    If you want an electronic readout, you could replace the needle by a disk with a print on it that can be read with a ray of light.
    Another way is attaching a pressure sensitive resistor directly to the  bourdon tube. This way you could use an old meter with a worn out mechanism. The picture below shows the inside of a bourdon tube gauge.
    image
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Catwell
    0 Catwell over 15 years ago in reply to jvdberg@ieee.org

    Johan,

     

    Good suggestion, I use something like that right now. But I am looking for a digital solution.

     

    Cabe

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to Catwell

    These devices are all over the place.

     

    http://images.grainger.com/B341_22/images/products/250x250/Pressure-Transducer-5DEK0_AS01.JPG

     

    Grainger.com about $200.

     

    If you don't need precision and tested calibration, but want to work it out yourself, any cheapo piezo crystal buzzer will deform proportionate to pressure.  For lower values can try a cheapo digital tire gauge and mod it as a pressure sensor far above its rating. Often the sensors can detect much higher than 200 psi,  just its out of range for the devices uC code.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 15 years ago in reply to Catwell

    These devices are all over the place.

     

    http://images.grainger.com/B341_22/images/products/250x250/Pressure-Transducer-5DEK0_AS01.JPG

     

    Grainger.com about $200.

     

    If you don't need precision and tested calibration, but want to work it out yourself, any cheapo piezo crystal buzzer will deform proportionate to pressure.  For lower values can try a cheapo digital tire gauge and mod it as a pressure sensor far above its rating. Often the sensors can detect much higher than 200 psi,  just its out of range for the devices uC code.