Test & Tools
  • Technologies
  • More
Test & Tools
Forum Are 15A Banana Jacks safe to use on an 18A output?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 386 subscribers
  • Views 1075 views
  • Users 0 members are here
Related

Are 15A Banana Jacks safe to use on an 18A output?

e14 Contributor
e14 Contributor over 13 years ago

I wasn't really sure where to put this, but here goes.

 

I recently got the idea to build myself a cheapo benchtop power supply using an old ATX computer PSU that I had. Everything works fine, and I've been using it, but now I think I want to make it more functional by adding a variable line and some banana jacks.

 

Here are the specs of the PSU:

 

+5.0V18.0A*
+3.3V11.0A*
+12.0V17.0A
-12.0V0.3A
+5.0VS2.0A
TOTAL 250W MAX

*Between the 5.0V and the 3.3V there is a little bridge that says TOTAL 120W MAX.

 

Obviously, the lower amps I'm not worried about, but the higher ones bring some confusion.

 

I was originally going to go with these Banana Jacks for my PSU: http://www.newark.com/johnson-emerson/108-0902-001/banana-jack-15a-solder-red/dp/39F1574

 

But, then I noticed that their current rating is 15.0A which is less than my power supply will supposedly put out.

 

Now I am considering using these Banana Jacks: http://www.newark.com/pomona/72930-0/banana-jack-36a-screw-black/dp/26M8715

(albeit from a different source, I'm not sure why these are so expensive here)

 

I was wondering if this change was necessary, because, the second set of jack's will cost me about 5x as much as the first set.

 

Any help is greatly appreciated.

  • Sign in to reply
  • Cancel
Parents
  • michaelkellett
    0 michaelkellett over 13 years ago

    I can't quite tell from the pictures but I think the cheaper 4mm sockets you refer to are the traditional type and the expensive ones are touchproof.  Since the supply you are making is for home use I would suggest you use the cheap sockets if cash is tight. This will only be  a problem if you use your supply continuously at the max 5V current which I expect is unlikely. Unless you also use good quality plugs the plug/socket interface will probably cause you more trouble than the socket itself. Depending on how you mean to use the supply perhaps you could provide two pairs of sockets for 5V.

     

    Michael Kellett

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 13 years ago

    I can't quite tell from the pictures but I think the cheaper 4mm sockets you refer to are the traditional type and the expensive ones are touchproof.  Since the supply you are making is for home use I would suggest you use the cheap sockets if cash is tight. This will only be  a problem if you use your supply continuously at the max 5V current which I expect is unlikely. Unless you also use good quality plugs the plug/socket interface will probably cause you more trouble than the socket itself. Depending on how you mean to use the supply perhaps you could provide two pairs of sockets for 5V.

     

    Michael Kellett

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to michaelkellett

    Thanks for the quick response.

     

    In an oddly startling moment I came to the conclusion that the PSU will only put out as many amps as the component it is powering requires. Why I thought otherwise, I have no idea.

     

    The plugs I was looking at are similar to the ones on my multimeter, which are, indeed, a pain to use.

     

    Thanks,

    Liam