Test & Tools
  • Technologies
  • More
Test & Tools
Forum Are 15A Banana Jacks safe to use on an 18A output?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 4 replies
  • Subscribers 386 subscribers
  • Views 1075 views
  • Users 0 members are here
Related

Are 15A Banana Jacks safe to use on an 18A output?

e14 Contributor
e14 Contributor over 13 years ago

I wasn't really sure where to put this, but here goes.

 

I recently got the idea to build myself a cheapo benchtop power supply using an old ATX computer PSU that I had. Everything works fine, and I've been using it, but now I think I want to make it more functional by adding a variable line and some banana jacks.

 

Here are the specs of the PSU:

 

+5.0V18.0A*
+3.3V11.0A*
+12.0V17.0A
-12.0V0.3A
+5.0VS2.0A
TOTAL 250W MAX

*Between the 5.0V and the 3.3V there is a little bridge that says TOTAL 120W MAX.

 

Obviously, the lower amps I'm not worried about, but the higher ones bring some confusion.

 

I was originally going to go with these Banana Jacks for my PSU: http://www.newark.com/johnson-emerson/108-0902-001/banana-jack-15a-solder-red/dp/39F1574

 

But, then I noticed that their current rating is 15.0A which is less than my power supply will supposedly put out.

 

Now I am considering using these Banana Jacks: http://www.newark.com/pomona/72930-0/banana-jack-36a-screw-black/dp/26M8715

(albeit from a different source, I'm not sure why these are so expensive here)

 

I was wondering if this change was necessary, because, the second set of jack's will cost me about 5x as much as the first set.

 

Any help is greatly appreciated.

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Like in all products there is a tolerance, I am sure the 15 Amp Jacks can withstand more than their rated amps. If pulling 18 Amps for a prolonged period i would check them and see if they are over heating if not go with it. I made some out of copper tubing and a rubber hose and sometimes get 45 amps out. No problems yet and no smoke!

    Giltronics

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 13 years ago

    Like in all products there is a tolerance, I am sure the 15 Amp Jacks can withstand more than their rated amps. If pulling 18 Amps for a prolonged period i would check them and see if they are over heating if not go with it. I made some out of copper tubing and a rubber hose and sometimes get 45 amps out. No problems yet and no smoke!

    Giltronics

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • e14 Contributor
    0 e14 Contributor over 13 years ago in reply to e14 Contributor

    Wow, that sounds pretty sketchy!

     

    I tested a few things to see what kind of amps I would usually be pulling. Nothing that I seem to had laying around (that I would want to test with this) seems to pull more than 5A. Infact, quite a few were around or under 2.

    I think these will be fine. image