Test & Tools
  • Technologies
  • More
Test & Tools
Forum Who does I2C address decode better - Agilent or Tektronix?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 8 replies
  • Subscribers 387 subscribers
  • Views 1231 views
  • Users 0 members are here
  • address
  • i2c
  • tektronix
  • decode
  • agilent
Related

Who does I2C address decode better - Agilent or Tektronix?

Instructorman
Instructorman over 12 years ago

This question is for anyone who has used I2C decode features on Agilent or Tektronix oscilloscopes, or anyone interested in how I2C address decode should be done.  The two manufacturers handle I2C addresses differently and I wonder how users feel about the two approaches.

 

On Tektronix 'scopes, I2C addresses are entered as full 8-bit hex values, so the R/W' bit is included in the hex value.  On Agilent scopes, I2C addresses are entered as 7-bit hex values, and the R/W' bit is tacked on as the letter R or W.

 

Obviously, both approaches work, but the Agilent approach strikes me as a little odd.  Here is why:  Most data sheets I've seen provide I2C addresses as 8-bit values with the R/W' bit included as the LSB.  For example, Maxim refers to the DS1307 address as 1101000 followed by a R/W' bit of either 0 (for write) or 1 (for read).  Put that all together and you get 11010000b = D0h for write and 11010001b = D1h for read.  These are the values a user would enter into a Tektronix 'scope to detect and decode I2C communication with a DS1307.  On the other hand, on an Agilent 'scope the I2C addresses for the DS1307 are entered as 68W and 68R.  These values correspond to the 7-bit I2C address followed by an R or W to denote an 8th bit.  Now, a hex digit should, to me, represent 4-bits of binary.  Agilent seems to be using an octal digit followed by a hex digit, followed by a letter.  I find that confusing and awkward.  I asked an Agilent rep about why I2C was handled this way, but never got a response.

 

So, which approach do you prefer, and why?

  • Sign in to reply
  • Cancel
Parents
  • sqkybeaver
    0 sqkybeaver over 12 years ago

    I definitely prefer it the way Tek does it. give me the actual value so i don't screw up my code.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to sqkybeaver

    I checked in the I2C standard (NXP document UM10204), and interestingly enough NXP don't express addresses in hex at all: from page 13:

    Data transfers follow the format shown in Figure 9. After the START condition (S), a slave

    address is sent. This address is seven bits long followed by an eighth bit which is a data

    direction bit (R/W) — a ‘zero’ indicates a transmission (WRITE), a ‘one’ indicates a

    request for data (READ)

    The table on page 17 gives a clue about NXP's prefered route, the address is binary with the R/W bit shown separately. This would suggest that Agilent and Tek are both wrong and that the address in Mark's example should be shown as 0x34 (which is confusing but is a method I have seen used in several data sheets).

     

    I think I have a marginal preference for the Agilent approach - it draws your attention to the fact that it is definitely NOT an 8 bit address.

     

    If I remember I'll post exactly how the LeCroy decoder and ZeroPlus logic analyser do it when I next have an I2C something running.

     

    BTW do ANY of these decoders cope with 10 bit I2C addressing (which I didn't even know about until I was reading the standard this morning !!)

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • michaelkellett
    0 michaelkellett over 12 years ago in reply to sqkybeaver

    I checked in the I2C standard (NXP document UM10204), and interestingly enough NXP don't express addresses in hex at all: from page 13:

    Data transfers follow the format shown in Figure 9. After the START condition (S), a slave

    address is sent. This address is seven bits long followed by an eighth bit which is a data

    direction bit (R/W) — a ‘zero’ indicates a transmission (WRITE), a ‘one’ indicates a

    request for data (READ)

    The table on page 17 gives a clue about NXP's prefered route, the address is binary with the R/W bit shown separately. This would suggest that Agilent and Tek are both wrong and that the address in Mark's example should be shown as 0x34 (which is confusing but is a method I have seen used in several data sheets).

     

    I think I have a marginal preference for the Agilent approach - it draws your attention to the fact that it is definitely NOT an 8 bit address.

     

    If I remember I'll post exactly how the LeCroy decoder and ZeroPlus logic analyser do it when I next have an I2C something running.

     

    BTW do ANY of these decoders cope with 10 bit I2C addressing (which I didn't even know about until I was reading the standard this morning !!)

     

    MK