Test & Tools
  • Technologies
  • More
Test & Tools
Forum finding out the amp usage of a part
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 14 replies
  • Answers 2 answers
  • Subscribers 390 subscribers
  • Views 2644 views
  • Users 0 members are here
Related

finding out the amp usage of a part

shanesissons
shanesissons over 11 years ago

hi sounds like quite a beginner question but I need to find out how much ma a device is using

as I'm having some trouble getting some components to work together through a power supply i have looked on the multimeter but can't seem to locate what i need and where on the component i need to add this to

the component in question is a peltier that i believe is 12v but due to it being sealed in a part i can not see

 

any advice would be great

 

many thanks

shane

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago +1
    Most multimeter's will have a high burden voltage , here is a video that talks about it by Dave Jones from the EEVBlog (An Early one of his) https://www.youtube.com/watch?v=u2yRR4G3yTA Goto about the 3…
Parents
  • D_Hersey
    0 D_Hersey over 11 years ago

    Gotta part company with you on this idea, Lupe.  The Peltier cooler acts like a diode rather than a resistor.  The Peltier cooler isn't linear and so Ohm's law cannot be applied well.

     

    You gotta do what the other guys said and break the circuit and insert the ammeter.

     

    "The ideal voltmeter has infinite input impedance.

    The ideal ammeter has zero input impedance."

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • supper_slash
    0 supper_slash over 11 years ago in reply to D_Hersey

    Well, i understand, but than we have another proble.

    From Shanes origional post, the pelter is overloading his available power supply.

     

    "Hi all,

    im working on the camping chair rebuild and i have came acroos some issues with the electronics im not sure if there a problem on my part or on the parts side.

     

    firstly i hooked up the fans and smoke detector tothe psu and to a 12v 500ma power supply everythink worked fine the fans were running at half speed due to the fans both trying to use 500ma each so i then unhooked this and attached the peltier to the psu... this is where the problems started.

    firstly the led on the psu was flashnig and there was a humming comming from the psu i hooked a temp monitor up to the cooler and i noticed it wasnt cooling i then tested the voltages the smoke detector was 5v and the cooler was only at 9.8v i had believed that the peltier was 12v.

    so i hooker the coller up to the 12v supply and hey presto the cooler dropped from 20 celcius to 15 in about a minute this was a dry run with the probe on the heat sink then problems again the power supply failed so i am guessing that the peltier uses more than 500ma?

     

    anybody have any ideas?

    and if ben happens to read this i would greatly apreciate  the volts of the peltier as i cant read the peltier because someone epoxied it inplace

     

    shane"

     

    In which case, i don't think the ammeter will work ether.

    Example: If i have a circuit that requires 1.5 amps, and i have a supply that will only supply 1 amp, will the meter only read the 1 amp of current flowing through the circuit?

     

    If the OHM  meter wont help, than the only other thing i can think of is to place a known resistance in series with the peltier, and measure the voltage drop difference between the the resistor than calculate the amperage that way?

    I am trying to help.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 11 years ago in reply to supper_slash

    The current rating on a power supply tells us the amount of power we can hope to get out of the supply without harm.  For a moment, depending upon its design, it may supply more.  If the supply features foldback limiting, it will just drop the output potential when challenged.   Ammeters can read the amount of current they are rated for.  Except that it can be a little lossy, inserting a series resistor to measure the drop and infer the current will work fine.  A ten Siemens conductor would probably work fine, provided it could handle the power.  Hall effect current sensing is also a possibility.  Sensing based on magnetic saturation is a possibility at higher current densities. 

     

    Our inquirer should find himself a larger PS.  It is perfectly okay to use a PS rated for more current than needed.  In a hot environment, if might even be a good idea.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • supper_slash
    0 supper_slash over 11 years ago in reply to D_Hersey

    I think that's his goal, finding out what size power supply he needs for the circut.

    So he can buy the supply he needs.

    But he don't know the requirement of the circuit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • jw0752
    0 jw0752 over 11 years ago in reply to supper_slash

    Peltiers are notoriously power hungry. If he has a variable power supply he could start at a low voltage and measure the current at successive points inorder to graph the power curve of the peltier. If his ammeter or power supply can't handle the full draw at the 12 volts he can interpolate the graph in order to estimate the current at the 12 volts. As Don pointed out don't expect the graph to be a straight line.

    John

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shanesissons
    0 shanesissons over 11 years ago in reply to jw0752

    ok that was a lot of reading to wake up to I'm going to see if i can find a better power supply with more amps to test again i don't have a variable bench power supply i will be looking into getting one of these I'm currently using left over power supply from previous projects and devices I'm going to go out on a limb and look for a 2 amp power supply as both of the parts run on a 1200ma power supply so hopefully 2 would be more than enough think i might do my electronics at college after christmas i need a brush up

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shanesissons
    0 shanesissons over 11 years ago in reply to jw0752

    ok that was a lot of reading to wake up to I'm going to see if i can find a better power supply with more amps to test again i don't have a variable bench power supply i will be looking into getting one of these I'm currently using left over power supply from previous projects and devices I'm going to go out on a limb and look for a 2 amp power supply as both of the parts run on a 1200ma power supply so hopefully 2 would be more than enough think i might do my electronics at college after christmas i need a brush up