Test & Tools
  • Technologies
  • More
Test & Tools
Forum Add piezo speaker to Cen Tech 7 function (free) multimeter?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Suggested Answer
  • Replies 4 replies
  • Answers 1 answer
  • Subscribers 386 subscribers
  • Views 1238 views
  • Users 0 members are here
  • multimeters
Related

Add piezo speaker to Cen Tech 7 function (free) multimeter?

modalpdx
modalpdx over 11 years ago

Okay, before anyone advises me to buy a real multimeter, here's a full disclosure: I own a military-grade Fluke 27 and it works perfectly.

 

Now, with that out of the way...

 

I just snagged one of those free Harbor Freight multimeters (brand and description are in the subject) and I am actually charmed by the thing, but there's one missing piece: no audible connectivity. It can test connectivity, but unlike my Fluke it does not give me a nice "beeeeeep" when I have a connection. If I had to guess, I'd say 80% or more of my multimeter use is testing connections so this is a bit of an inconvenience.

 

This seems like something that would be easy to change, but I know better than to assume it actually is easy. Folks out there have hacked these little multimeters to do all kinds of stuff but I have not yet seen anyone add a basic piezo speaker. Too hard? Too easy/boring? I can't say.

 

If anyone out there has done this and can offer hints, or if anyone has seen websites that describe the process, I'd love to hear about it.

 

Thanks!

 

E?

  • Sign in to reply
  • Cancel
Parents
  • sqkybeaver
    0 sqkybeaver over 11 years ago

    you can use 1/2 of dual opamp as an oscillator to drive the speaker, and the other half as a comparator on the adc input. power this circuit off the selector switch so it will only turn on when in continuity mode.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Reply
  • sqkybeaver
    0 sqkybeaver over 11 years ago

    you can use 1/2 of dual opamp as an oscillator to drive the speaker, and the other half as a comparator on the adc input. power this circuit off the selector switch so it will only turn on when in continuity mode.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
Children
  • modalpdx
    0 modalpdx over 11 years ago in reply to sqkybeaver

    Thanks Sheldon! I'll need to do some research to unwrap some of that (I'm more of a programmer than an electronics guru) but none of what you described is completely unfamiliar so I'm sure I'll be able to work it out. It's a direction to go in, and at this point that's all I'm after.


    Thanks again!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • sqkybeaver
    0 sqkybeaver over 11 years ago in reply to modalpdx

    your welcome,

     

    also it may be worth doing some probing with a scope to see if there is an unused output for a speaker.