Test & Tools
  • Technologies
  • More
Test & Tools
Forum Tenma 72-7730 and 72-7732A multimeter
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 4 replies
  • Subscribers 387 subscribers
  • Views 1251 views
  • Users 0 members are here
  • 72-7730
  • usb
  • dmm
  • tenma
  • 72-7732a
  • labview
  • 77-7732
Related

Tenma 72-7730 and 72-7732A multimeter

stevedoddsdesignltd
stevedoddsdesignltd over 11 years ago

Hi

I am trying to use a 72-7730 and 72-7732A multimeters USB interfaces at the same time., however even when I run a copy of each the 72-7730 and 72-7732A windows application they will only talk to one of the multimeters (they both communicate to the same DMM).  How do I communicate with both DMMs at the same time?

 

Do you have labview drivers so i can write my own application?

 

Many thanks

Steve

  • Sign in to reply
  • Cancel
  • clem57
    0 clem57 over 11 years ago

    The drivers for these are closed sourced, so they cannot be changed. sorry

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • stevedoddsdesignltd
    0 stevedoddsdesignltd over 11 years ago in reply to clem57

    OK.  How do I use two multimeters at the same time with their USB interface and the provided PC application?

    Thank you

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dougw
    0 dougw over 11 years ago

    Here is a user who seems to have figured out how to communicate without the factory drivers...

    https://relavak.wordpress.com/2009/10/04/tenma-72-7730-in-linux/

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • clem57
    0 clem57 over 11 years ago in reply to dougw

    Thanks Doug for the great answer. Seems like this comment says it all:

    Bill Cooper Says:

    February 2, 2015 at 11:34 am | Reply

    If you place an IR receiver against the transmitter you’ll find it’s a very simple rs232 comms format, 2400,7,1,none and no handshake (of course) you get back a string of 11 bytes first 5 are the reading 6th = decimal point position, with the rest being for range etc. feed this data into any terminal program to decode the last bytes – why even try to reverse engineer the USB? all sorted in a few hours. For my IR device I merely placed the anode to pin 4 of a 9 pin female and the cathode to pin 2 ( i found a regular + 6volts on pin 4!

    Happy days!