Test & Tools
  • Technologies
  • More
Test & Tools
Forum RF Connectors Assortment
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 383 subscribers
  • Views 7793 views
  • Users 0 members are here
  • connectors
  • mhf4
  • ipex
  • sma
  • rf
  • u.fl
Related

RF Connectors Assortment

shabaz
shabaz over 4 years ago

I spent a good 20 minutes the other day, trying to make an antenna fit a Wireless LAN (WLAN) card. It just wouldn't snap on, and finally, I realized the antenna had a U.FL plug, whereas the WLAN card had a MHF 4 socket : ) 

I'd never heard of MHF 4 before, but it seems to be very popular in the laptop computer world. Anyway, while I was at it trying to visually compare the connectors, I took this photo - perhaps useful for identifying connectors in the future : )

The photo is missing connectors, especially some common ones like N connector, and the PL-259 (popular in ham radio equipment).

BNC of course is very popular, as is SMA. I really like SMB, it's like a hassle-free version of SMA, but unfortunately, it is not as popular on equipment. 

(Click photo to enlarge):

image

EDIT:

Decided to re-take the photo and add N and TNC. Also added a PL-259.

image

  • Sign in to reply
  • Cancel

Top Replies

  • phoenixcomm
    phoenixcomm over 4 years ago +5
    Nice assortment. I also have some GR connectors like this one They are good from DC to 9 GHz find more info here ~~Cris
  • phoenixcomm
    phoenixcomm over 4 years ago in reply to shabaz +4
    BTW BNC comes in both flavors 50 & 75 ohms You have to check the pns ~~Cris
  • Jan Cumps
    Jan Cumps 1 month ago +4
    I got some SMA components recently. To check which ones I can use best for measurements. A few T-adapters, BNC to SMA adapters, a bit of 50 Ohm cable, 50 Ohm terminators.
  • obones
    obones 1 month ago in reply to shabaz

    I'm more of a glue gun kind of guy, but I guess there are reasons not to use that in such a situation . 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz 1 month ago in reply to obones

    Not a bad idea, since that won't drip inside the connector : ) 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave 1 month ago in reply to shabaz
    shabaz said:
    Incidentally, I was also wondering how to make it more permanent, because I won't be around when this board is installed in an enclosure, it is for a friend to fit in their garden watering "system". They would not know how to re-snap that connector in, if it worked loose. 

    Is this some sort of 'extreme watering/gardening' thing we should know about ? Slight smile

    Perhaps a couple of holes through the PCB and a thin cable tie or loop of tinned copper wire through them and around the back of the connector ? 

    Could do similar with the cable instead of the Polydoh/UV glue..

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz 1 month ago in reply to beacon_dave

    It's some off-the-shelf watering system they installed, just happens to not provide good alerts when the water is low. There is an enclosure and solar panel, so an option is to open up the box and stick it there if there's space (I have not thought the installation through! will leave that to them to figure out : ) The design is a bit ad hoc.. maybe a PCB antenna would have been better all round.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<