Test & Tools
  • Technologies
  • More
Test & Tools
Forum RF Connectors Assortment
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 383 subscribers
  • Views 7446 views
  • Users 0 members are here
  • connectors
  • mhf4
  • ipex
  • sma
  • rf
  • u.fl
Related

RF Connectors Assortment

shabaz
shabaz over 4 years ago

I spent a good 20 minutes the other day, trying to make an antenna fit a Wireless LAN (WLAN) card. It just wouldn't snap on, and finally, I realized the antenna had a U.FL plug, whereas the WLAN card had a MHF 4 socket : ) 

I'd never heard of MHF 4 before, but it seems to be very popular in the laptop computer world. Anyway, while I was at it trying to visually compare the connectors, I took this photo - perhaps useful for identifying connectors in the future : )

The photo is missing connectors, especially some common ones like N connector, and the PL-259 (popular in ham radio equipment).

BNC of course is very popular, as is SMA. I really like SMB, it's like a hassle-free version of SMA, but unfortunately, it is not as popular on equipment. 

(Click photo to enlarge):

image

EDIT:

Decided to re-take the photo and add N and TNC. Also added a PL-259.

image

  • Sign in to reply
  • Cancel

Top Replies

  • phoenixcomm
    phoenixcomm over 4 years ago +5
    Nice assortment. I also have some GR connectors like this one They are good from DC to 9 GHz find more info here ~~Cris
  • phoenixcomm
    phoenixcomm over 4 years ago in reply to shabaz +3
    BTW BNC comes in both flavors 50 & 75 ohms You have to check the pns ~~Cris
  • Jan Cumps
    Jan Cumps 2 days ago +3
    I got some SMA components recently. To check which ones I can use best for measurements. A few T-adapters, BNC to SMA adapters, a bit of 50 Ohm cable, 50 Ohm terminators.
  • rsjawale24
    rsjawale24 over 4 years ago

    Nice one! During my early days I always struggled with choosing the right connector.

    Each one comes with a maximum frequency limit. BNCs are good till a few hundreds of MHz. Above that only the SMA/SMB type or N type are useful. Among SMA and N type also there is a frequency limit. Most low cost SMAs are only good till 6GHz, good quality SMAs from TE, Molex, etc can go only till 18 GHz above which one has to go for the 2.92mm connectors very popular in mm-wave systems. They can go upto 40GHz.

    And the cable in the above picture is RG316- is good only till 6GHz. Would love to see another blog on types of RF cables :)

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 4 years ago

    I am familiar with all those connectors except the MHF4. Boy that is a tiny connector. My guess it can only handle 10 or 20 insertion/removal cycles.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 4 years ago in reply to rscasny

    Yes, these are usually specified as max. 10 connections.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to Jan Cumps

    I've probably wrecked the connector on the WLAN card. I'll soon know!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 4 years ago

     imageNice assortment. I also have some GR connectors like this one 

    They are good from DC to 9 GHz find more info here

    ~~Cris

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • jc2048
    jc2048 over 4 years ago in reply to rsjawale24

    "BNCs are good till a few hundreds of MHz."

    Doesn't that depend a little on what you're trying to do with them? Oscilloscope manufacturers seem to manage ok with them up to a couple of GHz.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 4 years ago in reply to shabaz

    BTW BNC comes in both flavors 50 & 75 ohms Slight smile You have to check the pns

    ~~Cris

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to phoenixcomm

    Hi Cris,

    That style looks very similar to RF connectors on UK TVs : ) 

    Nowadays the coax is better, but I remember as a kid the coax had air spacing (with polythene internal ribs holding the cable in shape), and if there was any damage at the antenna end, then rainwater would run down it, into the TV..

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • phoenixcomm
    phoenixcomm over 4 years ago in reply to shabaz

    this is the GR784-TNC Coax 50 ohms For sure

    GR-874-QTNJ

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • kkazem
    kkazem over 4 years ago in reply to phoenixcomm

    For those of us that work in RF, it's critical to have a drawer (or box) full of adapters to connect the unit you're testing to the test equipment you have. Although large, my favorite is type-N as it has a wide frequency range and low loss and is double-shielded.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
>