Test & Tools
  • Technologies
  • More
Test & Tools
Forum Suggestions for software to generate arbitrary (arb) waveforms?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 15 replies
  • Subscribers 383 subscribers
  • Views 8261 views
  • Users 0 members are here
  • waveform
  • arbitrary_function_generator
Related

Suggestions for software to generate arbitrary (arb) waveforms?

baldengineer
baldengineer over 4 years ago

To avoid the XY Problem, here's what I'm trying to do: I want to generate a repetitive waveform with an occasional glitch. I intend to use it as a demonstration of how oscilloscope acquisition modes, interpolation, and triggers work. So the exact characteristics are yet to be determined. A minimum example would be 10 cycles (with some pre-determined period) with 1 cycle having a glitch (not sure how "big" yet.) A maximum example would be 20 cycles with the glitch where the glitch varies in the waveform. (All depending on available sample memory.)

Off-hand, I'm not aware of any good tools that help automate generating an arbitrary waveform such as that. Ideally, I'd like a CSV export. I'd like the time/voltage as CSV to make it more compatible with various instruments. (Also seems like it'd be useful in simulations?)

Any suggestions? Or what do other people use?

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 4 years ago +6
    I normally just write something quick in Python or use MATLAB. Judicious use of the csv, math and random libraries may well make it a quick job. Another option is that some AWG vendors have their own…
  • shabaz
    shabaz over 4 years ago +6
    Hi James, I find Excel useless at it too : ) It can't handle large datasets. If you want a graphical tool, then a free download of Tektronix ArbExpress will do it : ) You can tell it to generate a…
  • scottiebabe
    scottiebabe over 4 years ago +5
    Lots of good suggestions already. Here is yet another Spice Then you can export the data as a tab delimited file (at least in LTSpice) could always find and replace tab to comma if needed.
  • baldengineer
    baldengineer over 4 years ago

    One idea that just came to mind is to use Excel. I'd like something a little better suited for the task. ;)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 4 years ago

    I normally just write something quick in Python or use MATLAB. Judicious use of the csv, math and random libraries may well make it a quick job.

    Another option is that some AWG vendors have their own software that will let you generate a function and then edit it graphically. I think R&S' HMExplorer allows that kind of editing or generation but is more tuned to generating signals for power supplies.

    - Gough

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 4 years ago

    Hi James,

    I find Excel useless at it too : ) It can't handle large datasets.

    If you want a graphical tool, then a free download of Tektronix ArbExpress will do it : )
    You can tell it to generate a sine or square wave or whatever of the desired number of samples, rate, amplitude, etc, and then edit with a pen toolbar icon on-screen, e.g. insert a glitch, even a single sample width.

    (Example screenshot, the green boxes show the things to click on):

    image


    It saves in .CSV format (the first few lines contain Tek info but that can be deleted in any text editor).
    Although it could be edited in Excel, I find Excel will hang for a long time if the CSV file is very large.

    However, like Gough, I'd probably pick Matlab, since it is designed for such tasks, i.e. matrix or sequence array manipulations.

    There is free GNU Octave, which is very similar. Or Python as mentioned, since that too is designed for (or at least is perfect for) dataset work.

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 4 years ago

    Keysight's InfiniiVision X-Series scopes have training waveforms built-into the scope. There is a list of the included student training signals here:

    https://www.keysight.com/us/en/assets/7018-02756/data-sheets/5990-6690.pdf

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 4 years ago in reply to baldengineer

    Darn, I was going to suggest Excel.  It fits the CSV goal.

    Actually, I have used Excel to generate complex sequences, like multiple phase signals.  I also have used Excel to test digital filter algorithms and other algorithms for signals processing.

    An other suite that I have used in the past was mathworks.  The ability to generate data sets through mathematical expressions is very powerful. With this product is was possible to write entire logic simulations of systems and then drive them with complex data sets.

    Good luck!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich over 4 years ago in reply to baldengineer

    Excel even has an FFT hidden somewhere in its big fat belly.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 4 years ago in reply to shabaz

    Perfect Shabaz. I should have thought to check Tek's tool. I assumed it would just do their binary format.

    Turns out, the R&S RTM3000 can import the CSV file directly from the tool (he he.) And it looks like for this case, it'll do what I want with minimal fuss.

    Thank you!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 4 years ago in reply to Gough Lui

    My MATLAB / Octave is way too rusty to do something quick. But I should spend some time tinkering with a Python script.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 4 years ago

    Lots of good suggestions already. Here is yet another Spice Slight smile

    image

    image

    Then you can export the data as a tab delimited file (at least in LTSpice) could always find and replace tab to comma if needed.

    image

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 4 years ago

    Success! Cross vendor fun!

    Here's what I setup in Tek's software.

    image

    And now here is what I see on my RTM Scope.

    Sample (Normal) Mode rarely shows the glitch even though it should appear every other cycle.

    sample mode, no glitch

    Yet, Peak Detect Sees it on every acquisition. (Though, it does flip back and forth between the cycles.

    peak mode sees it

    Not really a practical example, but it's what I needed to demonstrate what "peak detect" can help find.

    Thanks All! I'll use some of these other suggestions for other AWG needs in the (hopefully) near future.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
>