Test & Tools
  • Technologies
  • More
Test & Tools
Forum RF transmission testing inside a Faraday cage
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 26 replies
  • Subscribers 384 subscribers
  • Views 13088 views
  • Users 0 members are here
  • faraday shield
  • rf transmitter testing
Related

RF transmission testing inside a Faraday cage

ralphjy
ralphjy over 4 years ago

Since there is RF expertise in the community, so I thought I'd try to get some insight into an area where I don't have much experience.

I'm currently working a project testing BLE transmitters and my current workroom location can experience a fair amount of RF noise in the 2.4GHz ISM band (primarily due to existing WiFi and Bluetooth/BLE).  My primary mitigation when possible is to increase distance from or turn off noise sources.  I started thinking about whether I could test within an RF shield.  My previous experiences with testing within RF enclosures was over 40 years ago and we used room scale enclosures to house the equipment and operators.

I was wondering if anyone has tried small scale enclosures to shield only the EUT and measurement setup.  What would be a good minimum size at this frequency?

TIA for any feedback.

Ralph

  • Sign in to reply
  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 4 years ago +7
    For rudimentary functional tests, I have heard of individuals using old microwave ovens as 2.4GHz faraday cages lol
  • robogary
    robogary over 4 years ago +6
    Hi Ralph - Green Bank Radio Telescope Observatory has entire buildings constructed as Faraday cages. Besides being a really fun and interesting visit, it is a public treasure, open to collaboration with…
  • shabaz
    shabaz over 4 years ago +5
    Hi Ralph, For transmission testing, just a spectrum analyser type of tool can be used (with appropriate attenuation), and a coax would be connected from the 50 ohm output (i.e. not solder any antenna…
Parents
  • ralphjy
    ralphjy over 4 years ago

    Thanks for all your input and sorry for my unresponsiveness - I had an unplanned trip to urgent care which consumed the better part of my day.  Urgent care is definitely a misnomer lol...

    I realized that I was a little ambiguous about the specific type of information that I was looking for.  For an antenna based transmission system, what is the minimum separation between the antenna and the shield that would not compromise the RF transmission.  Question is oversimplified as it will be affected by the type of antennas used.  I guess I was trying to figure out if there was any value in building a small cage for reducing measurement noise.  This is probably a science project Smile.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 4 years ago in reply to ralphjy

    Hi Ralph,

    I hope all is well.
    I've rarely used a faraday cage larger than a biscuit/cookie tin so I'm the wrong person to comment, but gut instinct suggests as you say, that it could be a very experimental/science project to see if it meets your needs.

    You might see benefits or disadvantages, depending on the precise test. The Faraday cage will help eliminate external interference and prevent broadcasting unwanted signals to others.

    On the other hand, there are these issues/things to work through:

    (a) if it is a very small cage, antennas would be used in near field (it's a distance proportional to the square of antenna dimension), so it's not the same as a normal far-field condition. This is almost definitely not an issue at all, if the test is protocol testing, but if the desired test is to examine antenna performance, then it is a factor

    (b) the metalwork may cause some antenna detuning, depending on the particular antenna design, again it may or may not be an issue depending on what's being tested

    (c) there will be reflections off the inside walls

    (d) there could be an overload risk with close antennas (I guess not an issue for WiFi/BLE since these are at low power levels)

    For (a) to (c) above, it may be of zero concern for some tests like protocol tests, but for others like performance tests (e.g. antenna performance) it could be an issue. I've never tried it so it's definitely worth taking what I'm saying with a pinch of salt.

    I believe it could be very difficult to get both absolute measurements, and relative/performance comparisons, because even a slight change in angle or position could cause a different measurement, due to (a) to (c).

    Ordinarily, for measurements with an antenna, it would need a location where there are very few reflections, e.g. outdoor field. Even quite large firms won't own antenna test chambers themselves, I'm not sure of the cost or practicality to self-build one, they have RF absorbing materials and shapes internally. The outdoor field should in theory give very good results, provided it is a large field, but even a small garden kind of works from my limited tests.

    If you're mainly concerned about external transmissions influencing results (since you mention noise), I believe the value of the cage is reduced, because the effect of external transmissions is eliminated anyway, if you can control the transmit frequency (which you can if you're using the test modes), if you can tune out the unwanted frequencies (which a spectrum analyzer will do, as will any receiver). (Incidentally, using some test modes continuously outdoors is likely not legal in some countries, so that's a benefit of the faraday cage, but if there is no cage, keeping transmissions short in the ISM band (like a 1-second burst for a test) at typical BLE power levels, just from a technical perspective I cannot imagine would practically cause any problem to anyone, but from a legal perspective I cannot say, since it depends on your country, laws, etc). 

    So, in summary, I believe this would definitely be a science project : ) and you can probably eliminate some of the potential issues with clever test designs, but I reckon you may be better off just using your existing indoor environment (or using a garden/field) and changing some things like transmit frequency, or move some tests to coax environment if not every test is antenna related, and so on. Changing receive antenna to something like log-periodic might be a benefit too. It's all a bit subjective though, and some things are hard to predict. You're likely learning all sorts of on-the-job tips and tricks just by trying different things.

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • ralphjy
    ralphjy over 4 years ago in reply to shabaz

    Hi Shabaz,

    Thanks for the your insight.  I've gotten the sense that this is something that I should avoid trying at the moment for the sake of not going down a rathole.

    I recognize to some degree the issues that you pointed out.  Within the context of my project I realize there might be some issues with the accuracy of my measurements (due to effects that you mention and others), but I'm hoping to develop a reasonably simple and repeatable setup to compare boards and antenna configurations.

    Using a Faraday cage would be a good learning experience and fun to try (although a pain to construct), so I'll hopefully find some time to try it in the future.

    Ralph

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ralphjy
    ralphjy over 4 years ago in reply to shabaz

    Hi Shabaz,

    Thanks for the your insight.  I've gotten the sense that this is something that I should avoid trying at the moment for the sake of not going down a rathole.

    I recognize to some degree the issues that you pointed out.  Within the context of my project I realize there might be some issues with the accuracy of my measurements (due to effects that you mention and others), but I'm hoping to develop a reasonably simple and repeatable setup to compare boards and antenna configurations.

    Using a Faraday cage would be a good learning experience and fun to try (although a pain to construct), so I'll hopefully find some time to try it in the future.

    Ralph