Test & Tools
  • Technologies
  • More
Test & Tools
Forum Lead acid battery charging
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 15 replies
  • Subscribers 384 subscribers
  • Views 7705 views
  • Users 0 members are here
  • charging
  • battery
Related

Lead acid battery charging

Workshopshed
Workshopshed over 3 years ago

I have some small 12V lead acid batteries and was wondering how to charge these. I've previously charged 6v batteries using a constant current charger based on a L200 regulator. And I think I can tune that to work with 12v.

But I wondered if an easier option would be to use my bench power supply. That has a current limiting mode and can easily provide the charging current.

Has anyone done this? Any pitfalls?

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 3 years ago +8
    You can certainly do this - usually for cycle-based charging, a safe voltage cap would be 14.4V with a current limit that matches the manufacturer's limitation. You should manually terminate charge when…
  • Workshopshed
    Workshopshed over 3 years ago +7
    Thanks for all the tips. Am in the process of booking flights to Canada to buy a cheap battery charger....
  • scottiebabe
    scottiebabe over 3 years ago +5
    As you suggest a bench supply works just fine as a current source. I consider it more of a battery tester than battery charger, it isn't something I would recommended you leave unattended. I use a schottky…
Parents
  • Gough Lui
    0 Gough Lui over 3 years ago

    You can certainly do this - usually for cycle-based charging, a safe voltage cap would be 14.4V with a current limit that matches the manufacturer's limitation. You should manually terminate charge when the current falls to a low-enough level (varies depending on who you read) - excess charging can boil the electrolyte or cause significant bubbles to form in gel cells and loss of electrolyte causing permanent capacity reduction. For float based charging, 13.6-13.8V would be a better choice, some cells do not need current limiting under that condition and generally can sit there all the time without much degradation. The optimal voltage does vary slightly depending on ambient temperature.

    The main pitfalls are that a reversed connection will either kill the power supply or kill the internal reverse-connected bypass diode which will then kill the power supply. Another pitfall is that many power supplies don't have a true "switch" of the outputs, so connecting a battery can result in a spark as it charges up the output capacitors. When the power supply is off, any bleeder-resistors or down-programmers may end up discharging the battery slowly as well.

    But they're all pretty much no big issue. If you'd like, you could use a hefty external diode to keep the battery from draining into the supply but at the cost of heat and loss of voltage accuracy (unless using 4-wire connection). I personally just use a switch to isolate the battery and slam the switch shut after the supply is on and stabilised, opening the switch before turning it off.

    - Gough

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Gough Lui
    0 Gough Lui over 3 years ago

    You can certainly do this - usually for cycle-based charging, a safe voltage cap would be 14.4V with a current limit that matches the manufacturer's limitation. You should manually terminate charge when the current falls to a low-enough level (varies depending on who you read) - excess charging can boil the electrolyte or cause significant bubbles to form in gel cells and loss of electrolyte causing permanent capacity reduction. For float based charging, 13.6-13.8V would be a better choice, some cells do not need current limiting under that condition and generally can sit there all the time without much degradation. The optimal voltage does vary slightly depending on ambient temperature.

    The main pitfalls are that a reversed connection will either kill the power supply or kill the internal reverse-connected bypass diode which will then kill the power supply. Another pitfall is that many power supplies don't have a true "switch" of the outputs, so connecting a battery can result in a spark as it charges up the output capacitors. When the power supply is off, any bleeder-resistors or down-programmers may end up discharging the battery slowly as well.

    But they're all pretty much no big issue. If you'd like, you could use a hefty external diode to keep the battery from draining into the supply but at the cost of heat and loss of voltage accuracy (unless using 4-wire connection). I personally just use a switch to isolate the battery and slam the switch shut after the supply is on and stabilised, opening the switch before turning it off.

    - Gough

    • Cancel
    • Vote Up +8 Vote Down