Test & Tools
  • Technologies
  • More
Test & Tools
Forum Hot Air Tool Upgrade - Quick TR1300A
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 40 replies
  • Subscribers 383 subscribers
  • Views 11526 views
  • Users 0 members are here
  • TR1300A
  • HCT2-120
  • MP740784
  • st-862d
  • HCT2-200
Related

Hot Air Tool Upgrade - Quick TR1300A

shabaz
shabaz over 3 years ago


I’ve been really stuck for hot air tools for ages, every few months checking out the prices, and always giving up!

I decided to bite the bullet and purchase one. I wanted one with a spinning blower (i.e. not a noisy vibrating air pump), and with the blower in the main body of the unit, not integrated in the handle.

I considered these options:

(1) E-bay used JBC JT 6040 tool that looked like it was manufactured in the last century, for £250 (minimum bid, it could have gone higher), with a description that stated “..currently just gauging interest” (Edit: someone purchased that for £260 in the end)
(2) E-bay Weller tool WTHA 1  apparently "new without box", for £500 starting bid, at which it didn’t sell, but it’s now re-listed at a more sensible starting price (Edit: someone purchased that for £610 in the end)
(3) Quick 861DW, new, for £260 including delivery
(4) Atten ST-862D, new, for £190 including delivery
(5) Multicomp MP740784 , new, for £174 including delivery
(6) Quick TR1300A, new, for £320 including delivery

I was really close to choosing option (2), because it is a current model, and I would be able to buy accessories for it. However, £500 is just a bit too high at Xmas time (EDIT: it sold for £610 including delivery at the final bid by someone, so I'm glad I didn't wait the week bidding for it) especially since I would only use it intermittently because I can always fallback to doing some surface-mount work with a normal soldering iron, I prefer the soldering iron for the simpler components such as SOIC, TSSOP, etc. I wanted the hot air tool for the more complicated packaged components.

I ruled (1) out almost immediately, since perhaps the seller isn’t even sure what price to sell it at, and it all looked pretty ugly. Blowers and other parts can wear out, and it could be a nightmare to fix if/when it goes wrong.

I considered (4) and (5) to be near-similar options, and with hindsight, I should have chosen one of those. I didn’t at the time, because option (4) used a courier service that I wasn’t happy with, and option (5) was currently out of stock.

That left options (3) and (6). Since the price difference was not much between the two, I went with the newer model, i.e. option (6).

image

It’s a beast, absolutely huge. That’s a negative since it means I won’t keep it on the bench all the time. I’ve placed it on a mini-shelf because I just cannot see myself leaving it on the main desk surface with the fat hose covering a huge portion of the desk too. Now I can see why people would prefer an integrated soldering station and hot air station. Otherwise, it's just too much equipment footprint.

I used a laptop stand for the photo above, but I will replace that with a better stand when I use it, I've seen a little desktop speaker stand that will be ideal. I will probably put the Quick device away to keep the desk clear when I don’t need it.

I’ve not used it yet, I only powered it up and checked that the air and heat work. The display is great. The entire unit looks well built. The handle sometimes tends to stick in the stand, it doesn’t always easily lift out with one hand. That’s slightly annoying.


The nozzles are really nice, they click on and off nicely without a lot of effort, and I think they are identical to the Quick 861DW nozzles. The unit came with three straight nozzles, and I purchased a couple of angled ones from the same seller, they were very low-cost.


Just as a size comparison, the photo below shows the tiny Metcal HCT2-120 alongside the Quick unit. They are not really comparable in heating performance. The Metcal unit is used frequently, since it’s excellent for connectors/wires, for heat-shrink purposes. It’s like a super-accurate heat gun. There is a newer HCT2-200  model which would be a better choice than the HCT2-120 nowadays.

image


For the Quick unit, I will use it with a pre-heater – I have a very basic one called TMT-PH200. It uses quartz infra-red heating tubes, which tend to cook the face if you get too close to the board! I don't think I can recommend it. It's OK-ish for the price but that's it.

If anyone needs the info, I got the Quick TR1300A from the seller in the screenshot below:

image

But, if one really doesn't have the desk space and needs a hot air tool, then I believe the Atten or Multicomp products would be a far better option, (for occasional work, otherwise something like Weller/Metcal/JBC would be preferred!),  since the ST-862D has excellent reviews. If you have other suggestions, it would be great to hear them, since everyone needs to find ways of working with surface-mount parts at some stage.

Thanks for reading!

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 3 years ago +7
    A little demo of how I unsolder and resolder SMDs with hot air https://youtu.be/1MWqME8EeVE Filmed with a web cam that has a hard time focusing. Forgot to turn on the microphone, so did a talk over…
  • Gough Lui
    Gough Lui over 3 years ago in reply to shabaz +4
    Oddly enough, at the time, the combined station was the cheaper option, lest I get one of those wretched "fan-based" hot air guns which aren't so stable at low flow rates. They do work, but it just doesn…
  • Andrew J
    Andrew J over 3 years ago +3
    I have an Atten one and it’s been great so far, about the size of the Metcal one. I csn/have hand soldered SOIC etc as well, but now I just get a stencil with the boards I order and use this with a pre…
  • shabaz
    shabaz over 3 years ago in reply to Jan Cumps

    Hi Jan,

    The integrated iron+hot air is awesome. Really practical for keeping desk space usage to a minimum.

    I too like the pencil format, the little Metcal unit has a handle that is thinner than some soldering irons. I wish that was higher-powered since it's just 120W. It seems once the output power goes about 800W or so, then the hoses and handles all get considerably fatter, so a tool that's got power just below that seems ideal for use and for ergonomics.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to Andrew J

    Awesome. I'll try that ballpark temperature, and a low flow rate on a scrap PCB today. Excited to try it out : )

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 3 years ago in reply to Jan Cumps

    An area of electronics I have ZERO exposure and less knowledge. Thanks for the share.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago

    Very nice purchase! Congrats! I have one of these and its definitely nothing fancy but it works!

    image

    Just took a chip off

    image

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 3 years ago

    Just over a year ago, I bought an Aoyue 852A. I really like it. In terms of the hot air tool and tips, it looks similar to the Quick TR1300A. My only real issue with it is the controls for fan and temperature--especially temp.

    I really wish it had a knob instead of buttons to adjust the settings.

    I do not have a pre-heater / heating plate. So I'll start at a relatively low temperature, like 150C, to soak the PCB. And then, when I'm ready to reflow, I crank up the temperature. But the push button/digital controls are clunky.

    I'm also fortunate to have a Weller WXR-3 with its hot air tool and rework kit. It is really nice, small, and compact. But when I just want brute-force heat, the Aoyue unit works great.

    That said, it is relatively large. And it does make a significant amount of noise. But it does a great job of melting anything you need.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • genebren
    genebren over 3 years ago

    Thanks for sharing!  This really sounds a lot like my own search for a good hot air station.  I look and I look, but I have still not mad the leap to buy one (at least you have gotten farther down the road).  I will have to look again with fresh eyes and greater knowledge based on yours and others experience, triggered by your post.

    This is the true power of our wonderful community.  One brave soul makes a move, then others share their moves, and suddenly a whole bunch of others get a lot of valuable advice and knowledge.  Thank you all for sharing!

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago in reply to baldengineer

    My Aoyue 906 has control knobs and an iron. It has been working well for 18 years.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago

    One tool definitely not recommended is this ZD-939A. It's underpowered (300W) and the pump died after a couple of years of very lightweight work.

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • hlipka
    hlipka over 3 years ago

    I do have a Quick 861DW, and I was very surprised how quiet it it is. I had a ZD-939L before (which is sold under many different names), and the difference is beyond belief. The Quick is much more powerful and so much nicer to use that I really regret not buying it earlier.

    The only reason I did not buy the TR1300 was that it actually has even more power, and with all the tools at my workplace I was afraid to trip the circuit breaker...

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to genebren

    I was expecting prices to have shot up, but it was nice to see fairly recent models at OK prices. It was a bit of a gamble spending so much on a unit that I would find hard to return if it was faulty, but in the end it worked out smoothly. From order to delivery was 6 days (actually quicker than a pair of gloves I ordered nationally from a UK store.. I'm still waiting for those, they have not even been dispatched! customer focus is not great here : ).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
<>