Test & Tools
  • Technologies
  • More
Test & Tools
Forum What's your favorite through-hole desoldering tool?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 42 replies
  • Subscribers 382 subscribers
  • Views 10593 views
  • Users 0 members are here
Related

What's your favorite through-hole desoldering tool?

scottiebabe
scottiebabe over 3 years ago

I have a $5 solder sucker that is nothing fancy for desoldering through hole components. For occasional use it works well enough I suppose.

image

There appears to be a number of "fancier" solder suckers on the market like this made in japan model:

image

There are also some inexpensive vacuum desoldering tools, like:

image

I don't know if it is total junk or a diamond in the rough...

  • Sign in to reply
  • Cancel

Top Replies

  • scottiebabe
    scottiebabe over 3 years ago +4
    There also appears to be heated suckers: I didn't know they even existed...
  • Andrew J
    Andrew J over 3 years ago +3
    I use this: https://cpc.farnell.com/duratool/d00672/desoldering-station-uk-eu-plug/dp/SD01384 It works pretty well and I've desoldered lots of stuff off prototype boards to reuse. I think Multicomp…
  • beacon_dave
    beacon_dave over 3 years ago in reply to Andrew J +3
    Perhaps take a look at: /challenges-projects/element14-presents/workbenchwednesdays/w/documents/5300/workbench-wednesdays-37-desoldering-wick-tips-and-tricks-with-superwick?ICID=workbenchwed-episode…
  • maxpowerr
    maxpowerr over 3 years ago

    I use this desoldering pump.

    image

    Here is an example of how I tried to solder the VGA connector. First, I had to tin the contacts with low-temperature solder and then use a desoldering pump.

    image

    In some places, for some reason, it was not possible to remove the solder and therefore I had to use a soldering dryer. But in principle, for its price, this desoldering pump copes with its task.

    imageimage

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago in reply to maxpowerr

    How am I the last person to hear about these heated suckers... That's wonderful! Thanks for sharing. Desoldering anything out of a PC motherboard is very challenging with all the thermal mass of the internal ground planes, I'm amazed you were able to get the connector out!

    Thanks again for sharing your technique.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 3 years ago in reply to baldengineer

    ChipQuik is a good option to keep from applying to much heat and keeping the area clean, but it definitely needs to be removed before making a new joint with higher temperature solder.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to scottiebabe

    Hi,

    I think they're the same thing, or perhaps there is not a very significant difference (but I'm not sure, since the ChipQuik formulation is not advertised). 

    Incidentally, the bismuth solder is also available in paste form, so that's another option (at least for me where I am, it was cheaper to buy more paste than the solder wire. Also, not really related, but the paste may come in handy for general prototype soldering of difficult components, i.e. use it as if it were normal solder paste, but just happens to melt at a lower temperature. No good for most production, but it might get one out of some difficulties occasionally. That's not as easy with the solder wire form, because it's a thick wire (the thinner bismuth wire is expensive here).Not an issue for desoldering of course. I still have issues with some components however, because some component leads are almost exactly the same diameter as the through-hole, so it's difficult to make the solders mix there. But it was awesome for removing SOIC chips which is yet another moot point since the discussion's supposed to be through-hole! : )

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • baldengineer
    baldengineer over 3 years ago in reply to scottiebabe

    “Low-temp solder” comes in (at least) two alloys. One is Bismuth-based and the other is Indium. I have a lot more experience with Bismuth. If you’re re-working a SnPb board, the Lead(Pb) will drop the Bismuth-alloy’s melting point down as low as 100C. 

    This is great for removal, but could be a potential issue in the future. So it is recommended to clean the Bismuth as best as possible before re-soldering (with SnPb.)

    Indium seems to have an opposite effect. The couple of times I tried to use Indium-alloy, I had a heck of a time getting SnPb to melt. (With the Bismuth-alloy, I’ve had 20-pin DIPs fall out of the board without me pushing!) The people watching use it said I didn’t remove enough of the SnPb to make the Indium-alloy effective.

    So, my suggest is stick to the Bismuth-based alloy.

    ChipQuik sells both. They should have a datasheet on their site to say which is which. (Though, I think those SMD removal kits are usually the Bismuth one.)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • colporteur
    colporteur over 3 years ago

    image

    I was formally trained on a PACE system but for my limited home workshop projects the blue tube that sucks (not an MS product) has a spot on the bench.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 1 year ago in reply to scottiebabe
    scottiebabe said:
    I wish the braid spool was heat resistant perhaps other suppliers are:

     scottiebabe The Xuron WickGun Desoldering Braid Dispensers are the best you can get. I managed to find four guns and a lot of cassettes a long time ago.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 1 year ago

    scottiebabe Shop air powered Weller WDD80V and DSV80.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • KC7HP
    KC7HP over 1 year ago in reply to anniel747

    I followed the general progression described by others.

    I used an older Ebay weller station (with on-board vacuum pump). It worked long enough that parts were not available when it finally died.  It worked so nice I payed the money for a new one, for hobby use.

    I pick old solder out of the filter cartridges until the fiber pad disintegrates.  I also save the cardboard tube to recycle with my padding, when I finally use up the current supply of filters.

    It can be hard to hit the temperature sweet-spot with production no-lead solder.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • anniel747
    anniel747 over 1 year ago in reply to KC7HP

    Nice thing about the DSV80; it uses a reusable glass solder collection chamber. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>