Test & Tools
  • Technologies
  • More
Test & Tools
Forum Multimeters everywhere all at once - Viewing multiple BLE meters on desktop or mobile
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 13 replies
  • Subscribers 384 subscribers
  • Views 4384 views
  • Users 0 members are here
  • bluetooth
  • ble
  • mp730026
  • multimeters
  • bluetooth le
  • dmm
  • multimeter
  • MP730624
Related

Multimeters everywhere all at once - Viewing multiple BLE meters on desktop or mobile

shabaz
shabaz over 3 years ago

Finally having two Bluetooth (BLE) multimeters to try this, it was interesting to see if they could both be used simultaneously! This could be handy to monitor voltage and current together for instance.

Of course, I shouldn't be surprised that more than one BLE device can be used at any one time, but still, it's good to test new code to confirm its functioning. I don't know in practice how many BLE connections Windows supports simultaneously, but I'm guessing it's a reasonable amount. I was using my BLE mouse at the same time as well.

image

In the screenshot above, one multimeter is model MP730026 and the other is MP730624 (discussed here:  MP730624 Multimeter Quick Review: Surprisingly Accurate!   ), and each one is using their own app, but I see no reason why the same multimeter models could not be used.

These are the apps: MP730026 app , MP730624 app

One benefit of BLE is that new functions can be added that do not already exist on the physical device. For model '624, the app now has a Statistics view; it would be nice to extend that view further with a little histogram chart too! I don't know why handheld multimeters do not offer that:

image

I think the statistics is working OK, but it probably needs a bit more testing before I can be sure.

Incidentally, it is possible to view multiple multimeters on a mobile phone too, but it is visually messy. It ideally needs a single app. The screenshot below shows on the right what the BLE connections look like when adding a second meter to either mobile or desktop.

image

  • Sign in to reply
  • Cancel

Top Replies

  • aspork42
    aspork42 over 3 years ago +4
    Fluke has their bluetooth-enabled meters and add-on modules. I am fortunate enough (through Element14 contests) to have two different meters which were Fluke Connect compatible and the app was able to…
  • shabaz
    shabaz over 3 years ago in reply to Jan Cumps +3
    Time to steal the best ideas from each multimeter app! It would be awesome to have a temperature display, but the Multicomp meter doesn't support it sadly. For the chart view, in this mockup I've placed…
  • baldengineer
    baldengineer over 3 years ago +2
    Shabaz, I think we need to talk. You might have a DMM BLE addiction problem. Just kidding. I really like the idea of extending low-cost DMMs with statistical tools. With BLE enabled, I know my Multicomp…
Parents
  • Jan Cumps
    Jan Cumps over 3 years ago

    A utility that matches well with multimeter windows, is Microsoft's PowerToys Always on Top. I swear I didn't make up that name.

    You can select one or more windows that will stay on the top of the screen stack.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 3 years ago in reply to Jan Cumps

    Hi Jan,

    That's very neat! I was searching for something similar, and was looking at creating widgets, apparently that's possible by modifying a file, but that requires work which I really don't want to start. The method you mention doesn't require any changes, which suits me much better.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 3 years ago in reply to Jan Cumps

    Hi Jan,

    That's very neat! I was searching for something similar, and was looking at creating widgets, apparently that's possible by modifying a file, but that requires work which I really don't want to start. The method you mention doesn't require any changes, which suits me much better.