Test & Tools
  • Technologies
  • More
Test & Tools
Forum TENMA 72-13210 & Python UDP
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 8 replies
  • Subscribers 380 subscribers
  • Views 4126 views
  • Users 0 members are here
Related

TENMA 72-13210 & Python UDP

cfauvel
cfauvel over 3 years ago

Hi everyone,

Does anyone has been able to send UDP commands to a TENMA 72-13210 Power Load using a python 3.0 script ?

When I send an UDP command (*IDN? for example), I am unable to retrieve data from the UDP socket.

Best regards,

import os, sys
import re, string
import socket
import time
import logging


# Register logs from the module to the
# root logs
logs = logging.getLogger(__name__)




"""
    Power load class
"""
class Load():
    """
        Initialize everything
        @param  context     instrument context (ie. ip and port)
        @param  timeout     instrument timeout
        @return             none
    """
    def __init__(self,
                 context,
                 timeout = .5):
        # Open a pyvisa ethernet link to control the
        # power load
        try:
            self.ip = context['ip']
            self.port = context['port']
            logs.info("Open load (ip: %s, port: %d)" % (context['ip'],
                                                        context['port']))
        except:
            logs.error("Unable to open load (ip: %s, port: %d)" % (context['ip'],
                                                                   context['port']))

        # Configure power load by reading it's identifier
        # and resetting the device
        self.timeout = timeout
        print(self.query('*IDN?'))
        try:
            self.query('*REBOOT')
            time.sleep(1)
        except:
            logs.error("Unable to retrieve load identifier")
            logs.error("Ensure that load is VISA capable !")

    """
        Write function
        @param  self        object pointer
        @param  data        data command
        @return             none
    """
    def write(self, data):
        self.dev.sendto(data.encode(), (self.ip, self.port))
        logs.debug("Send data: %s" % data)

    """
        Read function
        @param  self        object pointer
        @return             data command
    """
    def read(self):
        try:
            data = self.dev.recv(64)
            print(data, server)
            logs.debug("Receive data: %s" % data)
            return data
        except:
            pass
           
    """
        Query function
        @param  self        object pointer
        @param  data        data command
        @return             data command        
    """
    def query(self, data):
        self.dev = socket.socket(socket.AF_INET, socket.SOCK_DGRAM)
        self.dev.connect((self.ip, self.port))
        self.dev.settimeout(self.timeout)
        self.write(data + '\n')
        return self.read()




if __name__ == "__main__":
    load = Load(context = { 'ip' : "172.16.169.70",
                            'port' : 18190 })
  • Sign in to reply
  • Cancel

Top Replies

  • cfauvel
    cfauvel over 3 years ago in reply to baldengineer +3 verified
    Hi everyone, The TENMA 72-13210 doesn't support TCP/IP protocol, as stated in the datasheet, only UDP or serial connection can be used to control the device. I have already used PyVISA to send an IDN…
  • cstanton
    cstanton over 3 years ago in reply to cfauvel +2
    Fyi UDP is a part of the TCP/IP protocol. Funny the EEVBlog thread also links back to the element14 Community :D Need Windows USB Driver for TENMA 72-13210 (electronic dc-load 30A/120V 300W) But it…
  • cfauvel
    cfauvel over 3 years ago in reply to baldengineer +2
    In fact it's really easy with UDP and raw python sockets. I use the code below : """ Write function @param self object pointer @param data data command @return none """ def write ( self…
Parents
  • Jan Cumps
    0 Jan Cumps over 3 years ago

    Can you try to connect to it via PyVISA, and then send that *IDN? command?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Jan Cumps
    0 Jan Cumps over 3 years ago

    Can you try to connect to it via PyVISA, and then send that *IDN? command?