Test & Tools
  • Technologies
  • More
Test & Tools
Forum Seeking Feedback - How often have you used a Low Resistance Micro-Ohmmeter?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 21 replies
  • Subscribers 383 subscribers
  • Views 4876 views
  • Users 0 members are here
  • low resistance mirco-ohmmeter
Related

Seeking Feedback - How often have you used a Low Resistance Micro-Ohmmeter?

rscasny
rscasny over 2 years ago

If you have the time, I'd appreciate if you voted in this poll. I'd like to get a sense of your need and use of low resistance micro-ohmmeters. Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • kmikemoo
    kmikemoo over 2 years ago in reply to rscasny +4
    rscasny Younger me used to use them to measure contact resistance on high voltage switchgear (aka circuit breakers) and transfer switches. Older me uses it to measure rotor and stator winding resistance…
  • shabaz
    shabaz over 2 years ago +4
    I can imagine them being extremely handy for measuring electrical contacts, such as relays to examine if they are failing, or for checking the resistance quality of shielding or grounding between different…
  • shabaz
    shabaz over 2 years ago in reply to beacon_dave +4
    Interesting use! Maybe the inductance may be an issue, although some meters may be more stable than others. Presumably the industrial meters are more immune to that. Also, some meters may use a slow…
  • rsc
    rsc over 2 years ago

    I've used bridge circuits to measure hot film and nano wire probes.  At Bosch we used them to measure relay contact resistance.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 2 years ago in reply to shabaz

    I've wondered if one could be used to monitor the condition of copper AFILS loop tapes. One of the problems I often see is water ingress rapidly corroding them due to the close proximity to concrete. (Another is damage from carpet fitters knives during carpet repairs.) However they are often laid under expensive floor coverings which makes routine inspection difficult and expensive. Being able to monitor the condition routinely would allow for scheduling a repair before it failed completely.

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago in reply to beacon_dave

    Interesting use! Maybe the inductance may be an issue, although some meters may be more stable than others. Presumably the industrial meters are more immune to that.

    Also, some meters may use a slow AC measurement I guess, although others use DC (such as Frank's one). That might not be an issue though.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • strb
    strb over 2 years ago

    I've never used one. Once I had to check copper thickness on a prototype board and I used a resistance measurement (1A current from a lab power supply and measured voltage drop with a multimeter) to indirectly calculate the overall copper amount. I guess it would've been useful in that situation!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • michaelkellett
    michaelkellett over 2 years ago

    I've never had one but have measured low resistance by 4 wire method using power supply (to provide current) and DMM to measure voltage drop on a few occasions.

    I don't do much high current work so I've not often been interested in measuring very low remittances.

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • three-phase
    three-phase over 2 years ago

    I have used high-current versions a lot for measuring bolted connections on busbars and contacts on breakers. I have used them on motor and generator windings but you are getting more into the milli-ohm range and the test current gets reduced, although some manufacturers have brought out high current units to meet these demands. Earth testers also use the 4-wire resistance method as well, but again milli-ohms range, they can both AC and DC. Finally, I use battery resistance testers, such as the Hioki BT3554 that I reviewed some time ago, again more in the milli-ohm range and uses AC rather then DC.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • scottiebabe
    scottiebabe over 2 years ago

    When I hear micro-ohm meter I think of those 40A continuity tester boat anchors not something like

    HIOKI RM3545 Resistance Meter

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 2 years ago in reply to kmikemoo

    transformer winding resistance too. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 2 years ago

    Not really micro-ohms, but I needed a couple of 450 milliohm resistors today, and just wound a bit of resistance wire (I calculated resistance, but verified with the milliohm meter). 

    image

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • dang74
    dang74 over 2 years ago

    I voted never.  I've only used the 'regular' ohmmeter setting on multimeters.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>