Test & Tools
  • Technologies
  • More
Test & Tools
Forum Tenma 72-7732A Comport / HID
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 384 subscribers
  • Views 1437 views
  • Users 0 members are here
Related

Tenma 72-7732A Comport / HID

Zacory
Zacory over 2 years ago

Hello,

I'm trying to write a Python Script that reads the output of Tenma 72-7732A Digital Multimeter, while I am aware of the software that comes with it on the installation disk, I want a Python Script.

When plugging in the Optical to USB lead into the machine, it appears as a "HID Vendor Compliant Device" not as a comport. 

I have attempted to read the USB, all I get is B[0,0,0,0,0,0]

I am wondering if anyone has successfully read this device with Python, as a comport or as a HID Device?

Thank you!

  • Sign in to reply
  • Cancel

Top Replies

  • cstanton
    cstanton over 2 years ago in reply to Zacory +1
    Hey Zacory Zacory said: Like I said in the post, "not as a comport" - the pyTenma software looks for a comport I'm sure aswinvenu was replying with this because: Zacory said: I am wondering if anyone…
  • battlecoder
    battlecoder over 2 years ago +1
    HID devices communicate exchanging "reports" which are just blocks of bytes. The Operating system can query their "Report Descriptor" which should tell the kind of device it is, the "endpoints" and the…
  • aswinvenu
    aswinvenu over 2 years ago

    https://github.com/swharden/pyTENMA

    Maybe this helps.!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Zacory
    Zacory over 2 years ago in reply to aswinvenu

    Like I said in the post, "not as a comport" - the pyTenma software looks for a comport Slight smile

    Thank you though

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • cstanton
    cstanton over 2 years ago in reply to Zacory

    Hey Zacory

    Zacory said:
    Like I said in the post, "not as a comport" - the pyTenma software looks for a comport 

    I'm sure aswinvenu was replying with this because:

    Zacory said:
    I am wondering if anyone has successfully read this device with Python, as a comport

    So maybe there's some hint in that code and you can change the way Python interrogates the device. 

    From my limited expertise I wouldn't expect a HID component to communicate in this way, and I would expect this to be a problem with the driver installed, assuming you're using windows, and it needing a replacement driver?

    You can find the windows software/driver here:

     Tenma 72-7732 Windows 7 Software 

      Tenma 72-7732A software win10.zip  

    I'd confirm that by looking at how the device identifies under Linux, maybe with a liveUSB (I appreciate you don't explicitly state what operating system you're using).

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • battlecoder
    battlecoder over 2 years ago

    HID devices communicate exchanging "reports" which are just blocks of bytes. The Operating system can query their "Report Descriptor" which should tell the kind of device it is, the "endpoints" and the sizes of the reports for input and output. They are not as simple as just sending bytes down the line, unfortunately.

    Now, if you are willing to do the reverse engineering of the protocol yourself, there's a library for Python called pyhidapi that would allow you to connect to the device and read and write these reports. Now, you will probably also need a tool that allows you to dump the report descriptor from the device, to see the structure of the reports (which will depend on what operating system you are running), or better yet, you can set up a USB monitoring tool to capture the reports sent back and forth between the device and the official software to get an idea of what is being sent or received.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • battlecoder
    battlecoder over 2 years ago in reply to cstanton

    This could also be the case. Sometimes devices will not show up in windows as comm ports until you install their driver.