Test & Tools
  • Technologies
  • More
Test & Tools
Forum Tektronix Unveils Complete Solution for Volume, Surface Resistivity Measurements
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 385 subscribers
  • Views 319 views
  • Users 0 members are here
  • keithley tektronix surface rsistivity measurement
Related

Tektronix Unveils Complete Solution for Volume, Surface Resistivity Measurements

prisma
prisma over 9 years ago

image

Tektronix Unveils Complete Solution for Volume,
Surface Resistivity Measurements

New Software Application Controls Keithley Test Instrumentation, Fixtures, Paving
the Way to Faster, More Accurate and Repeatable Material Characterization

 

BEAVERTON, Ore. Nov. 29, 2016 – Tektronix, Inc., a leading worldwide provider of measurement solutions, today unveiled a complete solution for performing high resistivity measurements in compliance with accepted industry standards including ASTM D257 and IEC 60093. Designed for use with the Keithley Model 6517B Electrometer and Model 8009 Resistivity Chamber, the new Model KICKSTARTFL-HRMA application automates volume and surface resistivity measurements for more accurate and repeatable results without the need for custom programming.

Material scientists and engineers use resistivity measurement to verify the electrical properties of insulating and other materials they are developing or evaluating. However, they tend to be materials experts rather than test equipment experts and need tools that allow them to characterize materials without having to learn how to program test instrumentation. The KICKSTARTFL-HRMA application requires no programming and performs all required computations based on the geometry of the Keithley test fixture.

“High resistivity measurements are critical to evaluating not just electrical insulating materials, but many other materials. For instance, the resistivity of materials used in the production of car tires is important in balancing electrostatic discharge safety with properties that affect rolling friction,” said Mike Flaherty, general manager, Keithley product line at Tektronix. “With this solution we are making these measurements much easier than they have ever been in the past, allowing our customers to focus on what they do best – developing new and improved materials for all types of applications.”

The KICKSTARTFL-HRMA application quickly and reliably allows users to determine resistivity of materials using setups and methods consistent with ASTM D257 and IEC60093 standards. Users can visualize the step response of the material and make a good decision on an appropriate test time to use for volume or surface resistivity testing. For improved accuracy, the software uses the Keithley alternating polarity measurement technique to eliminate inherent background currents. And, using optional probes, users can also observe how resistivity changes due to environment factors such as temperature or humidity. Resulting data is presented in both graphical and tabular formats.

Pricing & Availability

An option for Keithley KickStart Instrument Control Software, the Model KICKSTARTFL-HRMA is available now and priced at € 449. The full high-resistivity measurement solution includes Kickstart software, a Model 6517B Electrometer, and Model 8009 Resistivity Chamber. For more information go to: http://www.uk.tek.com/keithley-kickstart.

 

Wondering what else Tektronix is up to? Check out the Tektronix Bandwidth Banter blog and stay up to date on the latest news from Tektronix on Twitter and Facebook.

###

About Tektronix

Headquartered in Beaverton, Oregon, Tektronix delivers innovative, precise and easy-to-operate test, measurement and monitoring solutions that solve problems, unlock insights and drive discovery. Tektronix has been at the forefront of the digital age for over 70 years. Join us on the journey of innovation at TEK.COM. In 2010, Keithley Instruments joined Tektronix as part of its test and measurement portfolio.

Tektronix

Petra Quaedvlieg

Phone: +49-221 94 77 277

  1. petra.quaedvlieg@tektronix.com
  2. www.tektronix.com

 

Editorial Contacts:

PRismaPR (UK)

Monika Cunnington

Phone: +44-20 8133 6148

monika@prismapr.com

  1. www.prismapr.com

 

PRismaPR

Gabriele Amelunxen

Phone: +49-8106-24 72 33

info@prismapr.com

  1. www.prismapr.com