Test & Tools
  • Technologies
  • More
Test & Tools
Forum Tektronix Boosts PRISM Platform Capabilities for Monitoring Hybrid IP/SDI Infrastructure
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 0 replies
  • Subscribers 385 subscribers
  • Views 160 views
  • Users 0 members are here
Related

Tektronix Boosts PRISM Platform Capabilities for Monitoring Hybrid IP/SDI Infrastructure

prisma
prisma over 9 years ago

image

 

 

Tektronix Boosts PRISM Platform Capabilities for Monitoring Hybrid IP/SDI Infrastructure

New Software Updates Ease Hybrid Facility Operations, Enhances IP Video Network Quality; 4K/HDR and 12G-SDI Support to Be Previewed at NAB 2017

 

BEAVERTON, Ore., April 3, 2017 – Tektronix, Inc., an industry-leading innovator of video test and monitoring solutions, today released a series of enhancements to PRISM, the industry’s first software-based hybrid IP and SDI media analysis platform. The new features added to the PRISM platform include support for important industry specifications and help engineers boost IP video network quality, conquer integration and operations challenges and perform deep-dive analysis for troubleshooting. The platform is now also available in a 1RU form factor for use with external displays to complement the current 3RU product which has a built-in display.

New enhancements to be demonstrated at NAB 2017 April 22-27, 2017 in Las Vegas (booth #SU5006) include analysis of PTP synchronization timing, support for SMPTE ST 2022-7 redundancy, IGMP V3 and new API support for easy system integration into network management systems, and IP stream capture for deep dive analysis. These are in addition to the Packet Interval Time (PIT) histogram and trend graph as well as the trend graph of Time Stamped Delay Factor (TS-DF) as per EBU-TECH 3337 that are currently available on PRISM. These real time IP measurement capabilities assist broadcast and IT engineers quickly and easily troubleshoot the root causes of IP network issues.

“As the broadcast industry goes through the IP transition, engineers need to manage an increasingly complex and evolving hybrid IP and SDI environment,” said Charlie Dunn, general manager, Video Product Line, Tektronix. “PRISM is the first software-based platform with field upgradeability that offers customers long-term investment protection as technology and requirements evolve.”

“With easy to understand graphical displays, it helps engineers quickly get the information they need to troubleshoot IP network issues and related content layer issues to assure delivery of high quality content,” Dunn added. “The platform is seeing strong global industry adoption with one example being Globosat who used PRISM to support live IP media production at the 2016 Summer Olympic Games in Rio de Janeiro.”

In addition to the new enhancements for IP production facility applications, Tektronix will also demonstrate at the NAB Show, for the first time, 4K format support over quad-link 3G-SDI and single link 12G-SDI with High Dynamic Range (HDR) on PRISM for content acquisition and post production applications. The demonstration will also include eye pattern measurements for 12G-SDI interfaces for signal integrity verification.

Availability

The PRISM software feature enhancements including SMPTE ST 2022-7, IGMP V3 and new API support, PTP timing analysis, and IP stream capture are available now. The 1RU form factor is available for order now with shipment expected in June. The expanded SDI support as previewed at NAB will be available in the second half of 2017.

 

Wondering what else Tektronix is up to? Check out the Tektronix Bandwidth Banter blog and stay up to date on the latest news from Tektronix on Twitter and Facebook.

About Tektronix

Headquartered in Beaverton, Oregon, Tektronix delivers innovative, precise and easy-to-operate test, measurement and monitoring solutions that solve problems, unlock insights and drive discovery. Tektronix has been at the forefront of the digital age for over 70 years. Join us on the journey of innovation at TEK.COM.

# # #

Tektronix is a registered trademark of Tektronix, Inc. All other trade names referenced are the service marks, trademarks or registered trademarks of their respective companies.

Media Contact:

 

Tektronix

Petra Quaedvlieg

Phone: +49-221 94 77 277

  1. petra.quaedvlieg@tektronix.com
  2. www.tektronix.com

 

Editorial Contact:

 

PRismaPR

Gabriele Amelunxen

Phone: +49-8106-24 72 33

info@prismapr.com

  1. www.prismapr.com