Test & Tools
  • Technologies
  • More
Test & Tools
Forum Cool Tools To Giveaway for a Blog Review
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 117 replies
  • Subscribers 403 subscribers
  • Views 18350 views
  • Users 0 members are here
  • scasny
Related

Cool Tools To Giveaway for a Blog Review

rscasny
rscasny over 8 years ago

I kind of figured that anyone who considers him or herself a maker has a toolbox or a bench of tools they treasure. When I did technical work, I had my big tool box and a briefcase of my go-to tools, including a multimeter, driver set, sockets, extender magnet, etc. These were my cool tools. What are yours?

 

We are launching a cool tools campaign at element14 where we roadtest and giveaway some tools we think are pretty cool.

 

Cool Tools Giveaway for a Blog Review

Would you like to get any of these tools, play around with them, and write a blog review? I'm looking for a few members who are really into tools to do the reviews. Below are the tools I have to offer. If you are interested, drop me a line in the comments below. Tell me about your cool tools and persuade me to send you off any of these tools. And all you need to do for it is write a blog review on element14.


image

Milwaukee Tool 60-piece Shockwave Series Impact Driver Set

 

image

Leatherman 14 in 1 Multitool

 

image

Bit Set, Zyklop Mini Series

image

 

Peak Electronics ESR Meter (Capacitance)

 

image

Duratool PC Maintenance Tool Kit

  • Sign in to reply
  • Cancel

Top Replies

  • ipv1
    ipv1 over 8 years ago +16
    I started with 'making'(tearing down) stuff at a tender age and have gone through a lot of stuff. Unfortunately, I lost a big chunk of my tools in a burglary years ago and am left with only a large hammer…
  • jw0752
    jw0752 over 8 years ago +15
    My favorite tools are the ones that I have performed modifications on. When you twist a tool to your own purposes you make a special bond with it. Here are three of the tools which I have modified to do…
  • rsc
    rsc over 8 years ago +13
    This is my favorite tool, circa 1912:
Parents
  • shabaz
    shabaz over 7 years ago

    I can't believe I didn't think of this before, but I've decided to take up color-coding drill bits : )

    I'm using redred and green marker pensgreen marker pens, since they are the most popular fractional parts that I use. As per the resistor color code, I'll use red paint (red=2) for an X.2mm drill bit, and green=5 paint for a X.5mm bit.

    Therefore, the photo shows an 8.5mm drill bit in my 8.Xmm storage bin.

    I'm painting close to the flutes (so the marker paint doesn't wear off on the chuck) and painting at the end of it too.

    imageimage

    It would be cool to paint the entire value using multiple color bands, but just maybe that's taking it too far : )

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 7 years ago in reply to shabaz

    Cool idea. The color code is burned into my brain.

    Of course I use mostly English drills - not so amenable to color coding.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to dougw

    Ahh you're right.. not as easy then : (

    I needed a 7/32" hex bit a couple of weeks ago, and even the large DIY stores here don't stock the English sizes at all : (

    They have L sets (allen keys) but I can't get as much torque out of that compared to a bit in a ratchet driver, and the bolt was really stiff.

     

    In the end, I bought a cheap 6mm bit, put it in the vise, and filed the six surfaces down! Since 7/32" is 5.5mm.

    It worked, so now I do have a 7/32" bit : )

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 7 years ago in reply to dougw

    Ahh you're right.. not as easy then : (

    I needed a 7/32" hex bit a couple of weeks ago, and even the large DIY stores here don't stock the English sizes at all : (

    They have L sets (allen keys) but I can't get as much torque out of that compared to a bit in a ratchet driver, and the bolt was really stiff.

     

    In the end, I bought a cheap 6mm bit, put it in the vise, and filed the six surfaces down! Since 7/32" is 5.5mm.

    It worked, so now I do have a 7/32" bit : )

    • Cancel
    • Vote Up +5 Vote Down