Test & Tools
  • Technologies
  • More
Test & Tools
Forum Cool Tools To Giveaway for a Blog Review
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 117 replies
  • Subscribers 403 subscribers
  • Views 18338 views
  • Users 0 members are here
  • scasny
Related

Cool Tools To Giveaway for a Blog Review

rscasny
rscasny over 8 years ago

I kind of figured that anyone who considers him or herself a maker has a toolbox or a bench of tools they treasure. When I did technical work, I had my big tool box and a briefcase of my go-to tools, including a multimeter, driver set, sockets, extender magnet, etc. These were my cool tools. What are yours?

 

We are launching a cool tools campaign at element14 where we roadtest and giveaway some tools we think are pretty cool.

 

Cool Tools Giveaway for a Blog Review

Would you like to get any of these tools, play around with them, and write a blog review? I'm looking for a few members who are really into tools to do the reviews. Below are the tools I have to offer. If you are interested, drop me a line in the comments below. Tell me about your cool tools and persuade me to send you off any of these tools. And all you need to do for it is write a blog review on element14.


image

Milwaukee Tool 60-piece Shockwave Series Impact Driver Set

 

image

Leatherman 14 in 1 Multitool

 

image

Bit Set, Zyklop Mini Series

image

 

Peak Electronics ESR Meter (Capacitance)

 

image

Duratool PC Maintenance Tool Kit

  • Sign in to reply
  • Cancel

Top Replies

  • ipv1
    ipv1 over 8 years ago +16
    I started with 'making'(tearing down) stuff at a tender age and have gone through a lot of stuff. Unfortunately, I lost a big chunk of my tools in a burglary years ago and am left with only a large hammer…
  • jw0752
    jw0752 over 8 years ago +15
    My favorite tools are the ones that I have performed modifications on. When you twist a tool to your own purposes you make a special bond with it. Here are three of the tools which I have modified to do…
  • rsc
    rsc over 8 years ago +13
    This is my favorite tool, circa 1912:
  • three-phase
    three-phase over 8 years ago in reply to ntewinkel

    If you find yourself cutting up a lot of sheets then I can recommend investing in a track/plunge saw. Absolutely amazing pieces of kit, fast and accurate to use. The one I actually purchased was a Dewalt kit, but there are plenty out there.

     

    image

    Cutting a sheet lengthways, you have to join the two pieces of track together and the cut can be made without clamping the track down. I have however found the track joiner a little awkward to remove sometimes. Cutting across a sheet using only one section of track, I have found that the track can move, so I clamp the track to the work piece. The downside to the kit, is that it doesn't come with the special track clamps that fit into the bottom T-slot.

     

    Kind regards

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Cancel
  • s2000gt
    s2000gt over 8 years ago in reply to rscasny

    I would like to give the rotary set a go.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 8 years ago

    I'm looking for someone to review this one:

     

    image

     

    To review, sign up here:

     

    Cool Tools: Weatherproof Equipment Case

    • Cancel
    • Vote Up +6 Vote Down
    • Sign in to reply
    • Cancel
  • rscasny
    rscasny over 8 years ago

    I'm looking for someone to review this one:

     

     

    image

     

    If you are interested in reviewing it, go here:

    Cool Tools:  Pen Type Digital Multimeter

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
  • shunty85
    shunty85 over 8 years ago

    Hi Mate,

    As an industrial sparky, I'm always looking at getting a job done in extreme situations in the quickest time possible. Almost all these tools would be amazing in my growing arsenal of "quick response" tools. At the moment I have a tool bag that I need to carry around that has my immediate tools. Which is where the Milwaukee shockwave set would come in handy to sit next to my Milwaukee 12v impact driver. Some times when I have left my bag at a job to go and grab materials I need a knife, a driver, pliers or another tool to open a box or check terminals on a motor. This is where the Leatherman would be perfect and I would be able to run it to it's limits.

    The zyklop mini series I can use in all the tiny boxes and tight spaces that have to get into just to get a machine running again.

    The capacitor tester would be perfect for testing run and start capacitors on single phase motors that use to see and check which one has blown.

    And finally the PC tool kit, probably not in my area of expertise but there are occasions when we need to pull apart small circuit boards and check inside scales, computers, ups etc.

    I'd be more than happy to write a detailed review for you after I've put any one of these tools to the test. And happy to go the extra mile to make sure I go to there limits.

    Anything that I can add to my bag to get the job done in a better manner is always a win.

    Thanks for the opportunity and good luck to all the entries.

    Cheers

    Sam.

    • Cancel
    • Vote Up +4 Vote Down
    • Sign in to reply
    • Cancel
  • bradybowers
    bradybowers over 8 years ago

    Hey Randall,

     

    I'm all about the Milwaukee impact driver set.  My folks have the family flying out to visit soon and we've got 2 bathrooms ripped apart.  My mom is being a trooper having to walk up the stairs to use the restroom since she is disabled.   I'm helping my dad do complete renovations on them as fast as possible, but there was a lot of damage to the subfloor from previous work being done wrong.  Since my dad is a retired Air Force electrical engineer we really overdo the renovations to way past code, which comes in handy when riding out hurricanes here in south Texas.  I find I use the heck out of my Porter cable impact driver and the whole 20v 8 piece tool set.  I probably use the impact driver the most and it's funnest* tool to in the bag.  It just sounds like work when it's hammering away.  I find I need hearing protection for this.  I'm currently rebuilding my tool collection with limited funds because of being burglarized at my house.  I have many more remodels todo and I'd love a chance to try these out.  I've sheered dewalt torx bits in 2 before so I want to see how these stack up.  Thanks for your consideration.

     

    Brady Bowers

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • s8548a
    s8548a over 8 years ago

    Hi Randall,

     

    I would like to test the Peak LCR meter and a nice PCB holder stand.

    Thanks.

     

    Cheers,

    Sujith

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago

    I can't believe I didn't think of this before, but I've decided to take up color-coding drill bits : )

    I'm using redred and green marker pensgreen marker pens, since they are the most popular fractional parts that I use. As per the resistor color code, I'll use red paint (red=2) for an X.2mm drill bit, and green=5 paint for a X.5mm bit.

    Therefore, the photo shows an 8.5mm drill bit in my 8.Xmm storage bin.

    I'm painting close to the flutes (so the marker paint doesn't wear off on the chuck) and painting at the end of it too.

    imageimage

    It would be cool to paint the entire value using multiple color bands, but just maybe that's taking it too far : )

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Cancel
  • dougw
    dougw over 7 years ago in reply to shabaz

    Cool idea. The color code is burned into my brain.

    Of course I use mostly English drills - not so amenable to color coding.

    • Cancel
    • Vote Up +7 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 7 years ago in reply to dougw

    Ahh you're right.. not as easy then : (

    I needed a 7/32" hex bit a couple of weeks ago, and even the large DIY stores here don't stock the English sizes at all : (

    They have L sets (allen keys) but I can't get as much torque out of that compared to a bit in a ratchet driver, and the bolt was really stiff.

     

    In the end, I bought a cheap 6mm bit, put it in the vise, and filed the six surfaces down! Since 7/32" is 5.5mm.

    It worked, so now I do have a 7/32" bit : )

    • Cancel
    • Vote Up +5 Vote Down
    • Sign in to reply
    • Cancel
<>