Test & Tools
  • Technologies
  • More
Test & Tools
Forum Changing solenoid valve from normally open to normally closed
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 382 subscribers
  • Views 8044 views
  • Users 0 members are here
  • solenoid valve
Related

Changing solenoid valve from normally open to normally closed

avinashsootre
avinashsootre over 7 years ago

hey all,

i have bought rotex 20201 solenoid valve which is normally open and i wanted to change it to normally closed. Actually out of 3 ports, 1 port is made dummy to make it normally open. So can we change the dummy to other port to make it normally closed solenoid valve? Please do help me out with this.

 

Thanks in advance

  • Sign in to reply
  • Cancel

Top Replies

  • robogary
    robogary over 2 years ago in reply to Gwani +2
    ahhhhhh, be careful of what happens on power loss
  • Fred27
    Fred27 over 7 years ago +1
    The only answer is to take it apart carefully and try it out. With this sort of this you normally find it is either very easy or very difficult.
  • BigG
    BigG over 7 years ago +1
    You have to think about what happens when the valve has no power. In your case when there is no power it is Normally Open. When you energise, something happens to close the valve. In the case of solenoids…
  • Fred27
    Fred27 over 7 years ago

    The only answer is to take it apart carefully and try it out. With this sort of this you normally find it is either very easy or very difficult.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • BigG
    BigG over 7 years ago

    You have to think about what happens when the valve has no power. In your case when there is no power it is Normally Open. When you energise, something happens to close the valve. In the case of solenoids this typically means energising a magnetic field which then moves a coil to close the valve.

     

    You would now have to do the opposite. So I would presume this means moving springs about to ensure the valve is closed when you have no power and then change magnetic polarity to make the valve open. As you are dealing with water or air pressure I would suspect that more engineering is involved to ensure that valve can actually stay closed without power etc.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jw0752
    jw0752 over 7 years ago

    Hi Avinash,

    You can try plugging the top hole and opening the one that is currently capped. Keep in mind these valves have polarity and if you hook them up reversed they will bleed fluid past the valve once the pressure exceeds the compression strength of the internal spring.

     

    John

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Gwani
    Gwani over 2 years ago

    You can wire the coil through the normally closed contacts of an additional normally closed relay.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • robogary
    robogary over 2 years ago in reply to Gwani

    ahhhhhh, be careful of what happens on power loss

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • aspork42
    aspork42 over 2 years ago

    Looking at the data sheet, you really can’t change this. It is set up as normally open and needs power to energize and become closed. Whenever power is lost, there is a spring that will shuttle the valve over to the opened position. You’d need to look up the manufacturer part number to get the opposite version part number.
    Now with logic and a controller you can always invert the logic to get the function you want, but in the case of power loss it is fixed.