Test & Tools
  • Technologies
  • More
Test & Tools
Forum Why is this the meter of Choice, Fluke 87-5?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 388 subscribers
  • Views 4708 views
  • Users 0 members are here
  • dmm
  • meter
  • multimeter
  • fluke
Related

Why is this the meter of Choice, Fluke 87-5?

tbartonnewark
tbartonnewark over 7 years ago

Hello I working on some new marketing content with Fluke

 

What makes the Fluke 87-5 The meter of choice?  It's called an "industrial multimeter" but community members, students, engineers and hobbyist aren't really using it in an industrial setting. 

 

I assumed mA MilliAmp, mV millivolts, ohm settings and display range made it a fit.  But, I was curious what everyone else thought.

 

Thank TB 

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 7 years ago +8
    Hi Tom, I can only speak for myself, but I'm guessing all those categories of users want it for the brand, and all that goes with it (i.e. reliability, safety) and availability/support for many years,…
  • dougw
    dougw over 7 years ago +8
    I don't own one at the moment, but have bought Flukes in the past. People buy them because they have an edge in the following areas: reputation - Fluke has had an excellent reputation for building fine…
  • michaelkellett
    michaelkellett over 7 years ago +6
    I've got an 87-III and an 89-IV (both ancient - the 89 must be 20 years old) as well as several bench DMMs (mainly recent Keithley or Keysight). I look from time to time at new Flukes but the old ones…
Parents
  • shabaz
    shabaz over 7 years ago

    Hi Tom,

     

    I can only speak for myself, but I'm guessing all those categories of users want it for the brand, and all that goes with it (i.e. reliability, safety) and availability/support for many years, and the perception that Flukes stay close to calibration for decades. The 87-V still has some uniquenesses making it very suitable for design engineers, because it can measure current and voltage to extremely fine granularity - ideal for modern circuits.

    But, on a technical level alone, there are other multimeters (from Fluke and other manufacturers) that have better performance in certain areas, and higher count, and are more feature-rich (and some of those features are extremely compelling), but that only partially is responsible for the purchase decision. It can be the other stuff as mentioned too.

    Against non flagship brands, it is easy to make a distinction. Some can drift, others can have flaky rotary dials after a few years, (I experienced that with UNI-T and it put me off forever) and so on. Most students and hobbyists might not use the multimeter at high voltages often, but low-end brands can still fail even if you treat them with kid gloves. So personally I believe it is attractive for the brand associated qualities, plus the very handy granularity - so not necessarily the number 1 choice, but still a good choice depending on price. Anyway it's just an opinion : ) personally I'd like to use one of the logging Fluke's but the current Flukes I use are the 87-V, and 170 series, both purchased new, and an older Fluke model purchased used that I can't recall.

    I think the one observation I've realized over the years is that all engineers want to do more and want higher accuracy and granularity and features, so the multimeters of a decade or two ago that were considered fine for handheld use, although they still function, are no longer as desirable, hence the attraction of meters like the 87-V and other modern multimeters in general.

    If you need more thoughts on this, do let me know.

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • shabaz
    shabaz over 7 years ago

    Hi Tom,

     

    I can only speak for myself, but I'm guessing all those categories of users want it for the brand, and all that goes with it (i.e. reliability, safety) and availability/support for many years, and the perception that Flukes stay close to calibration for decades. The 87-V still has some uniquenesses making it very suitable for design engineers, because it can measure current and voltage to extremely fine granularity - ideal for modern circuits.

    But, on a technical level alone, there are other multimeters (from Fluke and other manufacturers) that have better performance in certain areas, and higher count, and are more feature-rich (and some of those features are extremely compelling), but that only partially is responsible for the purchase decision. It can be the other stuff as mentioned too.

    Against non flagship brands, it is easy to make a distinction. Some can drift, others can have flaky rotary dials after a few years, (I experienced that with UNI-T and it put me off forever) and so on. Most students and hobbyists might not use the multimeter at high voltages often, but low-end brands can still fail even if you treat them with kid gloves. So personally I believe it is attractive for the brand associated qualities, plus the very handy granularity - so not necessarily the number 1 choice, but still a good choice depending on price. Anyway it's just an opinion : ) personally I'd like to use one of the logging Fluke's but the current Flukes I use are the 87-V, and 170 series, both purchased new, and an older Fluke model purchased used that I can't recall.

    I think the one observation I've realized over the years is that all engineers want to do more and want higher accuracy and granularity and features, so the multimeters of a decade or two ago that were considered fine for handheld use, although they still function, are no longer as desirable, hence the attraction of meters like the 87-V and other modern multimeters in general.

    If you need more thoughts on this, do let me know.

    • Cancel
    • Vote Up +8 Vote Down
    • Sign in to reply
    • Cancel
Children
  • abrain
    abrain over 7 years ago in reply to shabaz

    I’ve got both an 87 and a179, but have had the opportunity to try one of those logging versions, a 200 something, I can’t remember which.

     

    Whilst the display was nice, the menu system just wasn’t quite as easy as simply turning the dial and pressing one or two buttons, so for me that ease of use while you’re trying to get your measurements was really important, more than I’d realised.

     

    Flukes are definitely dependable, and on those few occasions when the display seems to show something a little odd going on, there’s always been something odd going on that needed some investigation (like when you’re sure that’s a dc supply, but somehow the smoothing caps were left out and you’re measuring an unsmoothed fully rectified output instead....)

     

    A

    • Cancel
    • Vote Up +3 Vote Down