Test & Tools
  • Technologies
  • More
Test & Tools
Documents Wishlist - What do you need for Soldering?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: dychen
  • Date Created: 18 Jan 2023 11:08 PM Date Created
  • Last Updated Last Updated: 12 Jun 2023 1:58 PM
  • Views 37716 views
  • Likes 15 likes
  • Comments 63 comments
Related
Recommended

Wishlist - What do you need for Soldering?

Broken tip soldering iron
Oh no! I've broken the tip of my soldering iron. This wishlist is coming just in the nick of time!

If you're shopping around for a gift for an electrical engineer or maker, look no further! Soldering is something pretty much every engineer does, and the better the tools, the happier they'll be! In this wishlist, we'll focus on through-hole soldering.

Soldering Iron

Soldering iron

A soldering iron is used to melt the solder that joins the metal pieces together. A soldering iron with adjustable temperature is a useful feature, because component manufacturers will often specify a maximum temperature (along with a duration). An adjustable temperature lets you set the max temperature and not have to worry about damaging the component. 

Buy now

Soldering Iron Base

Soldering iron base

A soldering iron based includes a stand and a sponge for cleaning the tip of the soldering iron.

Buy now

Soldering Station

For engineers who will do a lot of soldering, it might be worthwhile to invest in a good soldering station. 

Soldering Station

Buy now

Soldering Iron Tip

Ah yes, this is what I was looking for! Tips of soldering irons don't last forever, but replacements are available in a variety of sizes.

soldering iron tip

Buy now

soldering iron tip

Buy now

Solder

Solder

Buy now

Flux

Flux Pen


Flux is a cleaning agent that removes oxidation from the metals that will be joined.

Buy now

Desoldering

If you have to repair a circuit, you'll need desoldering tools. Here are some of the most common:

Desoldering Braid (Wick)

Desoldering wick
Wicks are used to absorbing solder after it's been heated.

Buy now

Desoldering Pump

Desoldering pump
You can also use a pump to suck the melted solder in.

Buy now

Desoldering Iron

Desoldering iron
If you need to do a lot of desoldering, it's well worth it to get yourself a desoldering iron, which both melts and removes the solder. 

Buy now

Desoldering Rework Station

Desoldering rework station
A desoldering station lets you adjust the temperature of the desoldering iron, and comes with the desoldering iron, cleaning tools, and nozzles of various sizes.

Buy now

Soldering Iron Tip Cleaner, Brass Wool

Brass wool soldering iron tip cleaner

Buy now



Fume Extractor

The fumes that are released when soldering are pretty nasty. Every bench should have a fume extractor to prevent you from breathing them in.

Fume extractor

Buy now

Fume extractor

Buy now

Pliers

Pliers

To make sure you don't burn your fingers, grab a pair of pliers to hold the wire as you solder.

Buy now

Wire Stripper/Cutter

Wire Stripper Cutter

Wire strippers are a must have when soldering, although I have a friend who is surprisingly good at stripping wires with his teeth. 

Buy now


Helping Hands

Helping hands hold the components in place while you solder, helping to prevent soldering iron accidents.

Helping hands

Buy now

For smaller components, a magnifier is very helpful.

Helping hands with magnifier

Buy now

  • soldering station
  • fume extractor
  • repair
  • through hole
  • desoldering
  • soldering iron
  • soldering
  • flux
  • workbench
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • BigBozo
    BigBozo over 3 years ago +1
    There are quite a few things that can help a soldering procedure, but my biggest tip is to use flux every time. It basically does the work for you, first it lowers the melting point of the solder so even…
  • MarioPJ98
    MarioPJ98 over 3 years ago +1
    Here are the best tips and tricks on soldering: Cleanliness is crucial. Always make sure the soldering iron tip is clean before starting, as a dirty tip can cause poor conductivity and lead to bad…
  • Kolmanpg
    Kolmanpg over 3 years ago +1
    My best tip for soldering is just to practice as much as you can, you do not need to have the best equipment to be good at it, you just need to practice and do it as much as you can and you will become…
  • mikeakohn
    mikeakohn over 3 years ago

    When doing through-hole soldering, I slide the part in through on the top of the board and use masking tape to hold it place before I flip it over to solder the wires on the the bottom of the board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RBuschy
    RBuschy over 3 years ago

    Best "tip" is to get yourself a quality and adjustable iron. I still have the iron i purchased for College 20+ years ago and it is terrible. It has always taken forever to melt the solder... Save yourself the decades long struggle of using a subpar iron.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Davemac
    Davemac over 3 years ago

    Tip tinner/cleaner is one of the best things I ever invested in. It makes keeping the tip of the iron carbon free so much easier 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Kolmanpg
    Kolmanpg over 3 years ago

    My best tip for soldering is just to practice as much as you can, you do not need to have the best equipment to be good at it, you just need to practice and do it as much as you can and you will become a pro at it!!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • panjkov
    panjkov over 3 years ago

    I always make sure that I tin my iron tip after I finish soldering. That protects the tip and saves me from trouble when I need to solder again (I usually don't solder every day). 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Airpaper
    Airpaper over 3 years ago

    Some soldering tips:

    Make sure that your soldering iron is always clean and doesn't have any form of oxidation, especially if you didn't solder in a while. An oxidized tip will make soldering a lot more difficult, since it doesn't conduct the heat nearly as well as a clean tip, and at some point it will cause the solder to ball up on the tip, rather than flow freely.

    Always have some flux ready. Especially for soldering SMD components applying flux before soldering is indispensable. My colleague with over 35 years of experience once called flux "the most important thing in a hardware lab". While this of course is also a bit of an overstatement, the difference that some flux can make should really not be underestimated.

    And lastly, you don't need the best of the best to do a decent job. Of course, as a professional user you will get a lot of value out of a propper soldering station, and it will certainly improve your working process, but something like that 30€ digital soldering iron mentioned in the article is good enough to get started with, especially for people who don't need to solder on a regular basis.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • swalberg
    swalberg over 3 years ago

    I don't think there are a lot of shortcuts to good soldering, and trying to take a shortcut leads to sloppy work. Make sure your wires/boards are secured before soldering otherwise you'll be chasing them around the desk or they'll be moving as the solder cools.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • feralrecords
    feralrecords over 3 years ago

    Buy a soldering station with an adjustable heat dial. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • MarioPJ98
    MarioPJ98 over 3 years ago

    Here are the best tips and tricks on soldering:

    1. Cleanliness is crucial. Always make sure the soldering iron tip is clean before starting, as a dirty tip can cause poor conductivity and lead to bad connections. Clean the tip with a damp sponge or brass wire cleaner regularly.

    2. Choose the right soldering iron for the job. For smaller, delicate components, use a fine-tip soldering iron with lower power. For larger components, a higher-powered soldering iron may be necessary.

    3. Properly heat the joint. It's important to heat the joint for a sufficient amount of time to ensure proper flow of the solder. Heating the joint for too long can damage the component, while not heating it enough can lead to poor conductivity.

    4. Use the right amount of solder. Applying too much solder can lead to short circuits, while not enough can result in poor connections. A good rule of thumb is to use the smallest amount of solder possible to create a solid connection.

    5. Use flux. Flux helps the solder to flow smoothly and ensures a good connection. Apply flux to the joint before soldering, and use a solder with flux core for easier soldering.

    6. Hold the components steady. Use a third hand or other clamping device to hold the components in place while soldering to ensure that the joint remains steady.

    7. Practice, practice, practice. Soldering is a skill that requires practice to perfect. Keep practicing, and you'll soon develop a steady hand and a good eye for detail.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Ozalot
    Ozalot over 3 years ago

    I don't have no where near the knowledge you all have, I don't understand half the terms used. But if I had to give advice based on my limited knowledge it would be ... prepare your working area well making sure you dont burn yourself or the house down. I tend to use heat mats and soldering iron bases. Also make sure you have good lighting.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>