Test & Tools
  • Technologies
  • More
Test & Tools
Documents Wishlist - What do you need for Soldering?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: dychen
  • Date Created: 18 Jan 2023 11:08 PM Date Created
  • Last Updated Last Updated: 12 Jun 2023 1:58 PM
  • Views 37654 views
  • Likes 15 likes
  • Comments 63 comments
Related
Recommended

Wishlist - What do you need for Soldering?

Broken tip soldering iron
Oh no! I've broken the tip of my soldering iron. This wishlist is coming just in the nick of time!

If you're shopping around for a gift for an electrical engineer or maker, look no further! Soldering is something pretty much every engineer does, and the better the tools, the happier they'll be! In this wishlist, we'll focus on through-hole soldering.

Soldering Iron

Soldering iron

A soldering iron is used to melt the solder that joins the metal pieces together. A soldering iron with adjustable temperature is a useful feature, because component manufacturers will often specify a maximum temperature (along with a duration). An adjustable temperature lets you set the max temperature and not have to worry about damaging the component. 

Buy now

Soldering Iron Base

Soldering iron base

A soldering iron based includes a stand and a sponge for cleaning the tip of the soldering iron.

Buy now

Soldering Station

For engineers who will do a lot of soldering, it might be worthwhile to invest in a good soldering station. 

Soldering Station

Buy now

Soldering Iron Tip

Ah yes, this is what I was looking for! Tips of soldering irons don't last forever, but replacements are available in a variety of sizes.

soldering iron tip

Buy now

soldering iron tip

Buy now

Solder

Solder

Buy now

Flux

Flux Pen


Flux is a cleaning agent that removes oxidation from the metals that will be joined.

Buy now

Desoldering

If you have to repair a circuit, you'll need desoldering tools. Here are some of the most common:

Desoldering Braid (Wick)

Desoldering wick
Wicks are used to absorbing solder after it's been heated.

Buy now

Desoldering Pump

Desoldering pump
You can also use a pump to suck the melted solder in.

Buy now

Desoldering Iron

Desoldering iron
If you need to do a lot of desoldering, it's well worth it to get yourself a desoldering iron, which both melts and removes the solder. 

Buy now

Desoldering Rework Station

Desoldering rework station
A desoldering station lets you adjust the temperature of the desoldering iron, and comes with the desoldering iron, cleaning tools, and nozzles of various sizes.

Buy now

Soldering Iron Tip Cleaner, Brass Wool

Brass wool soldering iron tip cleaner

Buy now



Fume Extractor

The fumes that are released when soldering are pretty nasty. Every bench should have a fume extractor to prevent you from breathing them in.

Fume extractor

Buy now

Fume extractor

Buy now

Pliers

Pliers

To make sure you don't burn your fingers, grab a pair of pliers to hold the wire as you solder.

Buy now

Wire Stripper/Cutter

Wire Stripper Cutter

Wire strippers are a must have when soldering, although I have a friend who is surprisingly good at stripping wires with his teeth. 

Buy now


Helping Hands

Helping hands hold the components in place while you solder, helping to prevent soldering iron accidents.

Helping hands

Buy now

For smaller components, a magnifier is very helpful.

Helping hands with magnifier

Buy now

  • soldering station
  • fume extractor
  • repair
  • through hole
  • desoldering
  • soldering iron
  • soldering
  • flux
  • workbench
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • BigBozo
    BigBozo over 3 years ago +1
    There are quite a few things that can help a soldering procedure, but my biggest tip is to use flux every time. It basically does the work for you, first it lowers the melting point of the solder so even…
  • MarioPJ98
    MarioPJ98 over 3 years ago +1
    Here are the best tips and tricks on soldering: Cleanliness is crucial. Always make sure the soldering iron tip is clean before starting, as a dirty tip can cause poor conductivity and lead to bad…
  • Kolmanpg
    Kolmanpg over 3 years ago +1
    My best tip for soldering is just to practice as much as you can, you do not need to have the best equipment to be good at it, you just need to practice and do it as much as you can and you will become…
  • BigBozo
    BigBozo over 3 years ago

    There are quite a few things that can help a soldering procedure, but my biggest tip is to use flux every time. It basically does the work for you, first it lowers the melting point of the solder so even with a cheaper soldering iron it’s easy to work with. And it just directs the solder exactly where you want it, it’s basically telepathic. Another very useful tip is to tin your pads, instead of juggling everything around you already have the solder on the board all that’s left to do is align the part and add heat, 2 things to do with 2 hands, makes it steady and easy. A third tip would be to be careful how long you heat everything, leaving it on for too long could damage parts or the board so try to keep it minimal. Also if you’re working with smaller parts a 30$ digital microscope goes a long way. And don’t forget to always clean your board with some isopropyl when you’re done. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • emaker
    emaker over 3 years ago

    In my opinion, when soldering it is important to choose the right temperature and always use flux. I love soldering, it relaxes me and I love seeing the board being completed, solder by solder!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • MSM
    MSM over 3 years ago

    My Tip,

    Just Plug in and start soldering the broken electronic products.Joy

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rbhaaskar
    rbhaaskar over 3 years ago

    My best tips for better soldering work is first clean the leads of all components with knife to remove any rust or unwanted things. Then place it in PCB and apply little amount of flux. If you are using soldering station then set appropriate temperature for the components or if you are using normal soldering iron apply the lead with in short time to avoid damaging the components. Now you will get better soldering results. Then clean the board with IPA to remove the excess flux and melted flux.

    I am always using the above method for soldering components without getting dry soldering

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • dychen
    dychen over 3 years ago in reply to rsc

    It's actually my soldering iron...one of those ~$20 Wellers that is over 20 years old.  It's definitely served me well, but at some point, the tip broke off. I wasn't aware of mini-wave tips, but I just looked them up, and it would probably work well...the concave part holds solder pretty well.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • varunpandithurai
    varunpandithurai over 3 years ago

    My Best method to solder any SMD is to place the component on the pad and Solder the 1st pin followed by pins at all corner to keep the Component in place and Solder the other pins.

    Don't hesitate on using enough flux, if tue flux is too low then the solder might wear off quickly.

    Adjust the temperature of Soldering Iron as per the component datasheet, too much heat can damage the components, so its better to study the datasheet before.

    The most important thing is to leave your tip with some lead before turning of, by doing so u can avoid oxidation of the Tip.

    Do have a soldering wic to remove bridges or excess lead, Usually most of the bridge can be eliminated with proper soldering itself

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rsc
    rsc over 3 years ago in reply to rsc

    Did I mention - get some hemostats.....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rsc
    rsc over 3 years ago

    Sometimes desoldering ICs that have been soldered using lead free solder on smaller than normal plated through holes and ultra thin traces can be a nightmare.  To avoid damage to the traces and pads, don't try and heat up all the pins at once, instead cut the pins off at the chip first with a dremel or knife then unsolder each pin separately using tweezers or hemostats to pull them out.  Of course this only works if you no longer need the IC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • MarcusStein
    MarcusStein over 3 years ago

    A Silent place with good light, magnifying glass and silence is my idea. :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • spy1
    spy1 over 3 years ago

    my tip is not about soldering well, but soldering with a low quality iron whose tip cant melt solder at all. when im still waiting for my new iron, and i need to solder, i use the upper areas of the iron, and put it in between the pins. then i push a littpe solder in between the pin and the iron, and wait for it to melt, which takes about 10 seconds. its al ittle messy, but its ok for while waiting for a new iron

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>