Test & Tools
  • Technologies
  • More
Test & Tools
Documents Wishlist - What do you need for Soldering?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: dychen
  • Date Created: 18 Jan 2023 11:08 PM Date Created
  • Last Updated Last Updated: 12 Jun 2023 1:58 PM
  • Views 37525 views
  • Likes 15 likes
  • Comments 63 comments
Related
Recommended

Wishlist - What do you need for Soldering?

Broken tip soldering iron
Oh no! I've broken the tip of my soldering iron. This wishlist is coming just in the nick of time!

If you're shopping around for a gift for an electrical engineer or maker, look no further! Soldering is something pretty much every engineer does, and the better the tools, the happier they'll be! In this wishlist, we'll focus on through-hole soldering.

Soldering Iron

Soldering iron

A soldering iron is used to melt the solder that joins the metal pieces together. A soldering iron with adjustable temperature is a useful feature, because component manufacturers will often specify a maximum temperature (along with a duration). An adjustable temperature lets you set the max temperature and not have to worry about damaging the component. 

Buy now

Soldering Iron Base

Soldering iron base

A soldering iron based includes a stand and a sponge for cleaning the tip of the soldering iron.

Buy now

Soldering Station

For engineers who will do a lot of soldering, it might be worthwhile to invest in a good soldering station. 

Soldering Station

Buy now

Soldering Iron Tip

Ah yes, this is what I was looking for! Tips of soldering irons don't last forever, but replacements are available in a variety of sizes.

soldering iron tip

Buy now

soldering iron tip

Buy now

Solder

Solder

Buy now

Flux

Flux Pen


Flux is a cleaning agent that removes oxidation from the metals that will be joined.

Buy now

Desoldering

If you have to repair a circuit, you'll need desoldering tools. Here are some of the most common:

Desoldering Braid (Wick)

Desoldering wick
Wicks are used to absorbing solder after it's been heated.

Buy now

Desoldering Pump

Desoldering pump
You can also use a pump to suck the melted solder in.

Buy now

Desoldering Iron

Desoldering iron
If you need to do a lot of desoldering, it's well worth it to get yourself a desoldering iron, which both melts and removes the solder. 

Buy now

Desoldering Rework Station

Desoldering rework station
A desoldering station lets you adjust the temperature of the desoldering iron, and comes with the desoldering iron, cleaning tools, and nozzles of various sizes.

Buy now

Soldering Iron Tip Cleaner, Brass Wool

Brass wool soldering iron tip cleaner

Buy now



Fume Extractor

The fumes that are released when soldering are pretty nasty. Every bench should have a fume extractor to prevent you from breathing them in.

Fume extractor

Buy now

Fume extractor

Buy now

Pliers

Pliers

To make sure you don't burn your fingers, grab a pair of pliers to hold the wire as you solder.

Buy now

Wire Stripper/Cutter

Wire Stripper Cutter

Wire strippers are a must have when soldering, although I have a friend who is surprisingly good at stripping wires with his teeth. 

Buy now


Helping Hands

Helping hands hold the components in place while you solder, helping to prevent soldering iron accidents.

Helping hands

Buy now

For smaller components, a magnifier is very helpful.

Helping hands with magnifier

Buy now

  • soldering station
  • fume extractor
  • repair
  • through hole
  • desoldering
  • soldering iron
  • soldering
  • flux
  • workbench
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • BigBozo
    BigBozo over 3 years ago +1
    There are quite a few things that can help a soldering procedure, but my biggest tip is to use flux every time. It basically does the work for you, first it lowers the melting point of the solder so even…
  • MarioPJ98
    MarioPJ98 over 3 years ago +1
    Here are the best tips and tricks on soldering: Cleanliness is crucial. Always make sure the soldering iron tip is clean before starting, as a dirty tip can cause poor conductivity and lead to bad…
  • Kolmanpg
    Kolmanpg over 3 years ago +1
    My best tip for soldering is just to practice as much as you can, you do not need to have the best equipment to be good at it, you just need to practice and do it as much as you can and you will become…
  • mkrish_007
    mkrish_007 over 3 years ago

    Cleaning the tip once soldring because avoid Soldring 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • lahcen005
    lahcen005 over 3 years ago

    when I want to solder SMD capacitors I use solder flux and tweezers to hold components in place before soldering.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jaivik_Dhebar
    Jaivik_Dhebar over 3 years ago

    Best trick for soldering irons for through-hole are...

    Soldering iron should be 60W or more, Tip size medium & soldering wire normal.

    For soldering: 

    - grip the pcb, clean the tip

    - take some paste on wire (which is going to solder in pcb)

    - put tip on wire, add solder wire as required 

    - now take again some paste on soldering wire

    - put tip on the spot

    - add soldering wire on it

    - clean the pcb from the extra paste

    - make sure your soldering iron is more than 60W if doesn't then turn off the celling fan

    - now the best soldering is done on it!

    For solder removal:

    Two ways as we know for common: Soldering pump & De-soldering wire

    I prefer De-soldering wire more because soldering pumps does burnt after sometime then doesn't suck solder properly 

    - add soldering paste on pcb

    - grip the De-soldering wire with a small plier

    - put de-soldering wire's end on pcb (where to de-solder)

    - put tip on De-soldering wire then move soldering iron next to holes and pull De-soldering wire slightly till wire gets end

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • marksmol
    marksmol over 3 years ago

    I could use a fume extractor as solder smoke is harmful. In a previous employment they had an add on tube that attached to a wella soldering iron to extract solder fumes but I've not seen such a system in a very long time.

    I'm also on the lookout for a solder pot to tin wires as I make a lot of signal looms. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • TonyL777
    TonyL777 over 3 years ago

    Eye protection, always! Proper tinning of wire and tip... And I prefer a desoldering pump vs solder wick most of the time. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • scottiebabe
    scottiebabe over 3 years ago

    Someday I will try those silicone finger caps perhaps they would stop me from burning my fingers while holding a component in place. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 3 years ago

    my best tips and tricks for soldering are first we should find a high-quality soldering iron / soldering station. Secondly, We should use the correct iron tip shape and size for the required task. Third, we should clean the soldering iron tip from time to time to avoid any imperfection. Fourth, Soldering should be done in well ventilated place like environments or use fume extractor for the purpose as smokes from soldering are pretty harmful. Fifth, soldering irons are hot and should be handled with care and safety, and, should not be laid down on desk while its still being heated. Sixth, we should use flux for avoiding oxidation during soldering. And, Lastly, we should let the solder joints to be cool of its own and after that we should properly inspect the solder joints for any imperfection or loose connections.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • harikamalakarreddy
    harikamalakarreddy over 3 years ago

    1.)For joining two wires first time the both wires and then twist them and apply the solder

    2.) For breadboard modules or microcontrollers like Arduino nano align the male headers in the breadboard and then solder the headers to the module or microcontroller

    3.) For soldering tht components on a pcb bend their lead from other side and cover them with tape on the other side and then solder them

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Arnout
    Arnout over 3 years ago

    One trick I use often for removing two or more bridged pins on an IC package, is to firstly add some solder to the bridged pins, before using solder wick to get rid of the excess solder. This works more reliable than using solder wick without adding solder first!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rsc
    rsc over 3 years ago in reply to JWx

    I was asking myself - "How in the (______) did you break off your soldering iron tip like that?"

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>