Test & Tools
  • Technologies
  • More
Test & Tools
Documents Wishlist - What do you need for Soldering?
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: dychen
  • Date Created: 18 Jan 2023 11:08 PM Date Created
  • Last Updated Last Updated: 12 Jun 2023 1:58 PM
  • Views 37503 views
  • Likes 15 likes
  • Comments 63 comments
Related
Recommended

Wishlist - What do you need for Soldering?

Broken tip soldering iron
Oh no! I've broken the tip of my soldering iron. This wishlist is coming just in the nick of time!

If you're shopping around for a gift for an electrical engineer or maker, look no further! Soldering is something pretty much every engineer does, and the better the tools, the happier they'll be! In this wishlist, we'll focus on through-hole soldering.

Soldering Iron

Soldering iron

A soldering iron is used to melt the solder that joins the metal pieces together. A soldering iron with adjustable temperature is a useful feature, because component manufacturers will often specify a maximum temperature (along with a duration). An adjustable temperature lets you set the max temperature and not have to worry about damaging the component. 

Buy now

Soldering Iron Base

Soldering iron base

A soldering iron based includes a stand and a sponge for cleaning the tip of the soldering iron.

Buy now

Soldering Station

For engineers who will do a lot of soldering, it might be worthwhile to invest in a good soldering station. 

Soldering Station

Buy now

Soldering Iron Tip

Ah yes, this is what I was looking for! Tips of soldering irons don't last forever, but replacements are available in a variety of sizes.

soldering iron tip

Buy now

soldering iron tip

Buy now

Solder

Solder

Buy now

Flux

Flux Pen


Flux is a cleaning agent that removes oxidation from the metals that will be joined.

Buy now

Desoldering

If you have to repair a circuit, you'll need desoldering tools. Here are some of the most common:

Desoldering Braid (Wick)

Desoldering wick
Wicks are used to absorbing solder after it's been heated.

Buy now

Desoldering Pump

Desoldering pump
You can also use a pump to suck the melted solder in.

Buy now

Desoldering Iron

Desoldering iron
If you need to do a lot of desoldering, it's well worth it to get yourself a desoldering iron, which both melts and removes the solder. 

Buy now

Desoldering Rework Station

Desoldering rework station
A desoldering station lets you adjust the temperature of the desoldering iron, and comes with the desoldering iron, cleaning tools, and nozzles of various sizes.

Buy now

Soldering Iron Tip Cleaner, Brass Wool

Brass wool soldering iron tip cleaner

Buy now



Fume Extractor

The fumes that are released when soldering are pretty nasty. Every bench should have a fume extractor to prevent you from breathing them in.

Fume extractor

Buy now

Fume extractor

Buy now

Pliers

Pliers

To make sure you don't burn your fingers, grab a pair of pliers to hold the wire as you solder.

Buy now

Wire Stripper/Cutter

Wire Stripper Cutter

Wire strippers are a must have when soldering, although I have a friend who is surprisingly good at stripping wires with his teeth. 

Buy now


Helping Hands

Helping hands hold the components in place while you solder, helping to prevent soldering iron accidents.

Helping hands

Buy now

For smaller components, a magnifier is very helpful.

Helping hands with magnifier

Buy now

  • soldering station
  • fume extractor
  • repair
  • through hole
  • desoldering
  • soldering iron
  • soldering
  • flux
  • workbench
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • BigBozo
    BigBozo over 3 years ago +1
    There are quite a few things that can help a soldering procedure, but my biggest tip is to use flux every time. It basically does the work for you, first it lowers the melting point of the solder so even…
  • MarioPJ98
    MarioPJ98 over 3 years ago +1
    Here are the best tips and tricks on soldering: Cleanliness is crucial. Always make sure the soldering iron tip is clean before starting, as a dirty tip can cause poor conductivity and lead to bad…
  • Kolmanpg
    Kolmanpg over 3 years ago +1
    My best tip for soldering is just to practice as much as you can, you do not need to have the best equipment to be good at it, you just need to practice and do it as much as you can and you will become…
  • DeltaPi
    DeltaPi over 3 years ago

    Lots of lead free solder, as I do quite a bit of soldering, as well as more soldering iron tips, as the off brand japanese soldering station I got melts them after a few weeks of use. A heat gun for heating up shrink tubing would be quite helpful, and something I have been considering getting for a while. I have never used a desoldering iron before, but from what I have seen it looks like a really helpful tool. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • pandoramc
    pandoramc over 3 years ago

    I have been an interesting concept for SMT soldering. A Hot Plate could be useful for prototyping and quick soldering/desoldering process with SMT in PCB. You can check this video The Best way to Solder? Hot Plate to the rescue! (DIY or Buy) - YouTube for more information.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • manojroy123
    manojroy123 over 3 years ago

    Use thermocouple wire, while desoldering smt or BGA chip on Fr4 PCB, when using hot air. Else it will melt the Fr4 material. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • wolfgangfriedrich
    wolfgangfriedrich over 3 years ago

    Some tips to increase reliability of solder joints:

    The NASA workmanship standards

    Not everything in there applies to hobbyist work, but being aware of the attention to detail cranked up to '11' is not a a bad thing and it is a beautiful read on its own. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rahulkhanna
    rahulkhanna over 3 years ago

    Usage of solder flux helps the solder flow easily and prevents dry solders. Maintaining 350-400°C is the perfect temperature for most of the soldering tasks. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • javagoza
    javagoza over 3 years ago

    I need a precision vice like this one Hitec Mini precision vice

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • JWx
    JWx over 3 years ago

    low melt point solder (eg. Chip Quik)  shabaz mentioned in Hack the Holidays project looks interesting for SMD repair when one cannot use hot air...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • sheil
    sheil over 3 years ago

    I could really use a PCB work-holding solution for when I'm working on and repairing audio and music devices.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • JWx
    JWx over 3 years ago

    The first photo is misleading - it is home-made mini-wave tip. Something like DIY Farnell 2893455 (https://uk.farnell.com/pace/1130-0032-p1/soldering-iron-tip-mini-wave-3/dp/2893455?st=mini-wave) :)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • charlieo21
    charlieo21 over 3 years ago

    My best trick for soldering smd ICs like LQFPs or QFNs is first put solder in pin 1 and solder the IC only on that pin, then start with all the corner pins, this will fix the IC so you can solder the rest of the pins without worrying about the IC moving around.

    Another trick is using a chisel tip is much easier than conical tips.

    Last trick or tip is always use flux.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>