Test & Tools
  • Technologies
  • More
Test & Tools
Documents Tenma 72-7224, o/c  1283640
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: dsohal
  • Date Created: 21 Feb 2011 11:10 AM Date Created
  • Last Updated Last Updated: 27 Feb 2011 1:33 AM
  • Views 612 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Tenma 72-7224, o/c  1283640

1) The data-sheet  from Farnell's site states that the upper Frequency Measurement is  100MHz, whereas the Operating Manual supplied with the instrument limits this to  10MHz.
--reply: Manual 10MHz is correct  ,not 100MHz
2) And this is of  more importance to me. On switch-on and selecting DC current ranges (40A or  400A) the display reads  minus 1.7A changing to around minus1.4A after some  time.
--Reply, pls adjust VR9 and  VR6
 
Please confirm that,  as the Manual (page 41) appears to say, that the 'RELdelta' key is used to  actually ZERO the measurement system, PRIOR to attempting accurate  measurement. As yet I have not set up a test circuit to compare the  clamp-meter's measurement against a direct in-circuit ammeter.
--Reply, yes, pls press  "Rel delta" key before measurement, if so, the obtained  value should be more precise.
Q; Presumably your supplier is saying that, when powered on and switched to 'Amps'  (DC by default), and 'REL delta'  NOT selected, the display SHOULD BE ZERO, and  if not, to open the case and adj. VR9 and VR6 to zero out the  indication(s). This would be somewhat unusual on a (two !) new instrument(s), so  please confirm / elaborate / copy me a schematic, eg. which VR for which range ?  will upper measurement (span) accuracy be affected ? I do realise that the  72-722472-7224 is a low cost instrument but nevertheless (as an Electronics  Engineer) would not, nowadays, expect 'zero errors' of this magnitude. Also, I  can find nothing relating to this on-line".
A:
Generally , we don't recommend to adj VR9/VR6 for end user  as the stored value can be subtracted by press 'REL delta'  before measurement(  every time )to obtaine a precise reading .that is why we do not add the VR9/VR6  adj in user manual. however below information for your  reference.
Yes,  when powered on and switched to 'Amps'  40Vdc and 'REL delta'  NOT selected, the display SHOULD BE around ZERO, and if  not, to open the case and adj. VR9 (coarse)and VR6(fine) to  approach zero.
Attached part location drawing you can find out where  are VR9&VR6.
Attachments:
72-7224.xls72-7224.xls
  • 72-7224
  • tenma
  • o/c
  • 1283640