Test & Tools
  • Technologies
  • More
Test & Tools
Documents Handheld Digital Multimeter
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 12 Apr 2011 2:24 PM Date Created
  • Last Updated Last Updated: 12 Apr 2011 2:31 PM
  • Views 1601 views
  • Likes 0 likes
  • Comments 0 comments
Related
Recommended

Handheld Digital Multimeter

Instrumentation & Measurement Solutions -
Handheld Digital Multimeter

image

Multimeters are mainly used to measure resistance, as well as DC/AC voltage and current. Common multimeters can be divided into two types, desktop and handheld digital multimeters depending on their sizes. Desktop digital multimeters are usually used in labs for high-precision measurement and instrument calibration. Handheld digital multimeters are battery-powered devices, often used for on-site debugging. In recent years, handheld digital multimeters have gained tremendous improvement in measurement precision.

A handheld digital multimeter is basically composed of Analogue Front End (AFE), MCU, Human-machine interface and Power supply. The design of handheld multimeters should focus on the features of low power, high performance and compact size.

 

After a measurement function is selected by the switch, the AFE can start to collect input signals and convert them into digital signals in order to feed into the MCU for processing. http://uk.farnell.com/jsp/bespoke/bespoke7.jsp?bespokepage=common/en/technology-first/applications/instrumentation-measurement/handheld-digital-multimeter.jsp#When measuring resistance, the AFE provides a proper current generated by the inside resistance I-source so that the voltage detected on the measured object is within the input range of the ADC. The detected voltage is amplified and converted into digital signals for data processing by MCU.

  • When measuring AC current, a current shunt is selected to convert the AC current flowing through it into AC voltage. This voltage is converted by the RMS-to-DC converter into a DC voltage, which is then amplified and converted into digital signals for data processing by MCU.
  • When measuring DC current, another current shunt is selected to convert the DC current flowing through it into a DC voltage. The DC voltage is then amplified and converted into digital signals for data processing by MCU.
  • When measuring AC voltage, high voltage input is attenuated while low voltage input remains unchanged. And then it is converted by the RMS-to-DC converter into DC voltage, which is then amplified and converted into digital signals for data processing by MCU.
  • When measuring DC voltage, high voltage input is attenuated while low voltage input remains unchanged. And then it is amplified and converted into digital signals for data processing by MCU.

The MCU controls measurement processes and implements real-time calculations such as averaging and unit conversion for sampled data. The human-machine interface generally includes a display, several functional keys and a switch for selecting measurement functions. An entry-level handheld digital multimeter usually uses a 7-segment LCD, while a high-end multimeter may have a 1/4 VGA OLED. An isolated power supply is adopted in this solution to implement battery management and power conversion to drive different functional blocks.

image

APPLICATION NOTES

 

ANALOG DEVICEAmplifierLow Noise Amplifier Selection Guide for Optimal Noise PerformanceAN-940Click Here
ANALOG DEVICERMS to DCRMS-to-DC Converters Ease Measurement TasksAN-268Click Here
ANALOG DEVICERMS to DCRMS-to-DC ConvertersMT-081Click Here
ANALOG DEVICEDigital IsolatorESD/Latch-Up Considerations with iCouplerRegistered Isolation ProductsAN-793Click Here
LINEAR TECHNOLOGYData Conversion“Easy Drive” Delta-Sigma Analog-to-Digital Converters Cancel Input Current ErrorsDN368Click Here
LINEAR TECHNOLOGYData ConversionHow to Use the World’s Smallest 24-Bit No Latency Delta-SigmaTM ADC to its Fullest PotentialAN80Click Here
LINEAR TECHNOLOGYData ConversionAmplifier Selection Guide for Optimum Noise PerformanceDN355Click Here
TEXAS INSTRUMENTSAmplifierNoise Analysis In Operational Amplifier Circuitsslva043bClick Here
TEXAS INSTRUMENTSData ConversionWhat Designers Should Know About Data Converter Driftsbaa046Click Here
ManufacturerProduct TypeAN TitleAN NumberPart NumberURL


 

WHITE PAPERS

 

TEXAS INSTRUMENTSMicrocontrollerPush Performance and
Power Beyond the
Data Sheet
Click Here
TEXAS INSTRUMENTSMicrocontrollerSerial Wire Debug—Ideal for MicrocontrollersClick Here
TEXAS INSTRUMENTSMicrocontrollerMSP430F21x1 Architecture SummaryClick Here
TEXAS INSTRUMENTSMicrocontrollerThe ultra-low-power USB revolutionClick Here
TEXAS INSTRUMENTSPowerDigital power supply considerations for the analog engineerClick Here


 

EVAL KITS

 

OLIMEXMicrocontrollerMSP430F149 DEVELOPMENT BOARDMSP430-P149MSP430-P149MPS430F149Click Here
OLIMEXMicrocontrollerMSP430F1611 DEVELOPMENT BOARDMSP430-P1611MSP430-P1611MSP430F1611Click Here
OLIMEXMicrocontrollerMSP430F169 DEVELOPMENT BOARDMSP430-P169MSP430-P169MSP430F169Click Here
OLIMEXMicrocontrollerMSP430F249 DEVELOPMENT BOARDMSP430-P249MSP430-P249MSP430F249Click Here
TEXAS INSTRUMENTSMicrocontrollerLM3S2965-IQC50-A2LM3S2965-IQC50-A2 Evaluation Kit with Code Composer StudioEKS-LM3S2965EKS-LM3S2965LM3S2965-IQC50-A2LM3S2965-IQC50-A2Click Here
TEXAS INSTRUMENTSMicrocontrollerLM3S3748-IQC50-A0LM3S3748-IQC50-A0 Evaluation Kit with Code Composer StudioEKS-LM3S3748EKS-LM3S3748LM3S3748-IQC50-A0LM3S3748-IQC50-A0Click Here
TEXAS INSTRUMENTSMicrocontrollerLM3S1968-IQC50-A2LM3S1968-IQC50-A2 Evaluation Kit with Code Composer StudioEKS-LM3S1968EKS-LM3S1968LM3S1968-IQC50-A2LM3S1968-IQC50-A2Click Here
TEXAS INSTRUMENTSMicrocontrollerMSP430F5438 Experimenter BoardMSP-EXP430F5438MSP-EXP430F5438MSP430F5438Click Here
TEXAS INSTRUMENTSMicrocontrollerMSP430FG4618/F2013 Experimenter BoardMSP-EXP430FG4618MSP-EXP430FG4618MSP430FG4618/F2013Click Here
ManufacturerProduct TypeEvaluation Kits TitleEVKs Part NumberPart NumberURL


 

TRAINING

 

NATIONAL SEMICONDUCTORAmplifierLMP827x/LMP223x/LMP7721 Precision AmplifiersLMP827x/LMP223x/LMP7721Click Here
NATIONAL SEMICONDUCTORData ConversionSettling Time Challenges and Improvement Techniques in Precision Signal Path ConversionADC122S101CIMM/NOPBADC122S101CIMM/NOPB,  ADC161S626Click Here
TEXAS INSTRUMENTSAmplifierOPA376: Precision, Low Noise, Low Quiescent Current, Operational AmplifierOPA376Click Here
TEXAS INSTRUMENTSMicroprocessorLowering the Power Consumption of your DesignClick Here
TEXAS INSTRUMENTSMicroprocessorUltra-Low Power MSP430 - The World’s Lowest Power MCUMSP430Click Here
TEXAS INSTRUMENTSMicroprocessorMSP430 MCU Optimization for Ultra-Low PowerMSP430Click Here
TEXAS INSTRUMENTSMicroprocessorMSP430 Ultra-low Power Microcontroller OverviewMSP430Click Here
TEXAS INSTRUMENTSVoltage ReferencePrecision Voltage Reference, Low Noise, Very Low DriftClick Here