Test & Tools
  • Technologies
  • More
Test & Tools
Documents Handheld Oscilloscope
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 12 Apr 2011 4:09 PM Date Created
  • Last Updated Last Updated: 12 Apr 2011 4:14 PM
  • Views 1647 views
  • Likes 0 likes
  • Comments 1 comment
Related
Recommended

Handheld Oscilloscope

Instrumentation & Measurement Solutions -
Handheld Oscilloscope

image

Handheld oscilloscope is the abridged name of Handheld Digital Storage Oscilloscope, which is defined as a compact and reliable oscilloscope that can ensure sufficient operation time even if there is no external power supply when working in the wild. To make sure it can keep working for a sufficient lifetime when powered by the batteries, it is necessary to optimize the design for power consumption, battery capacity, and power conversion efficiency. Firstly, we should adopt the Li-ion batteries featured with high capacity and power density to be the power supply for handheld oscilloscope, which not only is able to provide more power, but also remains small in size. Secondly, we should use a high efficiency DC-DC converter in order to save the power stored in the batteries. Finally, we should simplify the features of the handheld oscilloscope to save power to the maximum extent, for example, reducing the sampling rate to an appropriate level (usually tens of MHz), reducing the times of harmonic analysis or entirely disable the function, and using a smaller display. Now many Handheld oscilloscopes integrate together oscilloscope, multi-meter and paperless recorder to combine measurement, waveform display and recording functions into one platform, greatly facilitating the applications that must be accomplished in the wild or those have no special requirement.

 

image

 

 

APPLICATION NOTES

ANALOG DEVICEDSPEE-349: ADSP-2146x Board Design Guidelines for DDR2 Memory ADSP-2146xClick Here
ANALOG DEVICEDSPUsing the On-Chip Thermal Diode on Analog Devices ProcessorsClick Here
ANALOG DEVICEDSPEE-319: Estimating Power Dissipation for ADSP-21375 SHARC ProcessorsClick Here
ANALOG DEVICEDSPEE-305: Designing and Debugging Systems with SHARC Processors (Rev 1, 11/2006)  Click Here
ANALOG DEVICEDSPEE-296: Using the UART Port Controller on SHARC Processors (Rev 2, 07/2007)  Click Here
ANALOG DEVICEDSPEE-286: Interfacing SDRAM Memories to SHARC Processors (Rev 5, 11/2010) Click Here
TEXAS INSTRUMENTSDSPProgramming the TMS320VC5503/C5506/C5507/C5509/C5509A I2C Peripheral (Rev. A)TMS320VC5506Click Here
TEXAS INSTRUMENTSDSPUsing the USB APLL on the TMS320VC5506/C5507/C5509A (Rev. B)TMS320VC5506Click Here
TEXAS INSTRUMENTSDSPUSB 2.0 Board Design and Layout GuidelinesClick Here
TEXAS INSTRUMENTSDSPUsing the TMS320VC5509/5510 Enhanced HPI (Rev. A) TMS320VC5509/5510Click Here
ManufacturerProduct TypeAN TitleAN NumberPart NumberURL

 

WHITE PAPERS

ManufacturerProduct Type White Paper Title URL

TEXAS INSTRUMENTS DSPEnhance DMA Efficiently Manages Multiple Real-Time Data Streams White PaperClick Here
TEXAS INSTRUMENTS DSPFixed vs. Floating Point white paperClick Her

 

EVAL KITS

ALTIUM FPGAAltium NanoBoard 3000 Series12-400-NB3000XN-0112-400-NB3000XN-01EP3C40F780C8NEP3C40F780C8NClick Here
ALTIUM FPGAAltium NanoBoard 3000 Series12-401-DB3112-401-DB31Cyclone II Click Here
ALTIUM FPGAAltium NanoBoard 3000 Series12-401-DB4012-401-DB40Cyclone III Click Here
ALTERA FPGAArria II GX FPGA Development KitDK-DEV-2AGX125NDK-DEV-2AGX125N Click Here
ALTERA FPGAMAX II Development BoardDK-MAXII-1270NDK-MAXII-1270N
ALTERA FPGANios II Embedded Evaluation Kit,Cyclone III EditionDK-N2EVAL-3C25NDK-N2EVAL-3C25NCyclone III Click Here
ALTERA FPGACyclone III FPGA Starter KitDK-START-4CGX15N/PDK-START-4CGX15N/PCyclone III Click Here
ANALOG DEVICES DSPADSP-21369 SHARC EZ-KIT Lite Evaluation Kit ADZS-21369-EZLITEADZS-21369-EZLITEADSP-21369Click Here
ANALOG DEVICES DSPADSP-21469 SHARC EZ-KIT Lite Evaluation Kit ADZS-21469-EZBRDADZS-21469-EZBRD ADSP-21469Click Here

 

TRAINING

ALTERAFPGACyclone III FPGA Overview Part1Cyclone IIIClick Here
ALTERAFPGACyclone III FPGA Overview Part2Cyclone IIIClick Here
ALTERAFPGAStratix FPGA OverviewStratixClick Here
ALTERAFPGACyclone II FPGA OverviewCyclone IIClick Here
LATTICE SEMICONDUCTORFPGAPower Saving Design Techniques with Low Cost FPGAs Click Here
ManufacturerProduct TypeTraining TitlePart NumberURL

 

  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

    Very informative collection of data and products

    Many thanks

    Peter

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14 Contributor
    e14 Contributor over 15 years ago

    Very informative collection of data and products

    Many thanks

    Peter