Test & Tools
  • Technologies
  • More
Test & Tools
Documents Tenma 72-2500 DDS/ARB WAVEFORM GENERATOR, user manual
  • Blog
  • Forum
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Test & Tools to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: dsohal
  • Date Created: 11 Jan 2016 9:23 AM Date Created
  • Last Updated Last Updated: 13 Jan 2016 11:04 AM
  • Views 2108 views
  • Likes 0 likes
  • Comments 2 comments
Related
Recommended

Tenma 72-2500 DDS/ARB WAVEFORM GENERATOR, user manual

TENMA  72-250072-2500 DDS/ARB WAVEFORM GENERATOR

 

 

 

TENMA 72-2500

Click to zoom

Image is for illustrative purposes only. Please refer to product description.

 

 

TENMA

 

  • Manufacturer: TENMA
  • Order Code: 2450669
  • Manufacturer Part No 72-250072-2500
  • Technical Data Sheet (281.05KB) EN

 

Product Overview


  • Intuitive Interface Design
  • Dual Channels with Standard Performance
  • 200MS/s Sample Rate, 14bits Vertical Resolution
  • Integrated Analogue and Digital Design
  • 4.3" HD Display Panel

Applications

Test & Measurement; System Monitoring; Sensing & Instrumentation; Maintenance & Repair

 

Contents

BNC Cable, Power Cord, USB Cable, PC Software CD

Q; What is duty cycle on wave form generator?

A; The actual duty cycle is limited by 19ns minimum pulse width (There's a design margin for 1ns),

For example: The minimum duty cycle 47.5%  for a 25MHz signal, 38% for 20MHz, 28.5% for 15MHz etc.

 

Attachments:
image72-2500 manual page 1 to 33.pdf
image72-2500 manual page 34 to 73.pdf
image72-2500 manual page 73 to 116 .pdf
  • waveform
  • manual
  • user
  • questions
  • and
  • tenma
  • dds/arb
  • generator
  • answers
  • 72-2500
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply
Parents
  • wa2pux
    wa2pux over 4 years ago

    I'd like to be able to programatically (C#) control the Tenma 72-2500 Sig Gen so I can use it to do some automated testing. Is there a document available that will help me interface with the sig gen to produce a testing program?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • wa2pux
    wa2pux over 4 years ago

    I'd like to be able to programatically (C#) control the Tenma 72-2500 Sig Gen so I can use it to do some automated testing. Is there a document available that will help me interface with the sig gen to produce a testing program?